Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
moving-air-slide10
When the application requires DC input, a brushless DC motor will typically be used.  A brushless DC motor, also known as an EC or “Electrically Commutated” motor, uses an electronic circuit and permanent magnets to generate rotation. The end result is a highly efficient and highly reliable motor. The commutation electronics are typically built right into the motor so the user only needs to apply DC voltage to the motor.
PTM Veröffentlicht am: