Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Fuse-Slide14

The fuse interrupting rating is the maximum amperage at the rated voltage the fuse can safely interrupt. This rating must be greater than the maximum fault (short-circuit) current the circuit can produce. Interrupting ratings for AC and DC currents are different and the fuse data sheet should be consulted before selection.

PTM Veröffentlicht am: