Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PowerStor Supercapacitors Slide 17

Active voltage balancing circuits continually monitor and adjust the voltage across each capacitor to maintain accurate voltage balancing. These circuits provide rapid voltage balancing with only a small amount of additional leakage current, typically only a few micro Amps. This makes active voltage balancing ideal for battery powered applications that require low leakage current. It is also commonly used when larger capacitance values are involved, as leakage current increases with capacitance value resulting in the need for very low value balancing resistors when a passive system is employed.

PTM Veröffentlicht am: