Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
PowerStor Supercapacitors Slide 17

Method one involves calculating an average current based on the provided parameters and then applying the Constant Current Application sizing method. Imax is calculated by Power/Vmin, Imin is calculated by Power/VWV. Now use the Constant Current Method to determine the capacitance value. Using equation 6, one can calculate the capacitance needed by using Iavg which equals 3.72 F. Now using equation 7 to solve for Ccell, the designer can determine the needed capacitance per cell which is 25 F.

PTM Veröffentlicht am:
PTM Updated on: 2021-09-30