Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
PSoC 4 BLE Low Power Wireless Systems Slide 15

This slide provides an overview of the PSoC 4 device families. The PSoC 4 BLE is an expansion of the current PSoC 4 family of which there are parts across the board, the PSoC 4000 starting at the lowest stand. There are the PSoC 4100s and 4200s that users may be familiar with, and Cypress is now adding the two families of the BLE parts in the PSoC 4100 and the PSoC 4200. Some of the future looking parts have also been listed, which are under NDA.

PTM Veröffentlicht am: