Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
ID-Slide6

The CW dual-in-line plug (DIP) connector is used for rapid, permanent connection of ribbon cable to a PC board or to a standard DIP socket when connect/disconnect capabilities are required. The cover is factory pre-assembled to the connector base to simplify assembly to cable and has ridges for cable alignment. CW DIP connectors are Mil-DTL-83503/6 approved. CW’s DIP connectors feature a one piece construction in 14, 16, 24 and 40 pin versions. The patented TORQ-TITE™ contacts ensure reliable gas-tight terminations and accept 28-30 AWG stranded or solid conductors. Optional metal strain relief straps are available and are easily installed. Connection is isolated from mechanical strain by the bend in the cable, as it is folded over the top of the assembled connector. The strain relief strap is placed over the cable and snaps into a recess on the connector. A centralized top cable exit is created in the finished cable assembly. Every contact position is numbered, per Mil- DTL-83503, for easy identification. In addition, a beveled corner at pin one enhances orientation of the connector to the mating DIP socket, even in blind installations.

PTM Veröffentlicht am: