Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
using mult
In this slide, series and parallel configurations of multiple fans are examined. As this figure shows, when a system air flow/pressure curve is overlaid with a parallel performance curve, a higher system resistance results in a lower increase in flow from the parallel configuration. Therefore, parallel configuration should only be used when the fans can operate with a low air impedance near free delivery. With the same analysis, it is shown that the series configuration achieves the best results in a high air impedance system.
PTM Veröffentlicht am: