Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
disc-slide5

The actuating temperature is the temperature when the thermostat will switch from its original state. It is important to note that a thermostat will not switch back to its original state when the temperature drops to just below the switching temperature. An example of this is a normally closed thermostat that switches open at 27°C/81°F, but may drop down to 15°C/60°F before it closes again.

PTM Veröffentlicht am: