Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
NEMA-Slide9

The second common error is to automatically choose metal as the enclosure material. Historically, metal was the standard in the US while plastic is much stronger in Europe and Asia. It is important to keep in mind that NEMA enclosures are available in a wide range of materials. These include various strength plastics, die-cast aluminum, fiberglass and steel.

PTM Veröffentlicht am: