Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Slide9
The TCS™ devices are intended to be used in coordination with an overvoltage limiting device. This voltage limiting device can be a TVS diode, a thyristor, or clamp diodes to a supply rail or ground. The TCS™ device will limit the current into the protected device during a surge event as well as provide voltage isolation between the voltage limiting device and the protected device.
PTM Veröffentlicht am: