Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
magjack-slide11

In order to meet electrical standards, the included components within the MagJack must provide isolation and EMI Suppression, this is done with Isolation Transformers, and the EMI suppression is done with the Common Mode Chokes. For the unused pairs within certain communication standards the MagJack is terminated with what is known as a Bob Smith Termination, which is composed of 75 ohm resistors and a 1000 pF, 2K(2000)volt capacitor.

PTM Veröffentlicht am: