Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
9159-slide9

This view shows the entire 9159 system. By placing a socket on one end of the PCB and a plug on the other, the designer can build a single LED board regardless of where it is in the assembly . This simplifies his entire product and only requires him to build a single PCB which is a huge design and cost savings. The wired plug creates the input of power and signals onto the PCB’s and the 2 position shorting socket will close the circuit.

PTM Veröffentlicht am: