Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
precision-slide4

The screw and nut lap joint is an improvement using high grade fasteners that ensure alignment of the two halves. Adjustment to compensate for wear is possible. There is a still a large area where the two halves meet on the bearing surface and the nut turns on one half with a metal-to-metal interface which can lead to premature wear and tear on the joint.

PTM Veröffentlicht am: