Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide2

NAND Flash memory stores data in an array of memory cells comprised of floating-gate transistors. Programming, reading and erasing NAND Flash cells is achieved by manipulating voltage applied to each cell. This electrical activity effectively wears out the physical structure of the cell over time, thus resulting in a finite lifetime for the memory cells. This lifetime is measured in terms of Program/Erase (P/E) cycles and is affected by both process geometry and the number of bits stored in each cell.

PTM Veröffentlicht am: