Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
four limit plate
The TS Series may be configured as a one axis or two axis joystick. Two axis configuration options include the Square, Guided Feel and Plus Limiter Plates. The Square option allows for free, 360 degree omnidirectional control. The Plus Limiter Plate option allows for two axis control, but only into the cardinal directions.
PTM Veröffentlicht am:
PTM Updated on: 2018-09-06