Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Weigh Scale Introduction Slide 11

As discussed on the previous slide, a high level of precision and resolution can be required in a weigh scale application. Also of critical importance are the stability and noise filtering. From the stability standpoint, weigh scales are subject to strict regulations regarding accuracy, and many scales are not in environments that allow easy calibration. Filtering capability is also critical for the same reasons. Additionally, the requirements for the different weigh scale markets are different, and require ADCs optimized for that type of market.

PTM Veröffentlicht am: