Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Amplitude-Slide5

The input and output buses of the map represent angle and amplitude values, respectively. But because the buses have finite resolution (P-bits of angle resolution and D-bits of amplitude resolution), the output is by definition quantized. Therefore, consider taking the entire contents of the map, that is, one complete cycle of a sinusoid and calculate its spectrum with an FFT. The resulting spectrum would show the main sinusoidal signal along with a plethora of spurious content, namely quantization spurs. The width of the map’s output bus D defines the amplitude resolution of the map and directly affects the MAGNITUDE of the quantization spurs. On the other hand, the width of the map’s input bus P defines the angle (or phase) resolution of the map, and determines the number of quantization spurs with only limited impact on the magnitude of the quantization spurs.

PTM Veröffentlicht am: