Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
26482-slide3

Some of the key benefits of the PT series are the capability of incorporating both power and signal into one contact insert arrangement along with the connector being fully mated in one-quarter turn of the coupling nut. The connector is water resistant when using an “E” service class version, with exceptional resistance to damage in high shock and vibration applications. Also, with a wide temperature range, the PT series will work in harsh climates. The connectors and the gold plated contacts will withstand more than five hundred mating cycles. The 26482 Series 1 connectors are UL recognized under file #E115497, Vol. 1, Sec. 5.

PTM Veröffentlicht am: