Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
LM2594-slide13

In the adjustable output practical design example, a maximum input voltage of 28V, and an output voltage of 20V will be selected. The maximum load current will be 0.5.A. Using the formula given in Step 1 of the previous slide, the E*T value will be 35.2V-usec.

PTM Veröffentlicht am: