Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Max10 Motor Control Slide 1

Welcome to the Intel® MAX®10 Motor Control using Single-Chip Low-Cost Non-Volatile FPGA product training module. The purpose of this presentation is to provide an introduction to the Intel® MAX®10 FPGA in motor control applications. It will discuss the benefits of this product in the motor control applications. Additionally, it will explain the Intel® motor control IP as well as cover the DoC (Device-on-Chip) system debug tools.

PTM Veröffentlicht am: