Maker.io main logo

Using Flask to Send Data to a Raspberry Pi

88

2017-12-05 | By SparkFun Electronics

License: See Original Project Wireless Arduino Raspberry Pi SBC

Courtesy of SparkFun

In this tutorial, we’ll show you how to send data from cheap WiFi nodes to a Raspberry Pi over an internal WiFi network. It relies on the Flask framework for Python, which is a relatively simple-to-use method of creating a web application that can execute Python scripts.

Using Flask to Send Data to a Raspberry Pi

We’ll use a Raspberry Pi 3 and SparkFun ESP8266 Thing to demonstrate. We’re going to send a very simple signal from the Thing board to the RasPi - just a signal to turn an attached LED on or off. Hopefully, it’ll be obvious from the example how to send more complex signals and run more complex scripts upon receipt.

Required Materials

You’ll need the items on this wishlist to complete this tutorial. Substitutions can be made; a Raspberry Pi Zero W can be substituted for the Pi 3, for instance, and individual components can be sourced instead of the full starter kit.

Raspberry Pi + Flask Tutorial

Break Away Headers - 40-pin Male (Long Centered, PTH, 0.1")

USB micro-B Cable - 6 Foot

SparkFun Beefy 3 - FTDI Basic Breakout - DEV-13746

Break Away Headers - Straight - Not Carried by Digi-Key

SparkFun ESP8266 Thing - WRL-13231

Raspberry Pi 3 Starter Kit - KIT-13826

Required Tools

No special tools are required to follow this tutorial. You will need a soldering iron, solder, and general soldering accessories.

Soldering Iron - 30W (US, 110V) - TOL-09507

Solder Lead Free - 15-gram Tube - TOL-09163

Hardware Hookup

You’ll need to do some basic breadboarding to prepare for this tutorial. Don’t worry, we’ll walk you through all of it.

Raspberry Pi Connections

The connections for the Pi are simple: we’re just connecting one LED to GPIO pin 2. See the Fritzing diagram below for information on how to do that.

Raspberry Pi Connections

ESP8266 Thing Connections

Hook up two of the buttons as seen in the Fritzing diagram below.

ESP8266 Thing Connections

One of the buttons will turn the remote LED on, the other will turn it off. We’re going to assume that you’re capable of soldering the headers onto the ESP8266 Thing board yourself, but if you need some help, check out our soldering tutorial.

This is also where you’ll use the long, centered breakaway headers. A six-pin group of them inserted into the breadboard aligned with the programming pins on the Thing will give you a place to plug in the FTDI board.

Raspberry Pi Software

Let’s get down to business and program the Raspberry Pi to serve a web app that we can use for data connection. This tutorial assumes that you have some familiarity with Linux and Python to follow along.

Installing Flask

The first step is adding support for Flask to the RasPi. Python is already installed and support for using GPIO through Python, so we don’t need to worry about that.

All of these commands can be run either on a serial terminal opened on the Raspberry Pi directly with the Pi hooked up to a monitor, or remotely with a Pi via an SSH connection. However, we’re not going to get into how to set up and run a Pi without a monitor.

The first thing you need to do is install the Flask framework. There are a lot of additional packages that can be used with Flask, but we only need the basic package for this tutorial.

Copy Code
sudo pip install flask

 Next, we’re going to create the directory within which the app will run. These commands will create the directory and ensure that you’re working inside that directory.

Copy Code
mkdir FlaskTutorial
cd FlaskTutorial

The next step is to create a blank Python file in the directory called "app.py". This is the file that we’re going to put our code into. Open that file in your favorite text editor (the Pi has VI, Nano, and a textpad).

Copy Code
touch app.py

Then put the following code into it.

Copy Code
#!/usr/bin/python

from flask import Flask
import RPi.GPIO as GPIO

GPIO.setmode(GPIO.BCM)  # Sets up the RPi lib to use the Broadcom pin mappings
                        #  for the pin names. This corresponds to the pin names
                        #  given in most documentation of the Pi header
GPIO.setwarnings(False) # Turn off warnings that may crop up if you have the
                        #  GPIO pins exported for use via command line
GPIO.setup(2, GPIO.OUT) # Set GPIO2 as an output

app = Flask(__name__)   # Create an instance of flask called "app"

@app.route("/")         # This is our default handler, if no path is given
def index():
    return "hello"

# The magic happens here. When some http request comes in with a path of
#  gpio/x/y, the Flask app will attempt to parse that as x=pin and y=level.
#  Note that there is no error handling here! Failure to properly specify the
#  route will result in a 404 error.
@app.route('/gpio/<string:id>/<string:level>')
def setPinLevel(id, level):
    GPIO.output(int(id), int(level))
    return "OK"

# If we're running this script directly, this portion executes. The Flask
#  instance runs with the given parameters. Note that the "host=0.0.0.0" part
#  is essential to telling the system that we want the app visible to the 
#  outside world.
if __name__ == "__main__":
    app.run(host='0.0.0.0', port=5000)

There are comments in the code to cover most questions but I want to highlight three things:

  • First, there’s no error checking here. The message is passed as the path requested via an HTTP request, and that request can contain just about anything. A request of the format GET /gpio/2/0 will set the pin low, for instance. However, GET /bats/are/bugs is equally valid, it just won’t do anything and the app will return a "404 error."

  • Second, the parameter host='0.0.0.0' is required to let the app know that you want the application visible to external clients. If you omit this, you’ll still be able to test the app by visiting localhost:5000 in a web browser on the Pi, it just won’t be visible externally.

  • Third, the most commonly used port number is 5000, but you can use any port you want.

ESP8266 Thing Firmware

Now we’ll need to program the Thing. This portion assumes that you’ve followed the SparkFun ESP8266 Thing hookup guide and can program the ESP8266.

Example Code

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Here’s the firmware that I’ve written to send the proper page requests to the Raspberry Pi.

Copy Code
#include <Arduino.h>
#include <ESP8266WiFi.h>
#include <ESP8266WiFiMulti.h>
#include <ESP8266HTTPClient.h>

ESP8266WiFiMulti WiFiMulti;

void setup() 
{
  Serial.begin(115200);

  // ESP8266 takes a few moments to boot, so we give it a few seconds
  for(uint8_t t = 4; t > 0; t--) 
  {
    Serial.printf("[SETUP] WAIT %d...\n", t);
    Serial.flush();
    delay(1000);
  }

  // Add the WiFi access point information
  WiFiMulti.addAP("SSID", "PASSWORD");

  // Set our buttons pins to inputs with pullup resistors enabled
  pinMode(12, INPUT_PULLUP);
  pinMode(13, INPUT_PULLUP);

}

void loop() 
{
  // wait for WiFi connection
  if((WiFiMulti.run() == WL_CONNECTED)) 
  {
    // Check if button 12 is pressed...
    if (digitalRead(12) == LOW)
    {
      //...and if so, issue a GET request of the format
      //  gpio/x/y, where x is the desired pin and y is the
      //  desired level to set the pin to. Currently the
      //  Flask app only supports pin 2.
      HTTPClient http;
      // Be sure to change this IP address and port number
      //  to match yours!!!
      http.begin("http://10.8.253.193:5000/gpio/2/0");
      int httpCode = http.GET();
      http.end();
    }
    // Repeat the process for pin 13.
    if (digitalRead(13) == LOW)
    {
      HTTPClient http;
      // Be sure to change this IP address and port number
      //  to match yours!!!
      http.begin("http://10.8.253.193:5000/gpio/2/1");
      int httpCode = http.GET();
      http.end();
    }
  }
  else
  {
    Serial.println("No WiFi");
  }
}

 Hopefully, the code and comments make it clear what’s going on. Two quick reminders:

  • First, the IP address and port number in the functions http.begin() are mine from development. You’ll have to change them to match the IP address and port number used on your Raspberry Pi.

  • Second, don’t forget to put in your SSID and PASSWORD for your wireless network.

Try It Out!

By now, you ought to have everything ready to go. You’ll need to start the script on the Raspberry Pi. Enter these commands in the subdirectory where you created the ‘app.py’ file:

Copy Code
chmod a+x app.py
./app.py

 You should see a message, then, like the one below.

Flask Tutorial

As you can see, I pressed the buttons a couple of times to show you what it looks like when a client makes an HTTP request. Flask reports the IP address of the client, the date and time stamp of the request, the contents of the request, and the result of the request (in this case, 200, or "success"). This is a useful tool to make sure that your requests are actually making it through to the Flask server and not disappearing into the ether somewhere.

Resources and Going Further

Now that you’ve successfully got Flask framework up and running between a Raspberry Pi and ESP8266, it’s time to incorporate it into your own project!

For more information, check out the resources below:

  • Flask Framework - Official Flask website.

  • Simple Flask Tutorial - This basic Flask tutorial will walk you through taking Flask a little bit farther than we have here. - Complex Flask Tutorial - This more advanced tutorial walks you through far more complex tasks with Flask, leading up to creating a Twitter clone that you can host yourself!

  • Complex Flask Tutorial - This more advanced tutorial walks you through far more complex tasks with Flask, leading up to creating a Twitter clone that you can host yourself!

Herst.-Teilenr. 13231
ESP8266 THING
SparkFun Electronics
Herst.-Teilenr. 13746
BRIDGE USB 2.0 MODULE
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.