Maker.io main logo

Sequencer in a PS4 Controller - YouTube Makers Secret Santa 2024

263

2024-12-22 | By bekathwia

License: See Original Project

This year, for YouTube Makers Secret Santa, I got Look Mum No Computer. Sam performs ‎with his modular synth and other cool audio equipment and collects obsolete technology for his ‎museum in Kent, UK. We share a love for hacking toys and other ways to use electronics to be ‎creative. I built him an audio sequencer in an old PS4 controller using sounds from his museum’s ‎sample packs.‎

Materials and tools:‎

I started this project two years ago. The first stage was making a breakout board for the buttons ‎on the PS4 controller, which is the most ubiquitous obsolete tech for me at the moment– I have a ‎bunch of these kicking around that no longer work for whatever reason, but the form factor is ‎ergonomic and the buttons work fine. I used my new breakout board to make a prototype ‎sequencer that plays sounds when the buttons are pressed. ‎

becky-stern-secret-santa-2024-06

This project went through a few different stages. The initial circuit I made was used to reverse ‎engineer the button mapping. The first versions of the sequencer circuit are based on John ‎Park’s open-source breakbeat breadboard project, which runs loops and one-shots in Circuit ‎Python on an RP2040 board.‎

Here’s where the perfboard prototype merges with the breakout board PCB project. Despite ‎having a lot of experience in the hardware world, this is only my second official PCB design ‎project. If you’re a perpetual beginner like me, you might like my introductory video series about ‎DIY electronics on the DigiKey YouTube channel.‎

Assembling the circuit

becky-stern-secret-santa-2024-02

I sent off the new board design to be manufactured. These new boards came quickly in the mail, ‎and I started populating them with the sequencer parts. It’s so satisfying when a component fits ‎perfectly. And it’s so annoying when you realize you’ve made a mistake. For one, I used the ‎wrong spacing for these plated through holes that are supposed to line up with my audio amp. ‎So, to connect the amp to my board, I had to fuss with individual wires or bend the headers to ‎make everything fit. At least it’s a workable mistake, and it's easy to fix for the next board ‎revision.‎

But this version with the sequencer on the PCB wasn’t working how I wanted it to. Previously, ‎the design used an external speaker component to play the audio. But I wanted to use the ‎controller’s onboard speaker, which involved carefully harvesting the special clips from the ‎original controller boards so that I could reattach them to my own. My aux-out audio was working ‎fine but when I flipped the switch to use the speaker, the amp would get hot, and no sound would ‎play. I spent a long time looking at my circuit design and probing at it with a multimeter before I ‎figured out my error, and the project sat on the shelf most of the time.‎

becky-stern-secret-santa-2024-07

When I found out I got Sam for Secret Santa, my motivation for the project was renewed, since I ‎knew Sam would get a kick out of using a newly obsolete toy to play with sounds created at his ‎museum. I had to figure out what was wrong with the speaker output part of my circuit. My ‎instinct was to phone a friend to ask if I could go over the board layout together. But half the ‎benefit of that is just having someone you must explain each element to, and often talking it out ‎will reveal the solution before any other feedback is provided. So before phoning a friend, I ‎utilized rubber duck debugging, which is a technique from the software world where you talk ‎through your project in plain language, to a rubber duck or something similar. This helped me ‎come up with new things to test, and eventually, I figured it out. I had mistakenly tied my speaker ‎negative to my circuit’s ground. They are most certainly not the same thing, but it was easy for ‎me to overlook during the transition from protoboard to custom PCB.‎

So, I took a sharp craft knife to my PCB to cut the traces connecting the speaker negative to the ‎circuit’s ground plane and used a multimeter to make sure there was no longer continuity ‎between the speaker negative and the circuit’s ground. I used a little wire to jump from the amp ‎to the speaker contact, and I was in business. It’s not like this speaker sounds great or anything, ‎but I think it’s super cool to make a circuit that reuses it. Of course, for performing or recording, ‎the aux out will give you better audio quality.‎

becky-stern-secret-santa-2024-03

I kept whipping up circuits until I got two that worked well. The tiny buttons under the Share and ‎Options buttons on the PS4 controller proved too small for me to solder by hand, even after ‎switching to the smallest tip I have. So, the next version of this project will have the surface ‎mount components machine assembled by a PCBA service such as JLCPCB.‎

Audio processing

The way this sequencer works is that the sounds designated as loops will always be playing in ‎the background, and the buttons toggle their mute status. The other sounds are one-shots, which ‎play once every time you press their buttons. What’s cool is that the sounds don’t interrupt each ‎other, they overlay, so you can really jam out and make your own composition.‎

becky-stern-secret-santa-2024-04

I shopped for sound samples from Sam’s museum store. I had a blast curating two groups of ‎sounds, one for each of the two controllers I wanted to send him. There are tons of sound packs ‎available, and hopefully after reading this guide, he’ll be able to swap out the sounds to suit his ‎needs on any given day.‎

To make the sounds compatible with life on a microcontroller, a little audio processing needs to ‎be done to each file. For this, I used the free software Audacity to mix stereo down to mono, ‎change the format to 16-bit PCM, and the project sample rate to 22Khz.‎

Then it’s just a matter of loading up the new, crunchier sound files onto the board, which mounts ‎like a USB drive on your computer and editing the code to make sure it references the file ‎names of the sounds we’re using.‎

While I still prefer coding in Arduino, I have to admit Python is really easy to learn, and these ‎days the cost has come way down on chips that have the extra processing power needed to run ‎an interpreted language like CircuitPython. So, I may be an old dog learning new tricks but I’m ‎not gonna be a curmudgeon about it.‎

Final Finishes

To decorate the controllers, I swapped out the plastic buttons with replacement ones I found ‎online and switched up the parts between them to make each one unique.‎

becky-stern-secret-santa-2024-05

I wanted to decorate them even further and, I remember meeting a little girl named Zelda at ‎Open Sauce this year who asked if I might make something with the Furby parts I have left over ‎from my teardown video. Great idea, Zelda. Sam loves Furbies even more than I do. Ultimately, ‎I went with just one of Furby’s ears, the one that still had its LED assembly intact, and wired it up ‎to power and ground on my circuit. Usually, I would use epoxy for something like this instead of ‎hot glue, but I simply didn’t have time to wait for the glue to dry, I was overdue to get this thing in ‎the mail on its way to the UK.‎

Check out Sam’s video to watch him open my gift. My Secret Santa this year was James ‎Bruton, and he made me a cool mechanical motorcycle game, which you can watch him build in ‎his video. This huge collab is a circle, so you can keep watching until you get back to where you ‎started.

Herst.-Teilenr. 5302
KB2040 RP2040 KEE BOAR DRIVER
Adafruit Industries LLC
Herst.-Teilenr. 1492
FPC ADAPTER 50PIN 0.5MM PITCH
Adafruit Industries LLC
Herst.-Teilenr. 50YXF10MEFC5X11
CAP ALUM 10UF 20% 50V RADIAL TH
Rubycon
Herst.-Teilenr. CF14JT220R
RES 220 OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
Herst.-Teilenr. CF14JT1K00
RES 1K OHM 5% 1/4W AXIAL
Stackpole Electronics Inc
Herst.-Teilenr. 430451035836
SWITCH TACTILE SPST-NO 0.05A 12V
Würth Elektronik
Herst.-Teilenr. R-667834
SWITCH TACTILE SPST-NO 0.02A 15V
Mitsumi
Herst.-Teilenr. JS102011SAQN
SWITCH SLIDE SPDT 300MA 6V
C&K
Herst.-Teilenr. THB001P
SWITCH JOYSTICK ANALOG 50V
C&K
Herst.-Teilenr. SJ-43516-SMT-TR-PI
CONN JACK 4COND 3.5MM SMD R/A
Same Sky (Formerly CUI Devices)
Herst.-Teilenr. PB-2712PQ
SPEAKER 8OHM TOP PORT 85DB ROUND
Mallory Sonalert Products Inc.
Herst.-Teilenr. 404070001
TWEEZERS POINTED FINE 12 5.32"
Seeed Technology Co., Ltd
Herst.-Teilenr. MN35
DIGITAL MINI MULTIMETER
FLIR Extech
Herst.-Teilenr. 32614
POCKET PRECISION 4-IN-1 SCREWDRI
Klein Tools, Inc.
Herst.-Teilenr. 3197
VISE 6.14" JAW LOW PROFILE
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.