Maker.io main logo

Overclocking Raspberry Pi Pico 2

576

2025-03-28 | By Pimoroni

License: See Original Project Microcontrollers Raspberry Pi MCU

Courtesy of Pimoroni

Guide by Pimoroni

How fast can RP2350 really go? Mike starts his Christmas holidays with a deep dive into ‎Pico 2 overclocking, with the assistance of a seasonally appropriate amount of dry ice ❄️‎

A couple of years ago Raspberry Pi posted about overclocking a regular Pico to a ‎ridiculous degree - achieving a 1 GHz overclock and (briefly) boosting the performance of ‎the Pico above the original Pi.‎

Picos overclock very well, and the original Raspberry Pi Pico will normally run at over ‎‎400MHz if given a 1.3V core voltage. On the RP2040 that is as far as you can easily go ‎because the on-board voltage regulator is limited to supplying a maximum of 1.3V.‎

When I first got my hands on the RP2350 datasheet, one thing I noticed rather quickly was ‎that the voltage regulator could have the voltage limit disabled, so that voltages above 1.3V ‎could be requested. And once I got a Pico 2, I was intrigued to see how it would behave at ‎higher core voltage (and whether the magic smoke would come out if I raised the voltage ‎too high!)‎

Initial experiments

Using this MicroPython script I was able to request different voltages from the regulator. To ‎find out how fast the RP2350 would clock at a given voltage I ran a simple test that ‎computed 100 factorial and checked the answer was correct, and then incremented the ‎clock speed and continued until it stopped working.‎

I then did a more rigorous test using the MicroPython performance benchmark to find out ‎whether things were stable. Generally, I had to back off the CPU clock by 20MHz or so in ‎order for the performance benchmark to run multiple times cleanly, compared to how fast it ‎would pass the very simple 100! test. I live bleated (that's what we're calling Bluesky posts ‎for now) my experimentation and some details about the RP2350 as I was doing this.‎

Voltage, max stable clock speed and temperature for those initial tests was as follows:‎

table_1

This was the first time I'd really felt an RP2 chip getting hot - RP2040s running at 400 MHz or ‎so and 1.3V only get a little warm.‎

Adding some cooling

adding_2

To combat the heat issue, I added a tiny heatsink to the RP2350 on the Pico 2, and set up a ‎small PC fan pointing at it to give good airflow. I again live bleated the experiment, pushing ‎the RP2350 to higher voltages and clock speeds:‎

table_3

I'll admit that I was rather concerned going above 2.0V - while the on-board regulator ‎provides 0.05V or 0.1V increments up to 2.0V, the next step up from 2.0V is 2.35V. This ‎seemed like it was getting a long way above the stock 1.1V core voltage, and I thought the ‎danger of cooking the RP2350 was rising.‎

However, it turned out the performance gain from 2.0 to 2.35V wasn't as much as would be ‎expected, and on further investigation the voltage that the voltage regulator was supplying ‎didn't actually make it above about 2.2V - the on-board regulator isn't able to provide ‎enough current to run the RP2350 at these high voltages.‎

Test Point 7‎

So, how did I find out that the supplied voltage wasn't as high as requested? It turns out the ‎Pico 2, rather handily, has a test point on the back that allows you to measure the core ‎voltage. It was therefore very easy to probe it with my multimeter and see the voltage being ‎delivered didn't match up to the requested voltage.‎

But if you can probe the voltage here, it would also be straightforward to inject a voltage ‎externally. That would mean we could use a bench power supply to provide as much voltage ‎and current as the Pico 2 could take!‎

Taking it further

A plan forms

I'd been chatting to the folks at Pimoroni about these experiments, whilst helping them with ‎the Presto firmware and other bits and pieces. Niko from the Pimoroni team suggested, ‎perhaps jokingly, that we should try a Liquid Nitrogen overclock.‎

I'd arranged to pop in to visit Pimoroni HQ at the start of my Christmas break, so we ‎wondered if it might be possible to give this a try. However, LN2 is a little tricky to handle ‎and not totally straightforward to acquire. I was also worried that we could have problems ‎with the soldering, PCB, or connections to the Pico cracking under the extreme cold of LN2.‎

Solid CO2 (AKA dry ice) on the other hand, is relatively easy to acquire and requires only ‎fairly basic safety precautions. It should allow cooling of the Pico 2 to around -80C, which ‎seemed like it would be enough to give a decent speed boost. Niko ordered some dry ice ‎and the plan was set.‎

‎⚠️ (Editorial note: do not experiment with solid CO2 / dry ice unless you know what ‎you're doing, have considered the problems that carbon dioxide sublimation and things ‎being cooled to -80C can cause and have taken appropriate safety precautions!)‎

Test setup

I wanted to make sure we were pretty rigorous about the testing - unlike the earlier ‎experiments using the MicroPython performance benchmark, I wanted to get both cores ‎running flat out. Therefore, I decided to use the freely available CoreMark benchmark as the ‎test, as this would report result comparable to other CPUs, and it would check for correct ‎operation and report errors if there were problems.‎

I also wanted the option of running the Pico from the ring oscillator, as described in the ‎Raspberry Pi article linked at the top. Additionally, we weren't quite sure whether the crystal ‎oscillator frequency might be changed by very low temperatures. Therefore, to measure ‎time accurately I sent a 1MHz clock into the Pico 2 under test, and used a simple PIO ‎program to count the cycles. This allowed us to run from the ring oscillator or crystal and ‎get accurate benchmark results measured using a known good clock.‎

I also made some other adaptations to Protik Banerji's version of Coremark for RP2040, ‎to:‎

  • Compile for RP2350, and get two core operation working

  • Use a copy to RAM build so we got maximum performance and didn't need to worry ‎about the flash clock divider

  • Use UART output rather than a USB console to avoid USB interrupts slowing down ‎the test and make it easier to recover from the RP2350 crashing‎

  • Print the temperature from the RP2350's on board temperature sensor after each run

  • Run repeatedly in a loop instead of just once

  • Add a prompt before the runs start to allow the voltage to be set (or the on-board ‎regulator to be disabled), and the frequency to be set or the ring oscillator to be ‎selected

  • Add a check for console input after each run, allowing the configuration to be ‎modified, or the pico to be rebooted into DFU mode without having to hit the ‎BOOTSEL button. The latter meant we could update things even if it was difficult to ‎press that button when it was buried in dry ice‎

I used a version of Álvaro Fernández Rojas' pico-uart-bridge on a Pico W to communicate ‎with the Pico 2 under test. This was modified to provide the 1 MHz reference clock, and also ‎look for lines starting "Temp" or "CoreMark" and send them over WiFi.‎

Using MicroPython on a PicoVision, and a modified version of the temperature display ‎example, I read the temperature and CoreMark readings from the Pico W and graphed them ‎on a monitor, so we could see what was happening while running the tests (I wrote this part ‎in traditional hacker style entirely in my hotel room the night before going into Pimoroni HQ, ‎using the dodgy hotel WiFi and the TV in the room to test it!)‎

Getting set up

First up we needed to get all three Picos involved in the setup, and the surrounding hardware ‎working and verified. At first, we had some problems with the WiFi communication, which ‎wasn't implemented in the most reliable way, but that seemed to settle down after some ‎initial hiccups.‎

We got the test Pico 2 running at 100MHz to establish a baseline. Jon at Pimoroni also ‎pointed out that to make things easier to read it would be better to report a number in MHz ‎instead of the CoreMark score, this was achieved simply by taking the ratio of the CoreMark ‎score at 100MHz to the CoreMark being reported. As the CoreMark was running from ‎internal RAM the score should be entirely linear with frequency.‎

getting_4

Let's cool the Pico 2!‎

Next up we got the Pico 2 I'd been using for all the testing so far, complete with its tiny ‎heatsink, and covered it in dry ice.

cool_5

We did some initial testing using the internal voltage regulator, and got it stable at 700MHz ‎with ease:‎

testing_6

Let's cook the Pico 2!‎

We wanted to push up to see where the limits were, so we wired up a power supply to test ‎point 7, disabled the onboard voltage regulator and nervously increased the voltage above ‎the maximum of 2.2 V that I had managed before.‎

Up and up the voltage went, and while we got diminishing returns on the frequency ‎achievable, the magic smoke stayed inside the chip!‎

Here we got to 800MHz at 2.8V:

cook_7

We realised our setup here was not ideal, as the ground for the core voltage was going via ‎the Pico W. We measured the voltage at the Pico in the dry ice and it was around 200mV ‎lower than the voltage being supplied, due to the resistance through that long path. With ‎that in mind we pushed the voltage up to 3.3V and even a little higher, but it didn't allow that ‎much more speed - the fastest we got to was 840MHz and that wasn't stable for long, we ‎think due to the RP2350 heating up while drawing around 1A of current!‎

Despite this abuse the Pico 2 still works just fine!‎

Ring oscillator experiments

The RP2350 datasheet suggests you can "automatically overclock" using the ring oscillator ‎‎- the concept is that because the ring oscillator itself changes frequency in line with the core ‎voltage and temperature of the chip, the same ring oscillator setting should be stable ‎across all conditions. This appears very much not to be the case (at least while using the ‎Arm cores - see later).‎

I had found that (air cooled) using the "TOOHIGH" setting and maximum drive strength the ‎Pico 2 ran ok up to around 1.5V and then failed, with the observed frequency at lower ‎voltages being lower than the maximum that could be run from the crystal oscillator, but ‎then it is going up past the maximum frequency as the voltage increased. I'm not sure why ‎this is. Using a drive strength one notch less for one of the two stages had it stable up to the ‎maximum I had tested air cooled, so this was the initial setting we tried using.‎

However, as we got the voltage higher, at around 2.6V again the RP2350 would crash when ‎running from the ring oscillator, we tried backing off the drive strength which helped a bit, ‎but ultimately it was difficult to find a setting that would run stably at the highest voltages, ‎while being close to the frequency we'd managed with the crystal. That was a bit ‎unfortunate, given that at frequencies above 800MHz we could only step the frequency from ‎the crystal in increments of 12MHz.‎

Finding a better Pico 2

The Pico 2 that we were using was just the first one I had bought, with no selection based on ‎whether it was a particularly good one for overclocking. Pimoroni rustled up 7 Pico 2s for me to test to try and find one that might overclock the best.‎

I quickly ran the MicroPython frequency search test (linked near the top) on all of them, ‎finding that at 1.1V they would max out at between 316 and 336MHz. Mark from Pimoroni ‎soldered up the two best ones for further testing. We soldered a few more pins this time to ‎get access to another ground, so the core voltage supply didn't go via the Pico W.‎

How fast can we go?‎

Despite being the fastest at 1.1V, the first Pico 2 we tested wasn't that much better than the ‎initial one. We were briefly able to run it at 850MHz at 3.05V, but it wasn't stable. (This is ‎‎850MHz measured by dividing the CoreMark, we requested 852MHz, but it seems got ‎slightly less due to the crystal being cold or some other effects of the high core voltage). ‎Going higher than 3.05V seemed to actually make it less stable, so this seemed to be the ‎limit. At 840MHz requested frequency it ran for a couple of minutes, but we saw errors ‎reported from the CoreMark so there must have been errors running some instructions.‎

Thinking that a lot of the problem in getting faster was just the chip warming up too fast, we ‎looked for a larger thermal mass to try and keep it cooler for longer. Paul produced a big ‎chunk of copper, significantly larger than the Pico 2 itself, which seemed promising.‎

fast_8

We tried attaching this to the Pico 2 with a couple of thermal pads, but it seems they didn't ‎provide great thermal conductivity at these low temperatures, because the results were ‎actually worse with this than without any heatsink at all! That was a shame - maybe we ‎should have tried just getting direct contact of the copper on top of the chip, but we were ‎worried about shorts.‎

We switched over to the other Pico 2 and attached a heatsink designed for the BCM2712 on ‎the Pi 5 to it. That got better results - obviously, the simple test at 1.1V room temperature ‎doesn't account for everything! This one would briefly manage 864MHz requested (reported ‎‎860.7MHz), and would run stable at 840MHz for some time, with no errors. The best so far!‎

switched_9

Testing the RISC-V cores

The RP2350 is an interesting chip, with two RISC-V cores in addition to the two more ‎established ARM cores. Mark had reminded me that we should try the RISC-V cores for ‎comparison, and I got the image built for them - this is pretty simple to do, you just need to ‎install the RISC-V version of gcc and change the PICO_PLATFORM setting to rp2350-riscv.‎

I found that CoreMark actually gave a slightly higher performance per MHz using the RISC-V ‎cores - just under 5% faster. So, if you have an integer-only use for the RP2350 it is definitely ‎worth checking if the RISC-V cores might give better performance!‎

Adjusting the PicoVision monitor for the CoreMark per MHz, we got the same Pico 2 running ‎again.‎

Maximum speed

Ramping the voltage up again running off the ring oscillator, with the drive strength one ‎notch off maximum on one of the two stages, this time we found it didn't crash as the ‎voltage increased, until we got to around 3.0V. That meant that at around 2.95V we had a ‎stable overclock of 820-840MHz running off the ring oscillator (with the fluctuation in ‎frequency due to temperature).‎

Switching over to the crystal, with 3.05V we got 861.6MHz (864MHz requested) running ‎cleanly, and it even ran for nearly a minute at 873.5MHz before crashing. We had no luck ‎trying to get a requested frequency of 888MHz to run.‎

speed_10

So, the top speed we managed was 873.5MHz, though when we tried this again the Pico ‎refused to start at 3.05V, so I guess we were beginning to cause some damage with the high ‎voltage.‎

For a final test we left it running on the ring oscillator at 2.95V, and it ran for around 10 ‎minutes before we let it get a little too warm (up to around -20C).‎

Conclusions

Firstly, the RP2350 and Pico 2 is incredibly hardy. Despite the cold temperatures, some ‎accidental shorting due to moisture when running it while cooling and extremely high core ‎voltages, none of the 3 Pico 2s we were playing with are dead - and I don't think there's any ‎way you would be able to tell that they had been through this treatment.‎

Above 700MHz the extra performance you get ramping up the voltage gives diminishing ‎returns. This maybe because we just weren't able to keep the chip cool enough - just ‎packing dry ice around it, it becomes difficult to carry enough heat away. Liquid nitrogen ‎might be interesting to experiment with to go further.‎

Given this experimentation, it seems around 1.6V from the voltage regulator should easily ‎allow a 500MHz or slightly faster overclock without needing any additional cooling and ‎likely without really causing much damage to the Pico - it might be interesting to run a Pico ‎‎2 loaded like that for a few days and see if anything bad happens.‎

Playing with dry ice is fun! If we get a chance to do this again, we should also try ‎overclocking a Pi 5, and see if we could get a speed record there. Although that could be ‎rather more expensive - the great thing about using Pico 2 for this, is that at under £5 per ‎board you can treat them with reckless abandon - after all, they each cost less than a pint ‎of beer!‎

That's all folks!

Herst.-Teilenr. SC1631
RASPBERRY PI PICO 2 RP2350
Raspberry Pi
Herst.-Teilenr. SC0915
RASPBERRY PI PICO RP2040
Raspberry Pi
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.