Maker.io main logo

Inspector Gadget: Making Penny’s Computer Book

110

2023-10-17 | By bekathwia

License: See Original Project

 

Today, I’m sharing a special Arduino project – a replica of Penny’s computer book from ‎Inspector Gadget.‎

book_1

book_2

book_3

I carved out a real book to fill it with electronics that look and behave like the book in the cartoon. ‎It’s powered by an Arduino Nano ESP32, which is available at DigiKey.‎

Research

research_4

The first step to any good prop replica is thorough research. I gathered up a bunch of visuals of ‎Penny’s book to inform my bill of materials. It’s a relatively thick book with a blue cover, and it’s ‎got a small screen and button matrix on the cover, though you never actually see Penny using ‎this feature in the show.‎

step_5

step_6

step_7

step_8

step_9

On the inside left, there’s a 3x4 button panel, a portrait-oriented screen, twelve illuminated green ‎buttons, a white button that lights up red, and three small square buttons, one each red, yellow, ‎and blue. On the inside right, there’s a large screen, which I plan to emulate stylistically rather ‎than literally.‎

Supplies

supplies_10

To shop for the parts I needed, I used DigiKey’s extensive catalog filters. Here's a list of all the ‎parts:

Tools:‎

Making the Body of the Book

body_11

For the main body of the book, I looked into blank books but couldn’t find any thick enough to ‎look right or hold all the components. So, I figured the least terrible printed hard-cover book to ‎destroy would be a collection of stories that are not at all scarce.‎

cut_12

I cut the cover to make way for a character LCD and matrix button panel. I sandwiched my ‎small cutting mat in the book to prevent cutting further than the cover layer.‎

inside_13

inside_14

Inside, I laid out the parts for the left panel and arranged the button sets onto some small ‎perfboards. The mockup was looking good, so I could go ahead and solder the buttons in place.‎

solder_15

solder_16

solder_17

Once I had the holes in the cover made and verified the components fit, I got to painting the ‎book blue. I used a mixture of blue acrylic paint and acrylic matte medium, and I covered the ‎interior pages of the book with painter’s tape so I could easily handle the whole thing, painted the ‎front, back, and spine, and set it up to dry overnight.‎

image36

Then I tested out my button panel by wiring it up to an Arduino Uno running a simple program to ‎toggle the LED on and off when the button is pressed.‎

Making the Inside of the Book

making_18

making_19

The next step is where things start to get messy– cutting out the interior body of the book. I used ‎a ruler and utility knife to make progressively deeper cuts through the pages and used some ‎clamps to help hold the pages in place. I also cut a passageway through the bound edge, so I ‎could run wires between the two sides of the open book.‎

passage_20

passage_21

I wired up the rest of the green button panel and fed its stranded wires through the hole I had cut ‎through the spine. Each button is wired up like the big white one shown here– all grounds are ‎connected to one wire, and then another two wires go to the switch and the LED.‎

panel_22

Next, it was time to install the other tested components into the book. I soldered stranded wires to ‎a TFT display and threaded them to the right side of the book.‎

install_23

I connected the gray button panel to an audio FX board loaded with sounds from the show and ‎installed the speaker in the right side of the book. Then, I used little pieces of cardboard and my ‎hot glue gun to secure the components in place.‎

connect_24

connect_25

I gave up on the idea that the book would fold shut again, so I glued the pages to each other in ‎the flipped-open position. I used rulers and clamps to hold the pages together while the glue dried.‎

idea_26

I’m using the Arduino Nano ESP32 as the microcontroller brain of this project. It’s got wifi and ‎Bluetooth crammed into a tiny footprint, supports both Arduino and MicroPython, and it’s ‎compatible with the Arduino IoT Cloud. I like that it has castellated pins so I can solder it directly ‎to a breadboard and keep my circuit profile as low as possible.‎

The Uncut Pages

uncut_27

uncut_28

uncut_29

Before I could embed any more components into the right side, I needed to sort out the ‎remaining uncut pages. Using a separate paper template cut to match the interface, I cut a few ‎pages to serve as the compartment’s solid cover.‎

Then I cut a piece of black paper to match the openings on the left, and one big opening on the ‎right. Since some of the printed pages and component perfboard was visible, I used smaller ‎pieces of black paper to shore up the layer behind the black paper.‎

paper_30

I used that rectangle to guide cuts through the remaining right-side pages to create one large ‎cavity where the microcontroller can live.‎

The Electronics

electronics_31

I have the ESP32 board driving the display and fun Wi-Fi features of this project, but it simply ‎doesn’t have enough i/o pins to deal with all the buttons and LEDs wired up on the left side, so I ‎employed an Arduino MEGA dedicated just to the illuminated buttons. They share power and ‎ground.‎

image37

The MEGA also drives the pixel animation on a NeoPixel stick, which I’m using to simulate a ‎screen animation from the book in the show. I took a tip from Nerdforge and layered printed ‎transparency and paper to create a graphic with more dimension.‎

More About the WiFi

more_32

The program generates a network you can join called Penny’s Computer Book, which launches ‎a captive portal after you join it.‎

program_33

program_34

The page you’re shown has buttons that control some different outputs on the TFT display ‎including the MAD graphic, calling Brain the dog, and showing you the components used to build ‎the book.‎

Project Code and Circuit Diagram

Here is the code for both the Arduino Nano ESP32 and MEGA.‎

And the circuit diagram for this project:‎

diagram_35

This project will be on display at the DigiKey booth at Maker Faire Rome 2023, along with ‎Penny’s video watch, which I’ll show you how to build in a future post.

Herst.-Teilenr. ABX00092
ARDUINO NANO ESP32 NO HEADERS
Arduino
Herst.-Teilenr. A000067
ARDUINO MEGA2560 ATMEGA2560
Arduino
Herst.-Teilenr. A000066
ARDUINO UNO R3 ATMEGA328P BOARD
Arduino
Herst.-Teilenr. 2478
GRAPHIC DISPLAY TFT RGB 2.4"
Adafruit Industries LLC
Herst.-Teilenr. 320.02E11.094GRY
SWITCH TACT SPST-NO 0.025A 50V
E-Switch
Herst.-Teilenr. CFPB-1CC-5G2
SWITCH PUSH SPST-NO 1MA 20V
Nidec Components
Herst.-Teilenr. UB215SKG035C-1JB
SWITCH PUSH SPDT 0.4VA 28V
NKK Switches
Herst.-Teilenr. 320E11RED
SWITCH TACT SPST-NO 0.025A 50V
E-Switch
Herst.-Teilenr. 320E11BLU
SWITCH TACT SPST-NO 0.025A 50V
E-Switch
Herst.-Teilenr. 320E11YEL
SWITCH TACT SPST-NO 0.025A 50V
E-Switch
Herst.-Teilenr. 4445
SPEAKER 4OHM TOP PORT
Adafruit Industries LLC
16MM PANEL MOUNT MOMENTARY PUSHB
Herst.-Teilenr. 1502
16MM PANEL MOUNT MOMENTARY PUSHB
Adafruit Industries LLC
Herst.-Teilenr. 292
I2C/SPI CHARACTER LCD BACKPACK
Adafruit Industries LLC
2MM PITCH 25-PIN FEMALE SOCKET H
Herst.-Teilenr. 2672
2MM PITCH 25-PIN FEMALE SOCKET H
Adafruit Industries LLC
Herst.-Teilenr. 2868
ADDRESS LED MODULE SERIAL RGBW
Adafruit Industries LLC
Herst.-Teilenr. 2030
EVAL BOARD FOR TPS61030
Adafruit Industries LLC
Herst.-Teilenr. MN35
DIGITAL MINI MULTIMETER
FLIR Extech
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.