Maker.io main logo

CLUE Case

75

2024-01-09 | By Adafruit Industries

License: See Original Project 3D Printing Displays LCD / TFT

Courtesy of Adafruit

Guide by Ruiz Brothers

Overview

 

In this project we’re making a wearable case for the Adafruit Clue ‎board!‎

The CLUE features the same shape and size as the BBC micro:bit so ‎it’ll work with existing add-ons.‎

Adafruit Clue has a 1.3in IPS LCD color display with tons of sensors, so ‎you can make projects with text and graphics!‎

case_1

case_2

We designed and 3d printed a case for the CLUE, so you can easily ‎wear it like a badge or watch.‎

It has enough room for a lipo battery, so you can make your projects ‎portable.‎

You have access to the edge connector, so you can use the touch ‎pads as controls for your projects.‎

case_3

The CLUE is packed with sensors like an accelerometer, gyroscope magnetometer, barometric pressure, humidity, temperature, ‎microphone, light, color, proximity and much more!‎

CLUE features the nRF52840 cortex M4 processor with 2mb of ‎internal flash memory.‎

It also has a microphone, speaker, NeoPixel, and a STEMMA ‎connector so you can plug and play even more sensors!‎

With Bluetooth, you can make wireless projects that can control your ‎BLE devices.

So, you can control your phone using Apple’s Music Service to play, ‎pause and even change the volume!

features_4

features_5

Parts

For a Badge - grab a lanyard

For 3D Printing‎

3D Printing

‎3D Printed Parts‎

STL files for 3D printing are oriented to print "as-is" on FDM style ‎machines. Original design source may be downloaded using the ‎links below.

  • clue-frame.stl

  • clue-case.stl

  • clue-lid.stl

  • clue-strapA.stl

  • clue-strapB.stl

parts_6

Download STLs

Edit CAD files

Edit Watch Bands

Slicing Parts

Supports recommended around the lanyard ears and slide switch. ‎Slice with setting for PLA material.‎

The parts were sliced using CURA using the slice settings below.‎

  • PLA filament 220c extruder

  • ‎0.2 layer height

  • ‎10% gyroid infill

  • ‎60mm/s print speed

  • ‎60c heated bed

slicing_7

Wrist band parts are optimized for flexible materials, rigid material ‎will not allow the bands to fit.‎

Flexible bands

This design requires an extruder capable of printing with flexible ‎materials. If you're using standard Ninjaflex material (85A shore ‎hardness), we recommend printing slow, around 20 to 40mm/s with ‎the extruder temperature set to 240c.‎

You can also use Cheetah Ninjaflex, which has a higher shore ‎hardness (95A). The only difference will be in how flexible and how ‎grippy the texture is.‎

bands_8

Dual Color Bands

Print from 0mm to 0.8mm to print the first bottom color. ‎

Then print from 0.8mm to 6mm to print the top colors of the band.‎

Retraction clean up

Flexible materials may need retraction disabled to print successfully, ‎so we'll need to clean any leftover material around the slots and ‎grooves on the bands.‎

Customize Watch Band

The design of the watch band can be adjusted using Autodesk ‎Fusion 360. Change the parameters to adjust the width, length, and ‎number of holes on the band.‎

Patterns

We can change the patterns for each band by editing the features in ‎the timeline.‎

design_9

design_10

‎Assemble

The bezel is attached to the front of the case to keep the display ‎nicely secured.‎

Use a drop of glue on each edge of the corners. Align the bezel to the ‎light sensor (rectangle). A fan is helpful, so the glue doesn't haze the ‎case.‎

assemble_11

Tabs on the end press fit into the slits on the side of the case. ‎

The wristband with the nubs is pressed into the slits with the ends ‎first. Orient the end vertically and press each end. Use pliers to pull ‎the ends through the slits on the case.

case_12

case_13

Slide switch

Use a slide switch with a JST adapter to turn the Clue on and off.‎

Short the JST extension cable to 120mm long. Split the power (red) ‎wire at 42mm and solder each end to the middle pin the on the slide ‎switch and either the left or right pin.‎

switch_14

Mount CLUE

Plug the JST cable into the CLUE. Carefully bend the wires and pass ‎them between the JST port and the reset button. ‎

Align the CLUE buttons to the cutouts on the case and press fit into ‎place.‎

mount_15

mount_16

Insert slide switch

Angle the slide switch between the two walls and carefully press fit ‎into place. You can gently pull the metal tabs on the slide switch to ‎increase the tolerance.‎‎ ‎

Plug in battery

Plug the lipo battery into the JST extension. Use a small amount of ‎sticky tac to adhere the battery to the CLUE. position the battery so it ‎doesn't overlap the reset button.‎

plug_17

Press fit lid

Make sure the battery and wires are away from the walls and reset ‎button. Align the tabs on the case to the divots on the lid and press ‎fit close.‎

press_18

press_19

Wear

The nubs on the wrist band press fit into the hole on the opposite ‎band. Use the slit on the end to tuck in the bands and keep it nice ‎and tight.‎

wear_20

Badge

The case is also badge compatible! You can attach our lanyard to the ‎cat ears and wear to your next conference! ‎

badge_21

Herst.-Teilenr. 4500
CLUE NRF52840 EXPRESS
Adafruit Industries LLC
Herst.-Teilenr. 3987
CIRCUIT PLAYGROUND LANYARD
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.