Maker.io main logo

Bluetooth LE based LCD messenger using STM32

91

2022-08-12 | By Sheikh Shuhad

License: General Public License

1. Introduction

The project is based on STM32 Nucleo-144 which controls LCD display using BleuIO.

For this project, we will need two BleuIO USB dongles, one connected to the Nucleo board and the other to a computer, running the web script. When the BleuIO Dongle is connected to the Nucleo board's USB port, the STM32 will recognize it and directly start advertising. This allows the Dongle on the computer port connect with the web script.

With the web script on the computer, we can send message to LCD screen connected to STM32 using BleuIO.

We have used a STM32 Nucleo-144 development board with STM32H743ZI MCU (STM32H743ZI micro mbed-Enabled Development Nucleo-144 series ARM® Cortex®-M7 MCU 32-Bit Embedded Evaluation Board) for this example. This development board has a USB host where we connect the BleuIO dongle.

If you want to use another setup you will have to make sure it supports USB Host and beware that the GPIO setup might be different and may need to be reconfigured in the .ioc file.

About the Code

The project source code is available at Github.

https://github.com/smart-sensor-devices-ab/stm32_bleuio_lcd.git

Either clone the project or download it as a zip file and unzip it into your STM32CubeIDE workspace.

If you download the project as a zip file, you will need to rename the project folder from ‘stm32_bleuio_lcd-master’ to ‘stm32_bleuio_lcd’

Bluetooth low energy lcd message

Connect the SDA to PF0 on the Nucleo board and SCL to PF1.

Then setup I2C2 in the STM32Cube ioc file as follows. (Make sure to change the I2C speed frequency to 50 KHz as per LCD display requirements.)

Bluetooth low energy lcd message

Bluetooth low energy lcd message

Bluetooth low energy lcd message

Bluetooth low energy lcd message

In the USBH_CDC_ReceiveCallback function in USB_HOST\usb_host.c we copy the CDC_RX_Buffer into an external variable called dongle_response that is accessible from the main.c file.

Copy Code
void USBH_CDC_ReceiveCallback(USBH_HandleTypeDef *phost)
{
if(phost == &hUsbHostFS)
{
// Handles the data recived from the USB CDC host, here just printing it out to UART
rx_size = USBH_CDC_GetLastReceivedDataSize(phost);
HAL_UART_Transmit(&huart3, CDC_RX_Buffer, rx_size, HAL_MAX_DELAY);

// Copy buffer to external dongle_response buffer
strcpy((char *)dongle_response, (char *)CDC_RX_Buffer);

// Reset buffer and restart the callback function to receive more data
memset(CDC_RX_Buffer,0,RX_BUFF_SIZE);
USBH_CDC_Receive(phost, CDC_RX_Buffer, RX_BUFF_SIZE);
}

return;
}

In main.c we create a simple interpreter so we can react to the data we are receiving from the dongle.

Copy Code
void dongle_interpreter(uint8_t * input)
{

if(strlen((char *)input) != 0)
{
if(strstr((char *)input, "\r\nADVERTISING...") != NULL)
{
isAdvertising = true;
}
if(strstr((char *)input, "\r\nADVERTISING STOPPED") != NULL)
{
isAdvertising = false;
}
if(strstr((char *)input, "\r\nCONNECTED") != NULL)
{
isConnected = true;
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_1, GPIO_PIN_SET);
}
if(strstr((char *)input, "\r\nDISCONNECTED") != NULL)
{
isConnected = false;
HAL_GPIO_WritePin(GPIOE, GPIO_PIN_1, GPIO_PIN_RESET);
}


if(strstr((char *)input, "L=0") != NULL)
{

isLightBulbOn = false;
//HAL_GPIO_WritePin(Lightbulb_GPIO_Port, Lightbulb_Pin, GPIO_PIN_RESET);
lcd_clear();

writeToDongle((uint8_t*)DONGLE_SEND_LIGHT_OFF);

uart_buf_len = sprintf(uart_tx_buf, "\r\nClear screen\r\n");
HAL_UART_Transmit(&huart3, (uint8_t *)uart_tx_buf, uart_buf_len, HAL_MAX_DELAY);
}

if(strstr((char *)input, "L=1") != NULL)
{
isLightBulbOn = true;
writeToDongle((uint8_t*)DONGLE_SEND_LIGHT_ON);


lcd_clear();

lcd_write(input);

}

}
memset(&dongle_response, 0, RSP_SIZE);
}

We put the interpreter function inside the main loop.

Copy Code
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();

/* USER CODE BEGIN 3 */
// Simple handler for uart input
handleUartInput(uartStatus);

// Inteprets the dongle data
dongle_interpreter(dongle_response);

// Starts advertising as soon as the Dongle is ready.
if(!isAdvertising && !isConnected && isBleuIOReady)
{
HAL_Delay(200);
writeToDongle((uint8_t*)DONGLE_CMD_AT_ADVSTART);
isAdvertising = true;
}
}
/* USER CODE END 3 */

Using the example project. What we will need:

Importing as an Existing Project

From STM32CubeIDE choose File>Import…

Bluetooth low energy lcd message

Then choose General>Existing Projects into Workspace then click ‘Next >’

Bluetooth low energy lcd message

Make sure you’ve chosen your workspace in ‘Select root directory:’

You should see the project “stm32_bleuio_SHT85_example”, check it and click ‘Finish’.

Bluetooth low energy lcd message

Running the example

Upload the code to STM32 and run the example. The USB dongle connect to STM32 will start advertising automatically.

Send Messages to LCD screen from a web browser

Connect the BleuIO dongle to the computer. Run the web script to connect to the other BleuIO dongle on the STM32. Now you can send messages to the LCD screen.

For this script to work, we need

Create a simple html file called index.html which will serve as the frontend of the script. This html file contains some buttons that help connect and read advertised data from the remote dongle, which is connected to stm32.

Copy Code
<!DOCTYPE html>
<html lang="en">
<head>
<meta charset="UTF-8" />
<meta http-equiv="X-UA-Compatible" content="IE=edge" />
<meta name="viewport" content="width=device-width, initial-scale=1.0" />
<link
href="https://cdn.jsdelivr.net/npm/bootstrap@5.1.3/dist/css/bootstrap.min.css"
rel="stylesheet"
integrity="sha384-1BmE4kWBq78iYhFldvKuhfTAU6auU8tT94WrHftjDbrCEXSU1oBoqyl2QvZ6jIW3"
crossorigin="anonymous"
/>
<title>Send message to STM32 LCD display using Bluetooth LE</title>
</head>
<body class="mt-5">
<div class="container mt-5">
<h1 class="mb-5">Send message to STM32 LCD display using Bluetooth LE</h1>
<button class="btn btn-success" id="connect">Connect</button>
<div class="row">
<div class="col-md-4">
<form method="post" id="sendMsgForm" name="sendMsgForm">
<div class="mb-3">
<label for="msgToSend" class="form-label">Your Message</label>
<input
type="text"
class="form-control"
name="msgToSend"
id="msgToSend"
required
maxlength="60"
/>
</div>

<button type="submit" class="btn btn-primary">Submit</button>
</form>
</div>
</div>

<br />
<button class="btn btn-danger" id="clearScreen" disabled>
Clear screen
</button>
</div>

<script src="script.js"></script>
</body>
</html>

Create a js file called script.js and include it at the bottom of the Html file. This js file uses the BleuIO js library to write AT commands and communicate with the other dongle.

Copy Code
import * as my_dongle from 'bleuio'
const dongleToConnect='[0]40:48:FD:E5:2F:17'
document.getElementById('connect').addEventListener('click', function(){
my_dongle.at_connect()
document.getElementById("clearScreen").disabled=false;
document.getElementById("connect").disabled=true;
document.getElementById("sendMsgForm").hidden=false;
})

document.getElementById("sendMsgForm").addEventListener("submit", function(event){
event.preventDefault()
console.log('here')


my_dongle.ati().then((data)=>{
//make central if not
if(JSON.stringify(data).includes("Peripheral")){
console.log('peripheral')
my_dongle.at_central().then((x)=>{
console.log('central now')
})
}
})
.then(()=>{
// connect to dongle
my_dongle.at_getconn().then((y)=>{
if(JSON.stringify(y).includes(dongleToConnect)){
console.log('already connected')
}else{
my_dongle.at_gapconnect(dongleToConnect).then(()=>{
console.log('connected successfully')
})
}
})
.then(()=>{
var theVal = "L=1 " + document.getElementById('msgToSend').value;
console.log('Message Send 1 '+theVal)
// send command to show data
my_dongle.at_spssend(theVal).then(()=>{
console.log('Message Send '+theVal)
})
})

})
});



document.getElementById('clearScreen').addEventListener('click', function(){
my_dongle.ati().then((data)=>{
//make central if not
if(JSON.stringify(data).includes("Peripheral")){
console.log('peripheral')
my_dongle.at_central().then((x)=>{
console.log('central now')
})
}
})
.then(()=>{
// connect to dongle
my_dongle.at_getconn().then((y)=>{
if(JSON.stringify(y).includes(dongleToConnect)){
console.log('already connected')
}else{
my_dongle.at_gapconnect(dongleToConnect).then(()=>{
console.log('connected successfully')
})
}
})
.then(()=>{
// send command to clear the screen
my_dongle.at_spssend('L=0').then(()=>{
console.log('Screen Cleared')
})
})

})
})

The script has a button to connect to COM port on the computer. There is a text field where you can write your message. Your messages will be displayed on LCD screen connected to STM32 board.

To connect to the BleuIO dongle on the STM32, make sure the STM32 is powered up and a BleuIO dongle is connected to it.

Get the MAC address

Follow the steps to get the MAC address of the dongle that is connected to STM32

  • Open this site https://bleuio.com/web_terminal.html and click connect to dongle.
  • Select the appropriate port to connect.
  • Once it says connected, type ATI. This will show dongle information and current status.
  • If the dongle is on peripheral role, set it to central by typing AT+CENTRAL
  • Now do a gap scan by typing AT+GAPSCAN
  • Once you see your dongle on the list, stop the scan by pressing control+c
  • Copy the ID and paste it into the script (script.js) line #2

Run the web script

You will need a web bundler. You can use parcel.js

Once parcel .js is installed, go to the root directory of web script and type “parcel index.html”. This will start your development environment.

Bluetooth low energy lcd message

Open the script on a browser. For this example, we opened http://localhost:1234

You can easily connect to the dongle and send your message to the LCD screen. The response will show on browser console screen.

The web script looks like this

Bluetooth low energy lcd message

Output

The message will show on the LCD screen.

Bluetooth low energy lcd message

Video of working project

 

 

 

Herst.-Teilenr. SSD005/4-V2B
BLUETOOTH 5 LOW ENERGY USB DONGL
Smart Sensor Devices
Herst.-Teilenr. NUCLEO-H743ZI2
NUCLEO-144 STM32H743ZI EVAL BRD
STMicroelectronics
Herst.-Teilenr. NHD-0420D3Z-NSW-BBW-V3
LCD MOD 80DIG 20X4 TRANSMISV WHT
Newhaven Display Intl
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.