Maker.io main logo

Projects

Blogs

BLOG
802

Aluminum Organic Polymer Capacitors

By Dave Knight

This post will detail the advantages and disadvantages of traditional electrolytic capacitors ad explain how organic polymer capacitors offer improved performance.

Tutorials See All

TUTORIAL
11.190

Introduction to Linear Voltage Regulators

By Dave Knight

Linear regulators are simple voltage regulator circuits commonly used in electronics. This paper briefly discusses how linear regulators work, their advantages and disadvantages, variations on the linear regulator, and important datasheet parameters.

TUTORIAL
648

Driving Low-Current LEDs

By Dave Knight

LEDs are used everywhere for status indicators, light sources, and more. This blog covers the basics of biasing low-current LEDs.

TUTORIAL
3.687

Introduction to Current Shunt Monitors

By Dave Knight

Current shunt monitors are a simple and easy way to measure current. This article introduces the ideas of current shunt sensing, some current shunt ICs, considerations when designing a current shunt monitor, and applications.

TUTORIAL
829

Improving Efficiency in DC-DC Converters Through Careful Component Selection

By Dave Knight

This paper discusses some loss mechanisms in DC-DC converters, and how careful component choices can optimize performance.

TUTORIAL
1.119

Constant Power Load Using PWM and ADC

By Dave Knight

This article discusses the basic ideas of pulse-width modulation (PWM) and analog-to-digital conversion (ADC), and describes a circuit and firmware using these tools to create a constant power load with closed-loop feedback.

TUTORIAL
2.230

Driving High-Current LEDs

By Dave Knight

High-power LEDs produce more lumens per watt than previous lighting technology and are replacing incandescent and CFL light bulbs.