Maker.io main logo

M5Stack Core ESP32 - Get Time and Date From the Internet

13

2026-06-03 | By Ron Cutts

License: GNU Lesser General Public License Microcontrollers Wifi Arduino ESP32

In this tutorial, we will learn how to get the date and time from the NIST time server using the M5Stack Core ESP32 and Visuino.

Watch the video!

Learn more about Visuino: What is Visuino

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

Start Visuino, and Select the M5 Stack Core Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "M5 Stack Core" as shown on Picture 2

Start Visuino, and Select the M5 Stack Core Board Type

Start Visuino, and Select the M5 Stack Core Board Type photo 2

WiFi Setup

Select M5 Stack Core, and in the editor Modules>WiFi>Access Points, click on the [...] button so that the "Access points" window will open. In this editor, drag the WiFi access point to the left side.

  • In the properties window, under "SSID" put the name of your WiFi network.

  • Under "Password" put the access password for your WiFi network

  • Close the "Access points" window

  • On the left in the editor, select Modules>Wifi>Sockets, click on the [...] button so that the "Sockets" window will open. Drag the TCP/IP Client from right to the left side, then under the Properties window, set port: 37 and host: time-c-g.nist.gov

  • Close the "Sockets" window

WiFi Setup

WiFi Setup photo 2

WiFi Setup photo 3

WiFi Setup photo 4

WiFi Setup photo 5

WiFi Setup photo 6

In Visuino, Add Components

  • Add "Pulse Generator" component

  • Add "Internet Time Protocol" component

  • Add "Delete Right Sub Text" component

  • Add "Delete Left Sub Text" component

  • Add "Split/Parse Text" component

If you want to learn more about the "Split/Parse Text" component, check out this amazing tutorial: The magic of Split Parse Text Component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Add Components photo 4

In Visuino Add Components photo 5

In Visuino Set Components

  • Select "PulseGenerator1" and in the properties window, set frequency to 0.1166667

  • Select "DeleteRightText1" and in the properties window set Length to 8

  • Select "SplitText1" and in the properties window set "Text" to: %0  %1 <<There are 2 spaces

  • Double click on the "SplitText1" and in the Elements window, drag 2X "Text Element" to the left side

  • Close the Elements window

Select M5 Stack Core and in the editor Modules>TFT Display>Elements, click on the [...] button so that the "Elements" window will open.

  • In the Elements window, drag "Text Field" to the left side and in the properties window set "Fill Color" to clBlack, "Horizontal Align" to thaCenter, "Size" to 12, "X" to 20

  • Select "Elements" and click on the 3 dots button. In the New Elements window, drag "Font" to the left side, and in the properties window, set "Font" to Adafruit\Org_01

  • Close the Elements window

  • In the Elements window, drag another "Text Field" to the left side and in the properties window set "Fill Color" to clBlack, "Horizontal Align" to thaCenter, "Size" to 5, "X" to 20, and "Y" to 100

  • Select "Elements" and click on the 3 dots button. In the New Elements window, drag "Font" to the left side, and in the properties window, set "Font" to Adafruit\Org_01

  • Close all the Elements windows

In Visuino Set Components

In Visuino Set Components photo 2

In Visuino Set Components photo 3

In Visuino Set Components photo 4

In Visuino Set Components photo 5

In Visuino Set Components photo 6

In Visuino Set Components photo 7

In Visuino Set Components photo 8

In Visuino Set Components photo 9

In Visuino Set Components photo 10

In Visuino Set Components photo 11

In Visuino Connect Components

  • Connect "PulseGenerator1" pin [Out] to "InternetTime1" pin [In]

  • Connect "InternetTime1" pin [Socket] to "M5 Stack Core" > TCP Client1 pin [In]

  • Connect "InternetTime1" pin [Out] to "DeleteRightText1" pin [In]

  • Connect "DeleteRightText1" pin [Out] to "DeleteLeftText1" pin [In]

  • Connect "DeleteLeftText1" pin [Out] to "SplitText1" pin [In]

  • Connect "SplitText1" > Text Element1 pin [Out] to "M5 Stack Core" > TFT Display > Text Field1 pin [In]

  • Connect "SplitText1" > Text Element1 pin [Out] to "M5 Stack Core" > TFT Display > Text Field1 pin [Clock]

  • Connect "SplitText1" > Text Element2 pin [Out] to "M5 Stack Core" > TFT Display > Text Field2 pin [In]

  • Connect "SplitText1" > Text Element2 pin [Out] to "M5 Stack Core" > TFT Display > Text Field2 pin [Clock]

In Visuino Connect Components

In Visuino Connect Components photo 2

Generate, Compile, and Upload the Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Code

Play

If you power the M5 Stack Core, it will connect to the internet, and the display should start showing the date and time from the NIST server.

You can also experiment with other servers that you can find here: https://tf.nist.gov/tf-cgi/servers.cgi

Congratulations! You have completed your Internet Time project with Visuino. Also attached is the Visuino project that I created for this tutorial. You can download and open it in Visuino: https://www.visuino.eu

Downloads

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.