Low-Cost, Power Efficient EMG Prosthetic Hand (Part 2)
Creating a low-cost prosthetic arm is challenging, but making one that is also easy to calibrate and accurate is even tougher.
Arduino Breakout Boards with IPS TFT Displays for Fast UI Prototyping
Arduino‑compatible TFT breakout boards from Newhaven Display simplify prototyping for user interaction with embedded displays.
Piezoelectric Ceramics: Driving the Silent Interaction Revolution
Piezoelectric ceramic technology generates an electric charge when subjected to mechanical stress and undergoes deformation when an electric field is applied.
Low-Cost, Power Efficient EMG Prosthetic Hand (Part 1)
Developing prosthetic technology that is both affordable and functional is challenging in today’s space, mainly due to the costly fabrication and specialized calibration requirements.
How to Select Flat-Panel HMIs for Optimal Results in All Industrial Environments
Publish Date: 2026-02-18
Matching the performance of human-machine interface flat-panel displays to requirements in industrial networking applications is complex.
Accelerate Small Display Integration with Plug-and-Play 3.5” IPS HDMI TFTs
Publish Date: 2026-01-15
Designers can now use plug-and-play 3.5" IPS HDMI TFT modules to simplify display integration for industrial and medical applications.
Visualization & Edge Connectivity with Schneider Electric Pro-face™ HMIs
Publish Date: 2025-12-23
How Schneider Electric’s Pro-face™ HMI portfolio supports automation requirements in packaging, material handling, assembly, and process applications.
The Role of Pulse Width Modulation in Electronics
Publish Date: 2025-12-05
A discussion of the basics of Pulse Width Modulation (PWM) as a power-control technique and some of the applications it’s used in.
How to Build a Sample Automation Project in CODESYS
Publish Date: 2025-12-03
Build an automation project in CODESYS, from initial setup to runtime testing by configuring the device tree, mapping I/O channels, programming logic, etc.
Piezoelectric Ceramics: From High-Frequency Compensation to Smart Tactile Feedback, Reshaping Audio and Interaction
An innovative application of piezoelectric ceramic earphone units effectively compensates for the shortcomings of traditional dynamic drivers.
Optimizing Industrial HMI Design with Modular 22 mm Pilot Devices
Publish Date: 2025-11-05
Explore a modular approach to 22 mm pilot devices that addresses industrial challenges with the Eaton M22 series field-configurable functionality pushbuttons.
Why Rear Enclosures Are Crucial for Miniature Speakers
Publish Date: 2025-10-30
Speakers depend not only on their internal components but also on the acoustic environment in which they operate, such as rear enclosures.
Webinar – Control Panel Solutions: Inside, Outside, and Beyond
Whether you're designing new panels or retrofitting existing ones, this webinar will help you optimize your layout, boost productivity, and ensure compliance.
Silent Tech Heart: How Piezoelectric Ceramics Drive an Intelligent Future
Using minimal current, haptic devices can be used to produce precise vibrations. Their ultra-thin profile makes them suited for space-constrained scenarios.
Save Space in Control Panels with Dual-Status LED Indicators
Publish Date: 2025-08-19
Learn how APEM Dual Icon series LED indicators use dichroic technology to save equipment panel space and provide clear visibility of system status.
Design efficient status displays using APEM dual icon LEDs. Explore the Q14 Series for smarter, versatile indicator solutions.
Breakthrough in Cost, Vibration Intensity, and Reliability!
Add haptic feedback to automotive user control by infusing digital interfaces with tactile logic to give smart cockpits a genuine "tactile language".
Nit Picking the Terms to Describe the Brightness of LEDs
While lumens measure overall light from the device, nits instead measure the intensity of light on a specific area. Valuable to know for display systems.
Behind the Robot: Sensing, Safety, and Control in Industry 4.0
Publish Date: 2025-06-19
How sensor, safety solutions and industrial control components contribute to safe motion control, adaptive system behavior, and deterministic decision-making.
Simplifying Panel Design and Safety with TeSys VLS Disconnect Switches
Publish Date: 2025-06-18
Industrial infrastructure requires disconnect switches to isolate electrical circuits safely for maintenance, emergency shutdowns, or regulatory compliance.