AS5600-POTUINO Eval Kit Manual Datasheet by ams

View All Related Products | Download PDF Datasheet
Eval Kit Manual
DN[Document ID]
ams Eval Kit Manual, Confidential
Page 1
[v1-0] 2015-Jan-21
Document Feedback
AS5600
Adapter Board
AS5600-POTUINO
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 2
[v1-0] 2015-Jan-21
Document Feedback
Table of Contents
1 Introduction .......................................................................................................................... 3
1.1 Kit Content ........................................................................................................................... 3
2 Board description ................................................................................................................. 4
3 Software ............................................................................................................................... 5
3.1 LabVIEW .............................................................................................................................. 5
3.2 Using the Arduino IDE ......................................................................................................... 7
3.2.1 Installing the Arduino library ................................................................................................. 7
3.2.2 Reading out the AS5600 sensor .......................................................................................... 8
4 AS5600-POTUINO Hardware ............................................................................................ 10
4.1 AS5600-POTUINO schematics .......................................................................................... 10
4.2 AS5600-POTUINO PCB layout .......................................................................................... 11
5 Ordering & Contact Information ......................................................................................... 12
6 Copyrights & Disclaimer ..................................................................................................... 13
Revision History
Revision
Date
Owner
Description
18.03.2015
mzie
Initial version
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 3
[v1-0] 2015-Jan-21
Document Feedback
1 Introduction
The POTUINO is a potentiometer shield compatible with the Arduino UNO board. It was designed to
evaluate the AS5600 Smart Potentiometer IC.
1.1 Kit Content
Figure 1: Kit content
Pos.
Item
Description
1
AS5600-POTUINO
Arduino shield
2
RMH05-DK
Rotary magnet holder
Note: An Arduino UNO board (not included) is required to use the POTUINO shield.
1
2
m m s n e s O 0 6 5 S A
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 4
[v1-0] 2015-Jan-21
Document Feedback
2 Board description
The POTUINO shield allows evaluation of the AS5600 position sensor. This Arduino shield is fully
assembled with the AS5600 IC and its necessary external components.
The Arduino shield includes different breakout options. A breakout magnet holder is available on the
left side of the PCB and in addition, an adapter board breakout is possible.
The headers on the bottom side of the PCB are used for mounting as well as for electrical
connection to the Arduino UNO.
Figure 2: AS5600-POTUINO shield
Breakout
magnet holder
AS5600 sensor IC
Hulk mFA_Base_A$5m}u [Z] Davin lhaflTmegam v coupon mm v 11m [E-
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 5
[v1-0] 2015-Jan-21
Document Feedback
3 Software
Custom firmware source code can be generated using the Arduino IDE. An example code and
Arduino library is available for reference. In addition, the AS5600 LabVIEW Evaluation GUI software
can be used to readout and configure the AS5600.
3.1 LabVIEW
The AS5600 LabVIEW Evaluation GUI supports the Arduino UNO. The latest version of the
software can be downloaded from the ams webpage.
Before the Arduino UNO can be used together with the POTUINO shield the LabVIEW interface
firmware has to be flashed onto the Arduino. Easiest way to do this is to download the free software
tool XLoader.
Figure 3: XLoader for flashing the Arduino UNO
Choose the LIFA_Base_AS5600.hex file which is also available for download from the ams
webpage. Then choose the Uno(ATmega328) in the Device dropdown menu. After this choose the
correct COM port which can easily be checked in the Windows Device Manager and finally click
Upload.
Hardware Sefllngs usu lax I I usw::odsz&:w16&mmm=uw ASmIZC Mrs I3: “faint? Error smu- vl
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 6
[v1-0] 2015-Jan-21
Document Feedback
After this procedure the Arduino UNO is ready for usage with the LabVIEW Evaluation GUI of the
AS5600.
If the Hardware Settings window opens, the switch has to be moved to “Arduino UNOr3”. This is
show in Figure 4: AS5600 Evaluation GUI Hardware Settings below.
A green tick indicates successful communication with the sensor. For further information about the
AS5600 LabVIEW Evaluation GUI please refer to the User Manual.
Figure 4: AS5600 Evaluation GUI Hardware Settings
skkhfinzzalhdm 1.0.5 Vuiiy/Camyil: cum: mm 3m Sketch Fuldu cum m n lmme blary... w": rnnmmvm Amymjmmy
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 7
[v1-0] 2015-Jan-21
Document Feedback
3.2 Using the Arduino IDE
3.2.1 Installing the Arduino library
The Arduino library for the AS5600 sensor can be downloaded from the ams webpage.
To add an existing library open the Arduino IDE, click Sketch in the menu bar. Then Import Library
and Add Library.
Then choose the AMS_5600_library.zip and open it.
Figure 5: Adding the AS5600 library
When including the header file to a new sketch all the functions of the library are available.
e.g.
#include <AMS_5600.h>
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 8
[v1-0] 2015-Jan-21
Document Feedback
3.2.2 Reading out the AS5600 sensor
Source code examples are also available for download on the ams webpage.
Following source code shows an easy example of reading out the sensor:
/*------------------------------------------------------
FILE: AS5600
Author: Mark A. Hoferitza, Field Application Engineer, ams AG
www.ams.com
Date: 27 May 2014
Description: Development of sketches for AS5600 "Potuino"
Read Raw Angle and Angle.
Single Value, no averaging.
-------------------------------------------------------*/
#include <Wire.h>
int AS5600_ADR = 0x36;
const int raw_ang_hi = 0x0c;
const int raw_ang_lo = 0x0d;
const int ang_hi = 0x0e;
const int ang_lo = 0x0f;
const int stat = 0x0b;
const int agc = 0x1a;
const int mag_hi = 0x1b;
const int mag_lo = 0x1c;
void setup(){
Serial.begin(9600);
Wire.begin();
}
void startup(){
}
void loop(){
// Wire.beginTransmission(AS5600_ADR);
// Wire.write(0x);
// Wire.write(0x00);
// Wire.endTransmission();
//***************************************************************
// Read Raw Angle Low Byte
Wire.beginTransmission(AS5600_ADR);
Wire.write(raw_ang_lo);
Wire.endTransmission();
Wire.requestFrom(AS5600_ADR, 1);
while(Wire.available() == 0);
int lo_raw = Wire.read();
// Read Raw Angle High Byte
Wire.beginTransmission(AS5600_ADR);
Wire.write(raw_ang_hi);
Wire.endTransmission();
Wire.requestFrom(AS5600_ADR, 1);
while(Wire.available() == 0);
word hi_raw = Wire.read();
hi_raw = hi_raw << 8; //shift raw angle hi 8 left
hi_raw = hi_raw | lo_raw; //AND high and low raw angle value
//**********************************************************
// Read Angle Low Byte
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 9
[v1-0] 2015-Jan-21
Document Feedback
Wire.beginTransmission(AS5600_ADR);
Wire.write(ang_lo);
Wire.endTransmission();
Wire.requestFrom(AS5600_ADR, 1);
while(Wire.available() == 0);
int lo_ang = Wire.read();
//Read Angle High Byte
Wire.beginTransmission(AS5600_ADR);
Wire.write(ang_hi);
Wire.endTransmission();
Wire.requestFrom(AS5600_ADR, 1);
while(Wire.available() == 0);
word hi_ang = Wire.read();
hi_ang = hi_ang << 8;
hi_ang = hi_ang | lo_ang;
//**************************************************
//Read Magnitude High Byte
Wire.beginTransmission(AS5600_ADR);
Wire.write(mag_hi);
Wire.endTransmission();
Wire.requestFrom(AS5600_ADR, 1);
while(Wire.available() == 0);
word hi_mag = Wire.read();
//Read Magnitude Low Byte
Wire.beginTransmission(AS5600_ADR);
Wire.write(mag_lo);
Wire.endTransmission();
Wire.requestFrom(AS5600_ADR, 1);
while(Wire.available() == 0);
word lo_mag = Wire.read();
hi_mag = hi_mag << 8;
hi_mag = hi_mag | lo_mag;
//**************************************************
//Read AGC
Wire.beginTransmission(AS5600_ADR);
Wire.write(agc);
Wire.endTransmission();
Wire.requestFrom(AS5600_ADR, 1);
while(Wire.available() == 0);
int agc_val = Wire.read();
//***************************************************
// Read Status Bits
Wire.beginTransmission(AS5600_ADR);
Wire.write(stat);
Wire.endTransmission();
Wire.requestFrom(AS5600_ADR, 1);
while(Wire.available() == 0);
int stat_val = Wire.read();
stat_val = stat_val & 0xa0; //Mask off all unnecessary bits
//Print Values Received
float Raw_Ang = hi_raw *0.0879;
float Ang = hi_ang * 0.0879;
Serial.print(" AS5600 Raw Angle = "); Serial.println(Raw_Ang, DEC);
Serial.print(" AS5600 Angle = "); Serial.println(Ang, DEC);
Serial.print(" AS5600 Magnitude = "); Serial.println(hi_mag, HEX);
Serial.print(" AS5600 AGC = "); Serial.println(agc_val, HEX);
Serial.print("AS5600 Status Bits = "); Serial.println(stat_val, BIN);
Serial.println();
Serial.println();
delay(2000);
}
|2CAdr9ss:0x36h U51 ‘ vDst DR J 4AD51$CL m 2 AM gogavsss: Mao flu GND PGO 1ODnF uF As5500 034 E JP1 P60 3 E E 3% 23% % ADS/SCL V ADA/SBA POWER 8x1F—H8.5 10X1F7H85 6x1F—H8 5 Aww>wm4m O‘wammw
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 10
[v1-0] 2015-Jan-21
Document Feedback
4 AS5600-POTUINO Hardware
4.1 AS5600-POTUINO schematics
Figure 6: AS5600-POTUINO schematics
f NHLI -a a1 n2 U - H3 @939
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 11
[v1-0] 2015-Jan-21
Document Feedback
4.2 AS5600-POTUINO PCB layout
Figure 7: AS5600-POTUINO PCB layout
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 12
[v1-0] 2015-Jan-21
Document Feedback
5 Ordering & Contact Information
Ordering Code
Description
AS5600-POTUINO
AS5600 Eval Kit Adapter Board
Buy our products or get free samples online at:
www.ams.com/ICdirect
Technical Support is available at:
www.ams.com/Technical-Support
Provide feedback about this document at:
www.ams.com/Document-Feedback
For further information and requests, e-mail us at:
ams_sales@ams.com
For sales offices, distributors and representatives, please visit:
www.ams.com/contact
Headquarters
ams AG
Tobelbaderstrasse 30
8141 Unterpremstaetten
Austria, Europe
Tel: +43 (0) 3136 500 0
Website: www.ams.com
AS5600 Adapter Board
ams Eval Kit Manual, Confidential
Page 13
[v1-0] 2015-Jan-21
Document Feedback
6 Copyrights & Disclaimer
Copyright ams AG, Tobelbader Strasse 30, 8141 Unterpremstaetten, Austria-Europe. Trademarks
Registered. All rights reserved. The material herein may not be reproduced, adapted, merged,
translated, stored, or used without the prior written consent of the copyright owner.
Demo Kits, Evaluation Kits and Reference Designs are provided to recipient on an “as is” basis for
demonstration and evaluation purposes only and are not considered to be finished end-products
intended and fit for general consumer use, commercial applications and applications with special
requirements such as but not limited to medical equipment or automotive applications. Demo Kits,
Evaluation Kits and Reference Designs have not been tested for compliance with electromagnetic
compatibility (EMC) standards and directives, unless otherwise specified. Demo Kits, Evaluation Kits
and Reference Designs shall be used by qualified personnel only.
ams AG reserves the right to change functionality and price of Demo Kits, Evaluation Kits and
Reference Designs at any time and without notice.
Any express or implied warranties, including, but not limited to the implied warranties of
merchantability and fitness for a particular purpose are disclaimed. Any claims and demands and any
direct, indirect, incidental, special, exemplary or consequential damages arising from the inadequacy
of the provided Demo Kits, Evaluation Kits and Reference Designs or incurred losses of any kind (e.g.
loss of use, data or profits or business interruption however caused) as a consequence of their use
are excluded.
ams AG shall not be liable to recipient or any third party for any damages, including but not limited to
personal injury, property damage, loss of profits, loss of use, interruption of business or indirect,
special, incidental or consequential damages, of any kind, in connection with or arising out of the
furnishing, performance or use of the technical data herein. No obligation or liability to recipient or
any third party shall arise or flow out of ams AG rendering of technical or other services.

Products related to this Datasheet

DEV SHIELD AS5600 POTUINO