Exploring XBees and XCTU~ Datasheet by SparkFun Electronics

View All Related Products | Download PDF Datasheet
Page 1 of 16
Exploring XBees and XCTU
Introduction
Is your project being dragged down by wires? Looking for an easy transition
to wireless communication? If you want reliable, low-cost, bi-directional
communication at moderate speeds XBee may be the solution for you!
XBees are hugely popular wireless transceivers for a number of reasons.
They’re flexible – they send and receive data over a serial port, which
means they’re compatible with both computers and microcontrollers (like
Arduino). And they’re highly configurable – you can have meshed
networks with dozens of XBees, or just a pair swapping data. You can use
them to remotely control your robot, or arrange them all over your house to
monitor temperatures or lighting conditions in every room.
Covered In This Tutorial
The pair of XBees alone won’t get you very far. In most cases you’ll want a
separate module to interface with the XBee. You can use an XBee Shield to
connect an XBee to your Arduino. Or you can use an XBee Explorer to
connect an XBee to your computer.
The focus of this tutorial is to explain how to use an XBee Explorer with an
XBee. There are a variety of Explorer boards, all designed to achieve the
same purpose: to create a communication gateway between your computer
and the XBee.
Page 1 of 1
6
Page 2 of 16
The Explorers: USB Explorer, Explorer Dongle, and Serial Explorer.
With an XBee Explorer connected between your computer and your XBee,
and with the help of the X-CTU software, you can easily configure XBees,
test connections, and pass data between your computer and remote
XBees. We’re going to show you how to do all of that in this tutorial!
Materials Required
XBees are really only useful if you have at least a pair of them. They need
buddies to talk to! Hence, there’s a lot of “2x” in this list of materials:
2x XBees – XBees exist in a variety of series, frequencies, and
ranges. If you’re just getting started with XBee, we highly
recommend going with Series 1 models – either with a trace
antenna, wire antenna or u.fl connector.
For more help picking an XBee, check out our XBee Buying
Guide.
2x Explorers – either the Explorer USB, Explorer USB Dongle, or
Explorer Serial.
These boards act as an interface between your computer and
an XBee. They’re used to configure your XBee and pass data
to and from your computer.
Depending on which explorer you have, you may also need a
matching mini-B USB or serial cables.
At least one computer with X-CTU installed.
The latest version of X-CTU is available for both Mac and
Windows!
Suggested Reading
This tutorial builds on some lower-level electronics concepts. If you’re not
familiar with the subjects below, we recommend checking out those
tutorials first.
Serial Communication – XBee’s communicate over a serial port. This
tutorial will get you familiar with terms like “RX”, “TX”, “baud rates”,
“stop bits”, and “parity”.
Serial Terminal Basics – The X-CTU software we’ll use has an
integrated serial terminal called the “console”. You can use your
preferred terminal instead; if you don’t have a preferred serial
terminal, check out this tutorial.
XBee Buying Guide – We highly recommend Series 1 XBee’s, if this
is your first time playing with them. If you’re curious about other XBee
classes, check out this guide!
Hexadecimal – XBee configuration settings – like addresses and
network ID’s – are all programmed in hex. Base 16. If you don’t know
how to make numbers with 0-9 and A-F, check out this tutorial.
Selecting an Explorer
The first step to communicating with your XBee is picking an interface
board that allows you to. XBee Explorers act as a gateway between your
computer and your XBee. There are a few to pick from, each offering their
own, key differences. Here’s a quick overview of each:
XBee Explorer USB
Page 2 of 1
6
Page 3 of 16
The XBee Explorer USB is the most popular of the Explorers. It’s equipped
with a mini-B USB connector, so you’ll need the proper USB cable to
connect it to your computer.
The highlight of this board is an FT231X USB-to-Serial converter. That’s
what translates data between your computer and the XBee. There’s also a
reset button, and a voltage regulator to supply the XBee with plenty of
power. In addition, there are four LEDs that’ll help if you ever need to debug
your XBee: RX, TX, RSSI (signal-strength indicator), and a power indicator.
This board also breaks out each of the XBee’s I/O pins to a pair of
breadboard-compatible headers. So if you want to make use of the XBee’s
extended functionality, you can solder some header pins into those, or even
just solder some wire.
XBee Explorer USB Dongle
The XBee Explorer Dongle is an extension of the Explorer. In fact, the only
real difference between this and its predecessor is the USB connector. The
Dongle can be connected directly to your laptop or PC USB port.
Or, if you need some distance from your computer, you can use a USB
extension cable.
The Dongle still shares all of the features of its sibling – reset button, LEDs,
voltage regulator, and breadboard-compatible pin breakouts.
XBee Explorer Serial
Computers with an RS-232 serial port are becoming harder and harder to
find, but if you do have one of those relics, the XBee Explorer Serial is a
viable option.
Page 3 of 1
6
Page 4 of 16
The Serial Explorer has a bigger footprint than its USB-based brethren, but
still shares most of the same features. There are RX and TX LEDs, reset
button, break-out pins, and a voltage regulator.
The Serial Explorer does require an external power supply. It’s got a barrel
jack connector which will work with either our 9V or 5V wall adapters.
If you’re using an Arduino, another option available is the XBee Shield.
That’s a subject for another tutorial.
Drivers and Assembly
The USB-based XBee Explorers all operate using an FTDI FT231X chip,
which converts serial to USB and vice-versa. This is one of our favorite
chips because it supports all computer platforms and it’s easy to work with.
If this is the first FTDI chip you’ve ever connected to your computer (it
probably won’t be your last), there is some driver installation to get out of
the way.
We’ve written a tutorial detailing How to Install FTDI Drivers tutorial. So go
ahead and plug your USB Explorer into your computer, and head on to
either the Windows, Mac, or Linux section there. (Ignore the final steps,
where Arduino software is invoked.)
Regardless of whether you’re on Mac or Windows, once your Explorer’s
drivers are installed it will be assigned a unique port number. Take note of
that port number, as you’ll need it on the next pages.
Basic Assembly: Plug In an XBee!
Time to “assemble” the XBee Explorer. Grab your XBee of choice. Notice
how it has a flat edge and a more angular/diagonal edge? Match that
footprint up to the white lines on your XBee Explorer, and carefully insert!
Take care not to bend any of the XBee pins – be gentle when you’re
plugging it in. (And be even more careful if you’re removing it!)
Page 4 of 1
6
Page 5 of 16
Nice work! You’ve assembled the XBee Explorer. You’re ready for the next
step. Or, if you’re a power user, looking to get the most out of your explorer,
you can check out the more “advanced” assembly below.
Advanced Assembly (Totally Optional)
For most basic-use cases, all Explorer boards should be good-to-go once
you’ve installed drivers. If you want to use any of the XBee’s I/O pins, you
can solder male headers to the 0.1"-pitch pins inside the XBee headers.
This will allow you to plug the board into a breadboard, so you can wire
other components up to the XBee.
The XBee Explorer can be used with a USB cable and breadboard
concurrently – just solder some headers into the breakout pins. (Actually
solder them, don’t pretend like we did in the image above.)
Each XBee pin is labelled on the bottom side of the board. You can also
check out the schematic for help locating a specific pin.
If male headers don’t fit your purpose, you can alternatively solder in female
headers (to plug jumper wires into), or even just bare wire. Just make sure
you don’t solder anything into the top side of the board – or you may be
unable to plug the XBee in!
We won’t cover it in this tutorial, but those “DIO#” pins can be configured as
either inputs or outputs. That means you can use an XBee to directly drive
LEDs or motors, and read analog sensors or buttons.
Starting With X-CTU
X-CTU is free software, provided by Digi (the manufacturer of XBee), which
we use to configure and manage XBees, and test XBee networks.
If you haven’t already, head over to their website and download the latest
release and follow their instructions to install the software.
Adding XBee’s
Before continuing on, make sure you’ve plugged an XBee (correctly) into
your Explorer, and have the Explorer plugged into your computer. When
you installed the drivers for your Explorer it should have been assigned port
number. You’ll need that shortly.
After initially opening X-CTU, you’ll be presented with a window like this:
Page 5 of 1
6
E X mus...“ NMMMWWMWD + mum-«tn ' whm... mm. (WWW mm mm mm m :l w _ w :l n-«_ lmmm—w ENE} Page 6 of 16
To add your XBee(s), click the “Add device” icon – in the
upper-left part of the window. That will prompt this screen to show up:
Select your communication port. If you’re lucky (or just don’t have a lot of
stuff connected to your computer) you may only have one option here.
Otherwise Windows users should look for the entry that says “USB Serial
Port” and Mac users should look for something like “usbserial-XXXXXXXX”.
(If you’re using a USB board, that is. If you’re using a Serial Explorer, pick
the “Communications Port” option.)
This window also allows you to specify more specific serial characteristics
like baud rate, data bits, and stop bits. Assuming this is the first time you’ve
used your XBee, you can leave those settings alone. So make sure those
values look just as they do in the image above and click Finish.
A “Discovering radio modules…” window will briefly scroll by, after which
you should be presented with the original window, but with an addition to
the “Radio Modules” section on the left. (If X-CTU failed to find a module,
check out our troubleshooting page.)
Click that new module, and wait a few seconds as X-CTU reads the
configuration settings of your XBee. You should then be presented with the
entire configuration of your XBee.
Page 6 of 1
6
Page 7 of 16
As you can see by scrolling down the right half, there are a lot of
configuration settings available. We’ll get to some of those later. For now,
though, verify that the configurable settings visible in the screenshot above
match those of your XBee (channel=C, PAN ID=3332, DH=0, DL=0, MY=0).
Do It Again
To test communication between your XBee’s you’ll need to connect your
second XBee to a computer as well. That means doing the “Add device”
dance one more time.
If you have another computer available, you can install X-CTU on that as
well and perform the same set up. You can certainly perform this test with
both XBees connected to the same computer as well, just make sure you
select the correct port number when you’re adding the second XBee.
If you add a second XBee to the same computer, a second entry will be
added to the “Radio Modules” list. Selecting either of those entries will show
the configuration settings for that, specific XBee.
Note that there are two XBees in the list on the left. The configuration
values shown are for the highlighted XBee.
If you’re ever unsure which XBee is which, try to match up the MAC
numbers. These numbers are printed on a sticker on the bottom side of
your XBee, and they’re also listed in XCTU. (It’s listed as the “Serial
Number” high and low, and is un-modifiable.)
Page 7 of 1
6
me: 1.1M I‘JIGQ v A38 ze—zassem .' XBQA-wa. um r-vE amen-DB w Page 8 of 16
Each XBee has a unique MAC address, printed on a sticker in the
highlighted area.
As with the last module, make sure all settings are defaulted (channel=C,
PAN ID=3332, DH=0, DL=0, MY=0). That’ll make the next step possible.
Quick and Easy Test
Click the “Switch to Consoles” icon – in the upper-right part of
the window. This will switch from the configuration tab to the console. We
can use the console to send characters to an XBee, which will route that
character over-the-air to any other XBee it’s connected to.
If you have two XBees connected to your computer, you can switch
between each radio’s console by selecting the device on the left.
First, open a serial connection on each device by clicking the connect
icon – . The icon will change, and the border of the console will turn
green.
Next, click into the left half of the console, and type a letter or number.
You should notice that character echoed in a blue font (the hexadecimal
digits on the right represent the ASCII value). Now click into the other
XBee’s console. As long as it was open, you should see that same
character, but red. Try typing a different character into the second XBee’s
console, and you should see it work the other way.
Page 8 of 1
6
Page 9 of 16
If that worked, then your XBees are configured to talk to each other! If not,
check out the troubleshooting page.
That your XBees can talk to each other out of the box is no real surprise.
They’re all configured to, by default, be on the same network with the same
addresses. That might be OK, but what if your neighbor is running an
XBee-based robot control network, while you’re trying to automate your
house? Every time they try to roll a bot forward, your garage door might
open! To be safe, you should configure your XBees to operate on a unique
network. Fortunately, that, and most other XBee settings are easy to
change. On to the next page!
Configuring Networks
As we’ve mentioned, XBees are awesome because they’re highly – and
easily – configurable. Most of the XBee configuration settings come down
to controlling which other XBees it can talk to. On this page, we’ll show you
how to configure three of the most important XBee settings there are: PAN
ID, MY address, and destination address.
There are a few levels to XBee networks. First, there’s the channel. This
controls the frequency band that your XBee communicates over. Most
XBee’s operate on the 2.4GHz 802.15.4 band, and the channel further
calibrates the operating frequency within that band. You can usually leave
the channel setting alone, or at least make sure every XBee you want to
have on the same network operates on the same channel.
The next level of an XBee network is the personal area network ID (PAN
ID). The network ID is some hexadecimal value between 0 and 0xFFFF.
XBees can only communicate with each other if they have the same
network ID. There being 65536 possible ID’s, there’s a very small chance
that your neighbor will be operating on the same network (as long as you
change it from the default!).
Finally there are MY and destination addresses. Each XBee in a network
should be assigned a 16-bit address (again between 0 and 0xFFFF), which
is referred to as MY address, or the “source” address. Another setting, the
destination address, determines which source address an XBee can send
data to. For one XBee to be able to send data to another, it must have the
same destination address as the other XBee’s source.
For example, if XBee 1 has a MY address of 0x1234, and XBee 2 has an
equivalent destination address of 0x1234, then XBee 2 can send data to
XBee 1. But if XBee 2 has a MY address of 0x5201, and XBee 1 has a
Page 9 of 1
6
Page 10 of 16 ChannelC
destination address of 0x5200, then XBee 1 cannot send data to XBee 2. In
this case, only one-way communication is enabled between the two XBee’s
(only XBee 2 can send data to XBee 1).
We can use X-CTU to easily configure each of those settings. Here’s how:
Radio Configuration
After the last page, you should already have at least one XBee connected
to X-CTU. If you’re still over in the console tab, click back over to the
Configuration tab . Take a peak at the very first handful of
settings, and you should see some familiar acronyms: CH, ID, DH, DL, and
MY. Beside each of those blocks is a text box – that’s where we’ll type in
our new settings.
Network ID (ID)
Begin by coming up with a unique network ID number. Think of your
favorite number between 0 and 65535, consult your friends and neighbors
to make sure your favorite isn’t their favorite, then convert it to hexadecimal.
Or if you don’t want to put that much effort into it, use a random value like
894B.
Type your 16-bit network ID into the white text box next to PAN ID.
MY Address (MY)
Your next job is to create addresses for each XBee in your network. These
values should be unique to each XBee in a network. The MY address can
be any value between 0x0000 and 0xFFFF. Type this address into the text
box next to “MY 16-bit Source Address”.
If you only have two XBees, you can assign the first an MY address of 0,
and the other an address of 1.
(Your XBee’s can share the same MY address, they’ll both receive the
same data if it’s broadcasted to that address.)
Destination Address (DH & DL)
The destination address defines which XBee your source XBee is talking to.
There are actually two values used to set the destination: destination high
(DH) and destination low (DL). You can use that pair of values in one of two
ways to set your XBee’s mate:
1. Leave DH set to 0, and set DL to the MY address of the receiving
XBee.
2. Set DH to the Serial Number High (SH) and DL to the Serial
Number Low (SL) of your destination XBee.
Either method works, but the former – setting DH to 0 and DL to the
destination’s MY address – is usually easier.
Page 10 of 1
6
Page 11 of 16
Here’s an example for setting up the ID, DH, DL, and MY values for a pair
of XBees:
Setting AcronymXBee 1XBee 2
Channel CH CC
PAN ID ID 894B 894B
Destination Address HighDH 00
Destination Address Low DL 10
16-bit Source Address MY 01
Notice how the only real differences are the DL and MY values, which are
flip-flopped on each XBee.
Write Changes
Once you’ve made your changes to the text field, click the brown pencil
icon ( ) to write your changes. The property background should turn
from green to blue, indicating it has been written to a non-default value.
XBee 1’s config tab after writing the changes.
Now, just like last time, you can try to send data from one XBee to the other
via the console. As long as the addresses and PAN ID’s match up, you
should have the same success as last time.
While it may seem like a lot of work to get right back to where you were,
using a unique PAN ID and addressing scheme will make your data transfer
more secure and reliable.
Troubleshooting
If your XBee’s are giving you any trouble, here are some common problems
and fixes we recommend:
Can’t Find Device – If XCTU can’t find your XBee, we recommend
recovery or discovery.
XBees Not Communicating Wirelessly – If a pair of XBees are failing
to communicate, we recommend resetting everything to default.
Resetting XBees – A trick to resetting your XBee (if you don’t have a
reset button).
Can’t Find Device
Are you having a hard time “finding” an XBee? If you’re “Add Device”
process is being followed by a window like this:
Page 11 of 1
6
Page 12 of 16 com mm: a», m "WM: Wm” WM“: mmmvmmw nm¢mnmwmmm mm»; mm m. mm mm mm saw-s mum“. am. K mnnxmmd m...“- m mwmmm w. my .m sham; ml- Mudfl- vmm ma mu”, ,m. Mummm Mm". mmmw am mflw. in mm. mamnmum Mummy-7mm“ mm»: m MM“ muymwumpwmmu (mum. mm. "as. Mk 8 mmmmmmmqummcmm M my". unmkmwm. Ham-w _E @ fl' (unflgwuhrkruwil Wu wnmmmmv mm mm . n... mm: m, 7 m . r 1 n m 7 5m 7 . r m 7 115m: r M v mm: ‘ m 1 mm L 5.x. 2 m Wu: MW 7 x 7 NM \ 5‘... z EwT EE
There are two options we recommend: discovery or recovery.
Discovery
The Discover radio devices tool is an extension of “Add devices”. Open
the discovery window by clicking the XBee/magnifying glass icon –
– in the top-left.
Once again you’ll be prompted to select which communication port your
XBee is connected to. Double check that you’ve selected the correct one
(or even try multiple). The next window will present you with every, single
serial setting available, and a whole lot of checkboxes:
Most of the cases where your XBee is hiding it’s because the baud rate
has been altered. A quick fix for this is to select all possible baud rates in
the discovery window, then click Finish. The discovery process works a lot
like the add process except it tests out every selection you make in this
window – that means it will take a little longer to finish.
Hopefully you’ve found an XBee that was just configured to talk at a weird
baud rate. If not you can select any of the other checkboxes as well, but it’ll
make for a longer and longer discovery process. Click every checkbox and
you might be waiting upwards of an hour for your XBee to be discovered
(permutations!).
If you’re not having any luck with discovery, the next step is recovery.
Page 1
2
of 1
6
Page 13 0f16 Rhian- mmmmmmmmmm Sidnwlmtamvwmm mmwm mum“...
Recover
y
If your XBee seems bricked, don’t worry! You can most likely recover it. To
get to the recovery screen, click the Tools icon, and select XBee
Recovery.
Once again, you’ll need to select your COM port, and you’ll also need to
select the product family. This can be found on the bottom sticker of your
XBee. If you’re using a series 1 module, the family should be XB24.
Beyond that you’ll need to select a “Function Set” and “Firmware Version”.
For both of those you should be safe selecting the top-most values in the
list.
Once you’ve made all of those selections, click Recover.
The recovery process may take a few minutes. You’ll be prompted to reset
your XBee. If your Explorer has a reset button, simply press it when
prompted, otherwise see the “Reset” section below.
During recovery, if XCTU can find your XBee it will. It’ll also update the
firmware, and set you back to the default settings. If you know what got
your XBee bricked in the first place…maybe don’t do that again.
XBee’s Not Communicating, Reset to Defaults
If no matter what changes you make to the config settings your XBee’s just
won’t communicate with each other, try resetting them both to the default
values.
In the config tab, click the “Load default firmware settings” icon –
(not sure how to describe that icon). Then click Yes to confirm that you
want to reset everything.
If you’re presented with any red-backgrounded error notifications (like
below), first try to refresh the value, by clicking the green icon – .
Page 1
3
of 1
6
Page 14 of 16 /\ ,I/ Kuhn-quid . o. - :- ACTION REQUIRED Reset your radio module. 1: me dialog is not clased wimin 10 seconds, click cancel.
If that doesn’t fix the error, you can probably get away with typing a “0” in
that box (usually this pops up for properties like encryption keys or other
values meant to be kept secret).
After you’ve loaded the default values, you still need to write the settings
by clicking the big pencil icon above – .
After defaulting both radios, the addresses, networks, and other settings
should all be compatible. Try communicating over the console again.
Resetting Old (Pre-Reset Button) Explorers
When it’s having trouble communicating with an XBee, XCTU may present
you with a notification like this:
The USB explorers were revised in May 2014 to include a reset button, so
resetting should be easily done on those newer boards. However, if you’re
using an older Explorer you’ll have to use the “jumper method”. Grab a
piece of jumper wire and, when prompted with the “Action Required”
window, briefly connect the RST pin to GND.
Page 1
4
of 1
6
Page 15 0f16 . as an 0. O as 65 O O mun m m5 0 0 «SE C mas o O .3. H Sun, 2 m as n o :2 m “50 O 1:. a 35 o o 55 was 0 0 )3 SE 0 0 ea . was a
Short them together for about a second, and then remove the wire. If you’ve
done it within the time window provided by XCTU, it should proceed to the
next step. If not give it another try…it takes some practice.
Resources & Going Further
That should be enough to get you started. If you’re looking for more XBee
and XBee Shield info, check out these resources:
XBee Explorer Schematic – If you’re confused about how parts are
interconnected on the breakout, check out this PDF.
XBee Explorer GitHub Repo – This is where you’ll find the latest and
greatest PCB design files.
XBee Series 1 Manual – For more advanced users, if you really want
to take advantage of the XBee’s unique abilities, check out this
guide.
XBee Wireless Class Materials – Check out our teaching materials
for the XBee class we lead every once-in-a-while.
Going Further
With XBee and the XBee Explorer you have most of the tools you’ll need to
take your project to the airwaves. If you’re looking to add Arduino to the
mix, we recommend using an XBee Shield and following along with our
XBee Shield Hookup Guide.
What are you going to make? Need some inspiration? Check out these
related tutorials:
XBee WiFi Hookup Guide – Take the next step with XBees, using the
XBee WiFi. These modules allow you to connect to a wireless
network and give your Arduino Internet access!
Simon Splosion Wireless – This tutorial demonstrates one of many
techniques to “hack” the Simon Says – use XBee’s to make the
Simon game wireless!
Page 1
5
of 1
6
Page 16 of16 https://lcam.sparkfun.com/tutorials/cxploring-xbccs—and-xctu?7ga=1.266449614.19394569... 6/24/2015
Getting Started With the RedBot – The RedBot is our popular,
Arduino-based robot platform. Once you get it rolling, you can take it
a step further by controlling it with an XBee!
Page 1
6
of 1
6
6
/
24
/
201
5
htt
s://learn.s
arkfun.com/tutorials/ex
lorin
-xbees-an
d
-xctu?
_g
a=1.266449614.1939456
9
...

Products related to this Datasheet

SPARKFUN XBEE EXPLORER USB
XBEE EXPLORER DONGLE