Q+products
Ferrite Beads
Axial EMI Suppression Ferrites
SMD Power Inductors
Q
+
products
Ferrite Beads
Axial EMI Suppression Ferrites
SMD Power Inductors

www.we-online.com207/14Würth Elektronik eiSos®
Q+products have given rise to plenty of discussions since their launch.
The most frequently asked questions: What advantage do these products give us?
To whom may I sell them? And for which applications are they suitable?
Q+products
Benefits
1Optimized
construction
4High process
capability level
Internal structures of the products in the Q+products portfolio are
very different from conventional ones. For example, the wire connec-
tion between coil wire and component is not made with a conven-
tional solder joint, but by means of a welding process. Another exam-
ple is ferrite sleeves; compared with the conventional industry
article, the surface form is optimized and this considerably simplifies
the routing of lines.
Process capability is determined by means of familiar statistics and
describes the stability of a manufacturing process. A statistical eval-
uation by itself will not make a manufacturing process more stable,
however. This also depends on the added values of other Q+prod-
ucts.
3
Automation vs. partial automation / manual process
Increasing the degree of automation in the manufacturing process
changes the variance of process parameters positively by eliminat-
ing the influence of the operator. This also ensures even more effec-
tive process controlling.
Higher level
of automation
2AEC-Q 200
qualification
All Q+products are qualified in accordance with the AEC-Q 200. The
Automotive Electronics Council Qualification (AECQ) does not reflect
the qualification standard of the automotive industry in all cases, but
describes product quality very precisely only by means of a variety of
reliability checks.

www.we-online.com 307/14 Würth Elektronik eiSos®
Q+products
Benefi ts
6Production on
strictly defined
production lines
Additional quality controls can be carried out efficiently only if they
are used for previously evaluated production lines. Even two identical
manufacturing processes can have different results. So pro-
cess-based influences are difficult to generalize, which is why we
specially select and monitor the production lines.
5
Additional quality controls are geared specifically to the familiar, crit-
ical quality features of the individual Q+products. These features are
directly monitored, documented and qualified according to their re-
quirements in the appropriate manufacturing step.
Additional
quality controls
7
The market requires tough products. So we have already extended
the temperature range of Q+products ferrite sleeves to -55 °C /
+150 °C. We also aim to extend such increases in temperature range
to include all Q+products.
Extended
temperature
range
Temperature range up to +150 °C

www.we-online.com4 07/14Würth Elektronik eiSos®
Q+products
Qualifi cation Standard
The qualification standard refers to the AEC-Q 200 and is performed for all products which are shown in this catalogue. For your reference, you can
find in the following table a short summary of the performed tests for inductors / transformers.
High Temperature Exposure
Storage for 1000 hours to at rated operating temperature (according
to the datasheet)
Temperature Cycling
1000 cycles at operating temperature (according to the datasheet,
e.g. -40 °C / +125 °C). with an maximum dwell time of one minute.
Biased Humidity
1000 hours at 85 °C and 85 % RH without electrical stress
Operational Life
1000 hours at operating temperature minus self-heating tempera-
ture under electrical stress (rated current)
External Visual
Inspection of the device looking / construction, workmanship and
marking.
Physical Dimension
The mechanical dimension have to be in between the specification
Terminal Strength (SMD)
The parts will be stressed with a pull of force of 17.7 Newton for
60 seconds. The focus is on the soldering joint.
Resistance to Solvents
Three different kinds of solvent do not have any impact to the device
construction, marking and looking.
Mechanical Shock
Mechanical shocks shall not have any impact to the device construc-
tion or function. These shocks will be simulated 18 times, by a am-
plitude of 100 g’s for 6 milliseconds.
Vibration
Vibrations of 10 g’s in a frequency range from 15 up to 2000 Hz for
20 minutes shall not have any impact to the construction of the
device. This process will be done in 12 cycles for each of the Axis.
Resistance to Soldering Heat
A Reflow Oven Test for five times shall not have any impact to the
device
ESD
An Electrostatic discharge of 6 kV with direct contact, 12 kV, 16 kV
and 25 kV with air contact shall not have any impact to the device.
Solderability
Three different Soldering procedures will be gone through. In each
case an impact to the device and construction isn’t allowed.
Electrical Characterization
Parametrically test which shows in a summary the min, max, man
and standard deviation at room temperature as well as at min and
max operating temperature.
Board Flex
At surface mounted devices, an impact due to bending, flexing and
pulling forces shall be not be given.

www.we-online.com 507/14 Würth Elektronik eiSos®
Q+products
Standards by Comparison
Although it might seem much better at the first sight, it doesn’t mean, that the industrial parts are less qualified than the Q+ Products. The
difference in here is the higher reliable requirements which we going to prove accordance to the AEC-Q 200. To show the difference, the
following table contrasts some main parts out of the industrial qualification standard of Würth Elektronik eiSos with the main necessary
qualification standards out of the AEC-Q 200.
Test description Industrial Standard Q+products Standard
High Temperature Exposure 500 hours 1000 hours
Temperature Cycling 500 cycles 1000 cycles
Biased Humidity – 1000 hours
Moisture Resistance 500 hours –
Operational Life 1000 hours 1000 hours
External Visual
Physical Dimension –
Terminal strength
Resistance to solvent – 3 different Solvents
Mechanical Shock –
Vibration
Resistance to Soldering Heat 5 time Reflow 5 time Reflow
ESD –
Solderability
Electrical Characterization –
Board Flex
Low Temperature Exposure –
Legend to the table:
both of the tests are the same
– not tested
Production Site
Quality & Design Center
Waldenburg (Germany)
Waldenburg (Germany)
Taichung (Taiwan)
Shenyang (China)
Shenyang (China)
Longgang (China) Seoul (Korea)

www.we-online.com6 07/14Würth Elektronik eiSos®
Characteristics
Reliable Ni-Sn electrodes
High rated current up to 5 A
Recommended soldering: Reflow
Operating temperature: -55 °C to +125 °C
WE-CBA
SMD EMI Suppression Ferrite Bead
Size 0402
Applications
Perfect as data lined filter and for uncoupling
of distribution voltage
Dimensions (in mm)
0,25 ±0,1
0,5 ±0,05
0,5 ±0,05
1,0 ±0,05
Land pattern (in mm)
0,5
W
0,6
WIDE BAND: W = 1,5
HIGH CURRENT: W = 2,2
Type definition of SMD ferrites WE-CBA
The special SMD chip bead ferrites can be put directly on the printed circuit board. They offer excellent anti-EMI properties and low
DC-resistance. Placed very close next to the interference source even with smallest size 0402, maximal impedance at 1000 Ω can
be reached.
High Speed:
“High Speed” SMD ferrites WE-CBA have lower impedance in the lower frequency ranges thus they have only a low attenuation
for fast signals.
Application e.g. USB 2.0, IEEE 1394, LVDS
Wide Band:
“Wide Band” SMD ferrites WE-CBA already show high impedance in low frequency range. Therefore they are wide band through
the whole spectrum.
Application e.g. control signals, RS232, RS422, DC/DC converter
High Current:
“High Current” SMD ferrites WE-CBA are designed for high current (over 1 A). The rated current refers to 40 K self-heating.
High current SMD ferrites are available in all three types (High Speed, Wide Band and High Frequency).
Application e.g. power supply, DC/DC converter
Advice: Pay attention for the use of SMD ferrites for high rated current >1 A and ambient temperature over +85 °C that the rated
current has to be reduced when temperature is above +85 °C (Derating).
The characteristic line in the right figure shows, that e.g. at +100 °C ambient temperature the maximal rated current has to add
up to only 60 % of the data sheet value, without an overload of the component.
Derating +85 °C
Derating +105 °C
Electrical properties
Order Code Z @ 100 MHz
(Ω)
Zmax
(Ω)
Testcondition Zmax
(MHz)
IR
(mA)
RDC
(Ω)
Type of
Application
782 422 101 100 180 500 500 0.30 Wide Band
782 422 221 220 330 400 400 0.30 Wide Band
782 422 331 330 640 300 300 0.50 Wide Band
782 422 511 510 730 300 200 0.80 Wide Band
782 422 601 600 800 300 200 0.80 Wide Band
782 422 102 1000 1200 170 200 1.00 Wide Band
782 423 100 10 17 700 1500 0.03 High Current
782 423 700 70 140 600 1000 0.09 High Current

www.we-online.com 707/14 Würth Elektronik eiSos®
WE-CBA
SMD EMI Suppression Ferrite Bead
Size 0402
782 422 101
1
10
100
1000
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 422 102
1
10
100
1000
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
10000
782 422 221
1
10
100
1000
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 422 331
1
10
100
1000
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 422 511
1
10
100
1000
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 422 601
1
10
100
1000
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 423 100
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 423 700
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
Typical impedance characteristics
Wide Band
High Current

www.we-online.com807/14Würth Elektronik eiSos®
WE-CBA
SMD EMI Suppression Ferrite Bead
Size 0603
Dimensions (in mm)
0,8±0,2
0,8±0,2
0,3±0,2
1,6±0,2
782 631 101
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 631 182
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
10000
782 631 331
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
Typical impedance characteristics
High Speed
Electrical properties
Order Code Z @ 100 MHz
(Ω)
Zmax
(Ω)
Testcondition Zmax
(MHz)
IR
(mA)
RDC
(Ω)
Type of
Application
782 631 101 100 610 400 500 0.20 High Speed
782 631 331 330 690 280 400 0.25 High Speed
782 631 182 1800 2300 130 100 0.75 High Speed
782 632 620 62 95 500 500 0.15 Wide Band
782 632 121 120 190 450 500 0.20 Wide Band
782 632 181 180 280 380 500 0.20 Wide Band
782 632 511 510 610 200 300 0.35 Wide Band
782 632 102 1000 1100 150 200 0.50 Wide Band
782 633 620 62 98 600 2500 0.04 High Current
782 633 601 600 660 190 1000 0.20 High Current
Land pattern (in mm)
0,8±0,2
0,8±0,2
0,3±0,2
1,6±0,2
0,8±0,2
0,8±0,2
0,3±0,2
1,6±0,2
0,7
0,7
W
WIDE BAND / HIGH SPEED: W = 2,2
HIGH CURRENT: W = 2,6

www.we-online.com 907/14 Würth Elektronik eiSos®
WE-CBA
SMD EMI Suppression Ferrite Bead
Size 0603
782 632 102
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
10000
782 632 121
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 632 181
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 632 511
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 632 620
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 633 601
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 633 620
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
Typical impedance characteristics
Wide Band
High Current

www.we-online.com10 07/14Würth Elektronik eiSos®
WE-CBA
SMD EMI Suppression Ferrite Bead
Size 0805
0,9 ±0,2
1,2 ±0,2
0,5 ±0,3
2,0 ±0,2
Land pattern (in mm)
Dimensions (in mm)
782 851 102
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
10000
782 851 202
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
10000
Typical impedance characteristics
High Speed
Electrical properties
Order Code Z @ 100 MHz
(Ω)
Zmax
(Ω)
Testcondition Zmax
(MHz)
IR
(mA)
RDC
(Ω)
Type of
Application
782 851 102 1000 1100 150 300 0.350 High Speed
782 851 202 2200 2200 100 200 0.450 High Speed
782 853 200 20 35 700 5000 0.008 High Current
782 853 270 27 45 700 4000 0.015 High Current
782 853 680 68 110 500 3000 0.025 High Current
782 853 910 91 105 400 2000 0.060 High Current
782 853 121 120 180 300 2500 0.035 High Current
782 853 221 220 290 200 2000 0.050 High Current
782 853 561 560 600 160 1500 0.100 High Current
782 853 112 1100 1400 70 800 0.300 High Current
782 853 152 1500 1800 70 700 0.350 High Current
0,9 ±0,2
1,2 ±0,2
0,5 ±0,3
2,0 ±0,2
0,9 ±0,2
1,2 ±0,2
0,5 ±0,3
2,0 ±0,2
1,0
1,2
W
HIGH SPEED: W = 3,0
HIGH CURRENT: W = 4,0

www.we-online.com 1107/14 Würth Elektronik eiSos®
WE-CBA
SMD EMI Suppression Ferrite Bead
Size 0805
782 853 112
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
10000
782 853 121
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 853 152
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
10000
782 853 200
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 853 221
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 853 270
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 853 561
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 853 680
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
782 853 910
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
Typical impedance characteristics
High Current

www.we-online.com12 07/14Würth Elektronik eiSos®
WE-CBA
SMD EMI Suppression Ferrite Bead
Size 1206
1,1 ±0,2
1,6 ±0,2
3,2 ±0,2
0,5 ±0,3
782 762 301
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 763 102
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 763 621
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 763 820
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
Land pattern (in mm)
Dimensions (in mm)
Typical impedance characteristics
Wide Band
High Current
Electrical properties
Order Code Z @ 100 MHz
(Ω)
Zmax
(Ω)
Testcondition Zmax
(MHz)
IR
(mA)
RDC
(Ω)
Type of
Application
782 762 301 300 360 160 500 0.100 Wide Band
782 763 820 82 130 500 3000 0.025 High Current
782 763 621 620 620 100 1500 0.100 High Current
782 763 102 1000 1200 80 1000 0.300 High Current
1,1 ±0,2
1,6 ±0,2
3,2 ±0,2
0,5 ±0,3
1,1 ±0,2
1,6 ±0,2
3,2 ±0,2
0,5 ±0,3
WIDE BAND: W = 4,2
HIGH CURRENT: W = 5,2
2,0
W
1,2

www.we-online.com 1307/14 Würth Elektronik eiSos®
WE-CBA
SMD EMI Suppression Ferrite Bead
Size 1806
1,6 ±0,2
1,6 ±0,2
4,5 ±0,2
0,5 ±0,3
Land pattern (in mm)
Dimensions (in mm)
782 963 560
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
782 963 820
1
10
100
1 10 1001000
Frequency [MHz]
XL
Impedance [Ω]
RZ
1000
Typical impedance characteristics
High Current
Electrical properties
Order Code Z @ 100 MHz
(Ω)
Zmax
(Ω)
Testcondition Zmax
(MHz)
IR
(mA)
RDC
(Ω)
Type of
Application
782 963 560 56 90 1000 5000 0.008 High Current
782 963 820 82 110 1000 3500 0.020 High Current
1,6 ±0,2
1,6 ±0,2
4,5 ±0,2
0,5 ±0,3
1,6 ±0,2
1,6 ±0,2
4,5 ±0,2
0,5 ±0,3
HIGH CURRENT: W = 6,5
1,2
3,0
W

www.we-online.com14 07/14Würth Elektronik eiSos®
WE-AEFA
Axial EMI Suppression Ferrite
Characteristics
Ferrite core made of NiZn, a material which works
in a wide frequency range
Many different types for the best possible
interference suppression
Operating temperature: -55 °C up to +150 °C
Applications
In general for: wires, coaxial cables, wire-wrapping
cables, multiconductor wires
Data and signal lines
On board power supply line
Multimedia cable interfaces
Various, other cable interfaces
Dimensions (in mm)
Cable diameter
HOD
ID
Electrical properties
Order Code OD
(mm)
ID
(mm)
H
(mm)
Cable Diameter
(mm)
Z @ 25 MHz
1 turn (Ω)
Z @ 100 MHz
1 turn (Ω)
782 013 033 150 12.0 3.55 15.0 ≤ 3.3 150 205
782 013 044 095 9.5 4.75 9.5 ≤ 4.4 60 84
782 013 046 185 11.5 5.0 18.5 ≤ 4.6 135 186
782 013 046 250 11.5 5.0 25.0 ≤ 4.6 185 255
782 013 057 450 12.0 6.1 45.0 ≤ 5.7 255 370
782 013 059 285 14.0 6.3 28.5 ≤ 5.9 195 270
782 013 068 250 14.0 7.2 25.0 ≤ 6.8 150 210
782 013 069 155 12.0 7.3 15.5 ≤ 6.9 70 100
782 013 069 285 15.5 7.3 28.5 ≤ 6.9 190 270
782 013 076 285 16.0 8.0 28.5 ≤ 7.6 170 240
782 013 076 508 16.0 8.0 50.8 ≤ 7.6 325 460
782 013 079 285 14.0 8.2 28.5 ≤ 7.9 140 200
782 013 086 280 16.0 9.0 28.0 ≤ 8.6 140 205
782 013 091 285 17.5 9.5 28.5 ≤ 9.1 150 220
782 013 100 280 15.5 10.5 28.0 ≤ 10.0 100 150
782 013 110 508 19.0 11.5 50.8 ≤ 11.0 235 345
782 013 125 280 19.0 13.0 28.0 ≤ 12.5 95 150
782 013 125 285 26.0 13.0 28.5 ≤ 12.5 170 240
782 013 150 285 26.0 15.5 28.5 ≤ 15.0 130 190
Temperature range
up to +150 °C
interference suppression
Temperature range
up to +150 °C

www.we-online.com 1507/14 Würth Elektronik eiSos®
WE-AEFA
Axial EMI Suppression Ferrite
Typical impedance characteristics
782 013 044 095
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 046 185
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 059 285
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 069 285
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 033 150
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 046 250
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 069 155
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 076 285
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 057 450
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 076 508
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 079 285
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 068 250
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn

www.we-online.com16 07/14Würth Elektronik eiSos®
Typical impedance characteristics
782 013 150 285
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 110 508
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 125 280
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 125 285
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 100 280
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
WE-AEFA
Axial EMI Suppression Ferrite
782 013 091 285
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn
782 013 086 280
1
10
100
1000
1 10 1001000
Impedance [Ω]
Frequency [MHz]
1 Turn

www.we-online.com 1707/14 Würth Elektronik eiSos®
WE-PDA
SMD Shielded Power Inductor
Size 7332
Characteristics
Wire connection: welding technology
Operating Temperature -40 °C up to +125 °C
Highes possible current loading for SMD Inductors
Magnetically shielded version which results in a
low leakage field
High storage capacity
Low self-losses
Core Material: NiZn
Applications
Multimedia applications
Switching regulators with low operating voltages
(Computer, Notebook, smart phones)
Integrated DC/DC-converter
Perfect suitable for switching regulators with
extremely high efficiency (> 86 %)
Dimensions (in mm)
Electrical properties
Order Code L
(μH)
Tolerance
(%)
RDC
(mΩ) max.
IR
(A)
ISat
(A)
784 778 010 1.0 20 % 36 5.37 6.40
784 778 022 2.2 20 % 50 4.00 4.80
784 778 033 3.3 20 % 65 3.42 4.20
784 778 047 4.7 20 % 79 2.90 3.90
784 778 068 6.8 20 % 95 2.50 2.75
784 778 082 8.2 20 % 103 2.2 2.4
784 778 100 10 20 % 126 1.83 2.20
784 778 220 22 20 % 190 1.40 1.40
784 778 470 47 20 % 350 1.10 1.00
784 778 101 100 20 % 720 0.75 0.67
784 778 221 220 20 % 1620 0.54 0.42
784 778 471 470 20 % 3300 0.32 0.31
784 778 102 1000 20 % 7200 0.20 0.18
Land pattern (in mm)
4,0
8,0
1,7
2,0
no vias and traces in restricted area
Solder Resist
Inductance vs. Current
3,2 ± 0,3
4,0 ± 0,3
1,5 ± 0,3
7,3 ± 0,3
7,3 ± 0,3
0,1
1
10
100
1000
0111,0
78477801
0
78477810
0
78477810
1
78477810
2
Rated current [A]
Inductance [µH]

www.we-online.com18 07/14Würth Elektronik eiSos®
Inductance vs. Current
0,1
1
10
100
1000
0,1 1 10
784777010
784777100
784777101
784777102
Rated current [A]
Inductance [µH]
WE-PDA
SMD Shielded Power Inductor
Size 7345
Dimensions (in mm)
Land pattern (in mm)
Electrical properties
Order Code L
(μH)
Tolerance
(%)
RDC
(mΩ) max.
IR
(A)
ISat
(A)
784 777 010 1.0 20% 38 3.7 8
784 777 022 2.2 20% 60 2.7 5.25
784 777 033 3.3 20% 69 2.5 4.7
784 777 047 4.7 20% 84 2.35 3.7
784 777 068 6.8 20% 99 2.2 3.2
784 777 082 8.2 20% 115 2 2.8
784 777 100 10 20% 126 1.9 2.6
784 777 220 22 20% 215 1.4 1.8
784 777 470 47 20% 300 1.15 1.25
784 777 101 100 20% 470 0.72 0.80
784 777 221 220 20% 1135 0.56 0.53
784 777 471 470 20% 2720 0.35 0.38
784 777 102 1000 20% 5760 0.25 0.28
4,0
8,0
1,7
2,0
no vias and traces in restricted area
Solder
Resist
4,0 ± 0,3
4,0 ± 0,3
7,3 ± 0,3
7,3 ± 0,3
1,5 ± 0,3

www.we-online.com 1907/14 Würth Elektronik eiSos®
WE-PDA
SMD Shielded Power Inductor
Size 1260
Dimensions (in mm)
Land pattern (in mm)
4,0
8,0
1,7
2,0
no vias and traces in restricted area
Solder Resist
Electrical properties
Order Code L
(μH)
Tolerance
(%)
RDC
(mΩ) max.
IR
(A)
ISat
(A)
784 771 010 1.0 20% 8.50 9.00 16.50
784 771 022 2.2 20% 12.50 7.20 10.50
784 771 033 3.3 20% 14.70 6.50 9.00
784 771 047 4.7 20% 17.50 6.20 8.00
784 771 068 6.8 20% 21.50 5.50 6.00
784 771 082 8.2 20% 24.00 5.05 5.50
784 771 100 10 20% 26.50 5.00 5.25
784 771 220 22 20% 41.00 3.20 3.50
784 771 470 47 20% 77.00 2.30 2.50
784 771 101 100 20% 174 1.50 1.70
784 771 221 220 20% 348 0.99 1.10
784 771 471 470 20% 706 0.65 0.75
784 771 102 1000 20% 1704 0.48 0.53
Inductance vs. Current
0
1
10
100
1000
0,1 1,0 10,0
784771010
784771100
784771101
784771102
Rated current [A]
Inductance [µH]
6,0 ± 0,3
12,0 ± 0,3
12,0 ± 0,3
8,0 ± 0,3

www.we-online.com20 07/14Würth Elektronik eiSos®
WE-PDA
SMD Shielded Power Inductor
Size 1280
Dimensions (in mm)
Electrical properties
Order Code L
(μH)
Tolerance
(%)
RDC
(mΩ) max.
IR
(A)
ISat
(A)
784 770 10 1.0 20% 9.8 8.3 22.0
784 770 22 2.2 20% 14.5 7.0 15.0
784 770 33 3.3 20% 21.4 6.6 12.0
784 770 47 4.7 20% 19.8 6.0 11.0
784 770 68 6.8 20% 25 5.2 8.5
784 770 100 10 20% 31 5.0 6.8
784 770 220 22 20% 45 4.0 4.7
784 770 470 47 20% 70 3.1 3.4
784 770 101 100 20% 145 2.1 2.3
784 770 221 220 20% 300 1.2 1.4
784 770 471 470 20% 570 0.8 1.0
784 770 102 1000 20% 1199 0.72 0.8
Land pattern (in mm)
4,0
8,0
1,7
2,0
no vias and traces in restricted area
Solder Resist
Inductance vs. Current
0,1
1
10
100
1000
0,1 1 10
78477010
784770100
784770101
784770102
Rated current [A]
Inductance [µH]
12,0 ± 0,38,0 ± 0,3
8,0 ± 0,3
12,0 ± 0,3

www.we-online.com 2107/14 Würth Elektronik eiSos®
WE-PDA
SMD Shielded Power Inductor
Size 1210
Dimensions (in mm)
Electrical properties
Order Code L
(μH)
Tolerance
(%)
RDC
(mΩ) max.
IR
(A)
ISat
(A)
784 770 9010 1.0 20% 9.60 9.2 23
784 770 9022 2.2 20% 14.5 7.5 16
784 770 9033 3.3 20% 17.00 7.0 13.5
784 770 9047 4.7 20% 19.50 6.0 11.0
784 770 9068 6.8 20% 24.50 5.5 9.0
784 770 9100 10 20% 29.50 5.0 7.5
784 770 9220 22 20% 45.00 4.3 5.0
784 770 9470 47 20% 67.00 3.2 3.5
784 770 9101 100 20% 123.00 2.2 2.4
784 770 9221 220 20% 247.00 1.45 1.6
784 770 9471 470 20% 495.00 0.9 1.1
784 770 9102 1000 20% 1060.00 0.63 0.7
Land pattern (in mm)
6,8
12,8
5,4
3,0
no vias and traces in restricted area
Solder Res
ist
Inductance vs. Current
0,1
1
10
100
1000
0,1 1 10
7847709010
7847709100
7847709101
7847709102
Rated current [A]
Inductance [µH]
12,0 ± 0,3
12,0 ± 0,3
10,0 ± 0,3
8,0 ± 0,3

www.we-online.com22 07/14Würth Elektronik eiSos®
WE-PD2A
SMD Power Inductor
Size 4532
Characteristics
Open size
Current capability up to 14 A
Operating temperature: -40 °C to +125 °C
Recommended solder profile: Reflow
Applications
Switching regulators with low operating voltage
(navigation system, air conditioning, entertainment,
park assistance control)
Integrated DC/DC-converter
Perfectly suitable for switching regulators with
extremely high efficiency
Electrical properties: Size 4532
Order Code L
(µH)
Tolerance
(%)
RDC
typ. (Ω)
RDC
max. (Ω)
IR
(A)
Isat
(A)
784 773 0 1.0
±20
0.014 0.049 4.00 5.72
784 773 018 1.8 0.028 0.064 2.70 3.60
784 773 022 2.2 0.034 0.071 2.50 3.38
784 773 033 3.3 0.041 0.086 2.00 2.88
784 773 039 3.9 0.054 0.094 1.88 2.57
784 773 047 4.7 0.059 0.110 1.82 2.46
784 773 056 5.6 0.069 0.126 1.58 2.43
784 773 068 6.8 0.076 0.131 1.54 2.10
784 773 082 8.2 0.116 0.146 1.50 1.80
784 773 10 10 0.118 0.182 1.45 1.74
784 773 112 12 0.156 0.210 1.28 1.62
784 773 115 15 0.204 0.235 1.20 1.46
784 773 118 18 0.225 0.338 1.10 1.29
784 773 122 22 0.261 0.370 1.00 1.22
784 773 127 27
±10
0.328 0.522 0.94 1.00
784 773 133 33 0.370 0.540 0.86 0.90
784 773 139 39 0.418 0.587 0.77 0.87
784 773 147 47 0.523 0.844 0.68 0.77
784 773 156 56 0.714 0.937 0.64 0.75
784 773 168 68 0.754 1.117 0.56 0.68
Note
The ambient temperature when operating the WE-PD series of storage chokes at full current rating load should generally range from
-40 °C to +85 °C. The self-heating of the component must be taken into account at higher ambient temperatures in order that the
permissible solder joint temperature is not exceeded or the wire insulation damaged. The wire used can withstand a temperature of
up to +150 °C. The ferrite core itself may be used over a far greater temperature range (approx. -50 °C to +250 °C [Curie tempera-
ture]). However, in this case, the tolerance limits of the inductor may be exceeded due to the temperature dependence of permeability.
Current derating at ambient
temperature of > 85 ºC
Inductance vs. DC bias current
Dimensions (in mm): Size 4532
4,0 ±0,3
4,5 ±0,3
3,2 ±0,3
1,0 ±0,3

www.we-online.com 2307/14 Würth Elektronik eiSos®
WE-PD2A
SMD Power Inductor
Size 4532 / Size 5848
Land pattern (in mm): Size 4532
Solder Resist
4,5 ref.
1,5 ref.
5,0 ref.
1,75 ref.
Dimensions (in mm): Size 5848
Land pattern (in mm): Size 5848
Electrical properties: Size 5848
Order Code L (µH) Tolerance (%) RDC typ. (Ω) RDC max. (Ω) IR (A) Isat (A)
784 774 003 0.33 ±20 0.006 0.008 10.8 15.30
784 774 006 0.6 -40/+20 0.009 0.018 8.20 13.50
784 774 022 2.2
±20
0.026 0.041 4.60 8.20
784 774 027 2.7 0.032 0.045 4.00 8.00
784 774 033 3.3 0.042 0.060 3.70 7.50
784 774 047 4.7 0.056 0.071 3.00 5.50
784 774 068 6.8 0.071 0.082 2.40 4.50
784 774 10 10 0.078 0.100 2.20 2.50
784 774 112 12 0.082 0.110 2.00 1.94
784 774 115 15 0.089 0.140 1.53 1.90
784 774 118 18 0.104 0.150 1.45 1.69
784 774 122 22 0.109 0.180 1.28 1.53
784 774 127 27 0.133 0.200 1.19 1.40
784 774 133 33
±15
0.150 0.230 1.09 1.17
784 774 139 39 0.215 0.320 0.94 1.10
784 774 147 47 0.260 0.370 0.86 1.00
784 774 156 56
±10
0.298 0.420 0.77 0.90
784 774 168 68 0.313 0.460 0.64 0.86
784 774 182 82 0.475 0.600 0.60 0.72
784 774 20 100 0.510 0.650 0.57 0.68
784 774 212 120 0.660 0.930 0.49 0.63
784 774 215 150 0.720 1.100 0.46 0.54
784 774 218 180 0.850 1.380 0.42 0.50
784 774 222 220 0.945 1.570 0.41 0.47
2,0 ±0,4
5,8 ± 0,3
5,2 ±0,3
4,5 ±0,35
Solder Resist
1,7 ref.
6,0 ref.
5,5 ref.
2,15 ref.
Inductance vs. rated current: Size 5848
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
784 773 168
784 773 127
784 773 0
784 773 082
100
784 774 222
784 774 156
784 774 118
784 774 022
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
784 775 222
784 775 247
784 775 127
784 775 012
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
784 776 222
784 776 247
784 776 127
784 776 012
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
784 773 168
784 773 127
784 773 0
784 773 082
100
784 774 222
784 774 156
784 774 118
784 774 022
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
784 775 222
784 775 247
784 775 127
784 775 012
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
784 776 222
784 776 247
784 776 127
784 776 012
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
Inductance vs. rated current: Size 4532

www.we-online.com24 07/14Würth Elektronik eiSos®
WE-PD2A
SMD Power Inductor
Size 7850
Dimensions (in mm)
Electrical properties
Order Code L
(µH)
Tolerance
(%)
RDC typ.
(Ω)
RDC max.
(Ω)
IR
(A)
Isat
(A)
784 775 012 1.2
±20
0.005 0.006 6.18 8.00
784 775 022 2.2 0.008 0.010 6.00 6.00
784 775 033 3.3 0.012 0.014 4.90 4.90
784 775 047 4.7 0.016 0.019 4.50 4.50
784 775 056 5.6 0.018 0.022 4.00 4.00
784 775 068 6.8 0.022 0.026 3.70 3.80
784 775 082 8.2 0.024 0.029 3.20 3.20
784 775 10 10
±10
0.040 0.070 2.30 2.95
784 775 112 12 0.042 0.080 2.18 2.23
784 775 115 15 0.044 0.090 1.93 2.20
784 775 118 18 0.053 0.100 1.89 2.14
784 775 122 22 0.065 0.110 1.76 1.81
784 775 127 27 0.074 0.120 1.48 1.62
784 775 133 33 0.089 0.130 1.35 1.47
784 775 139 39 0.116 0.160 1.25 1.33
784 775 147 47 0.134 0.180 1.17 1.24
784 775 168 68 0.218 0.280 0.99 1.05
784 775 182 82 0.248 0.370 0.90 0.95
784 775 20 100 0.281 0.430 0.77 0.86
784 775 212 120 0.340 0.470 0.67 0.81
784 775 215 150 0.467 0.640 0.60 0.71
784 775 218 180 0.574 0.710 0.55 0.57
784 775 222 220 0.614 0.960 0.51 0.56
784 775 227 270 0.699 1.110 0.47 0.51
784 775 233 330 0.980 1.260 0.43 0.48
784 775 239 390 1.151 1.770 0.38 0.43
784 775 247 470 1.370 1.960 0.360 0.38
Land pattern (in mm)
Solder Resist
2,0 ref.
8,0 ref.
7,5 ref.
3,0 ref.
Inductance vs. rated current
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
784 773 168
784 773 127
784 773 0
784 773 082
100
784 774 222
784 774 156
784 774 118
784 774 022
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
784 775 222
784 775 247
784 775 127
784 775 012
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
784 776 222
784 776 247
784 776 127
784 776 012
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
7,0 ±0,3
5,0 ±0,5
7,8 ±0,3
3,0 ±0,45
7,0 ±0,3
5,0 ±0,5
7,8 ±0,3
3,0 ±0,45

www.we-online.com 2507/14 Würth Elektronik eiSos®
WE-PD2A
SMD Power Inductor
Size 1054
Dimensions (in mm)
Electrical properties
Order Code L
(µH)
Tolerance
(%)
RDC typ.
(Ω)
RDC max.
(Ω)
IR
(A)
Isat
(A)
784 776 012 1.2
±20
0.004 0.0048 7.40 11.00
784 776 022 2.2 0.007 0.0078 7.00 8.00
784 776 033 3.3 0.009 0.0102 6.00 7.00
784 776 047 4.7 0.012 0.014 5.00 6.00
784 776 056 5.6 0.015 0.018 4.80 5.50
784 776 068 6.8 0.016 0.019 4.40 5.00
784 776 082 8.2 0.020 0.024 4.20 4.25
784 776 10 10 0.028 0.060 2.98 3.24
784 776 112 12 0.033 0.070 2.72 3.15
784 776 115 15 0.034 0.080 2.47 2.88
784 776 118 18 0.043 0.090 2.36 2.43
784 776 122 22 0.051 0.100 2.04 2.07
784 776 127 27 0.063 0.110 1.95 1.98
784 776 133 33 0.083 0.120 1.78 1.89
784 776 139 39 0.088 0.140 1.62 1.80
784 776 147 47
±10
0.095 0.170 1.45 1.62
784 776 156 56 0.112 0.190 1.36 1.53
784 776 168 68 0.138 0.220 1.19 1.49
784 776 182 82 0.150 0.250 1.11 1.17
784 776 20 100 0.200 0.350 1.02 1.10
784 776 212 120 0.243 0.400 0.94 0.99
784 776 215 150 0.300 0.470 0.81 0.90
784 776 218 180 0.320 0.630 0.76 0.78
784 776 222 220 0.451 0.730 0.67 0.77
784 776 227 270 0.500 0.970 0.62 0.68
784 776 233 330 0.750 1.150 0.52 0.59
784 776 239 390 0.794 1.300 0.49 0.54
784 776 247 470 0.969 1.480 0.44 0.50
Land pattern (in mm)
2,5 ref.
10,0 ref.
9,5 ref.
Solder Resist
3,75 ref.
10,0 ±0,4
9,0 ±0,4
5,4 ±0,5
3,5 ±0,5
Inductance vs. rated current
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
784 773 168
784 773 127
784 773 0
784 773 082
100
784 774 222
784 774 156
784 774 118
784 774 022
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
784 775 222
784 775 247
784 775 127
784 775 012
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
784 776 222
784 776 247
784 776 127
784 776 012
0,1
1
10
0,1 1 10
Rated current [A]
Inductance [µH]
100
10,0 ±0,4
9,0 ±0,4
5,4 ±0,5
3,5 ±0,5

www.we-online.com26 07/14Würth Elektronik eiSos®
WE-MAIA
SMD Metal Alloy Power Inductor
Size 2506 / Size 2508
Characteristics
Magnetic iron alloy allows high rated currents
Compact design
Magnetically shielded
High current capability and handles high transient
current spikes
Low acoustic noise and low leakage flux noise
Operating temperature: –40 °C to 125 °C
Applications
DC/DC-converter for high current power supplies
DC/DC-converter for Field Programmable Gate Array
(FPGA)
POL-converters
Portable power like PDA, digital camera
Mainboards/graphic cards
Battery powered devices
Wireless communication devices
Power supplies for smartphones, tablet PCs and
other mobile devices
Electrical properties: Size 2506
Order Code L
(µH)
Tolerance
(%)
IR
(A)
Isat
(A)
RDC typ.
(mΩ)
RDC max.
(mΩ)
784 383 210 047 0.47 ±30 2.2 3.7 76.0 95.0
784 383 210 10 1.0 1.25 2.5 163.0 196.0
IR referring to 40 K heating above ambient temperature
Isat referring to inductance loss of 20% typical
Dimensions (in mm)
Soldering Pad (in mm)
1,10
2,80
2,30
no vias and traces in restricted area
Solder Resist
Electrical properties: Size 2508
Order Code L
(µH)
Tolerance
(%)
IR
(A)
Isat
(A)
RDC typ.
(mΩ)
RDC max.
(mΩ)
784 383 220 047 0.47
±30
2.25 4.4 70.0 87.0
784 383 220 10 1.0 1.75 3.35 107.0 133.0
784 383 220 22 2.2 1.34 2.2 252.0 302.0
IR referring to 40 K heating above ambient temperature
Isat referring to inductance loss of 20% typical
Soldering Pad (in mm)
Dimensions (in mm)
1,10
2,80
2,30
no vias and traces in restricted area
Solder Resist
2,50 ±0,2
2,00 ±0,
2
0,70 ±0,2
0,60 max.
0,70 ±0,2
2,50 ±0,2
max. 0,80
2,00 ±0,
2
NEW!
4-times higher saturation current
Best efficiency Minimized package

www.we-online.com 2707/14 Würth Elektronik eiSos®
Electrical properties: Size 2510
Order Code L
(µH)
Tolerance
(%)
IR
(A)
Isat
(A)
RDC typ.
(mΩ)
RDC max.
(mΩ)
784 383 230 033 0.33 ±30 3.4 6.2 29.0 38.0
784 383 230 047 0.47 ±30 3.2 5.5 37.0 48.0
784 383 230 068 0.68 ±30 3.1 4.7 46.0 60.0
784 383 230 082 0.82 ±30 2.6 4.25 53.0 69.0
784 383 230 10 1.0 ±20 2.5 4.0 63.0 75.0
784 383 230 12 1.2 ±20 1.9 3.8 82.0 106
784 383 230 15 1.5 ±20 1.8 3.5 92.0 110
784 383 230 22 2.2 ±20 1.3 2.5 147 176
784 383 230 33 3.3 ±20 1.25 2.1 220 264
784 383 230 47 4.7 ±20 0.94 1.75 338 388
784 383 230 68 6.8 ±20 0.85 1.55 563 648
784 383 230 82 8.2 ±20 0.7 1.45 646 743
784 383 231 00 10.0 ±20 0.6 1.35 733 843
IR referring to 40 K heating above ambient temperature
Isat referring to inductance loss of 20% typical
Soldering Pad (in mm)
Dimensions (in mm)
2,80
1,10
2,30
no vias and traces in restricted area
Solder Resist
Electrical properties: Size 3010
Order Code L
(µH)
Tolerance
(%)
IR
(A)
Isat
(A)
RDC typ.
(mΩ)
RDC max.
(mΩ)
784 383 330 22 2.2
±20
1.4 3.9 150 172
784 383 330 33 3.3 1.1 2.95 232 266
784 383 330 47 4.7 0.9 2.4 305 350
IR referring to 40 K heating above ambient temperature
Isat referring to inductance loss of 20% typical
Soldering Pad (in mm)
Dimensions (in mm)
3,40
0,80
3,40
no vias and traces in restricted area
Solder Resist
0,70 ±0,2
2,50 ±0,2
max. 1,00
2,00 ±0,
2
max. 1,20
3,00 ±0,2
max. 1,00
3,00 ±0,2
WE-MAIA
SMD Metal Alloy Power Inductor
Size 2510 / Size 3010

www.we-online.com28 07/14Würth Elektronik eiSos®
Electrical properties: Size 3012
Order Code L
(µH)
Tolerance
(%)
IR
(A)
Isat
(A)
RDC typ.
(mΩ)
RDC max.
(mΩ)
784 383 340 033 0.33 ±30 4.8 11.1 13.2 15.8
784 383 340 047 0.47 ±30 4.0 9.4 16.6 19.9
784 383 340 056 0.56 ±30 3.6 8.5 27.0 32.4
784 383 340 068 0.68 ±20 3.5 7.7 28.7 34.4
784 383 340 10 1.0 ±20 2.75 6.6 41.2 50.5
784 383 340 12 1.2 ±20 2.65 6.0 46.8 56.1
784 383 340 15 1.5 ±20 2.0 5.7 75.3 90.3
784 383 340 22 2.2 ±20 1.80 5.0 100 115.0
784 383 340 33 3.3 ±20 1.4 4.0 136.8 164.2
784 383 340 47 4.7 ±20 1.1 3.8 222.6 256
784 383 340 56 5.6 ±20 1.0 3.0 338.3 389
784 383 340 68 6.8 ±20 0.88 2.7 368.2 423.4
IR referring to 40 K heating above ambient temperature
Isat referring to inductance loss of 20% typical
Dimensions (in mm)
Soldering Pad (in mm)
3,40
0,80
3,40
Solder Resist
no vias and traces in restricted area
3,00 ±0,2
3,00 ±0,2
max. 1,20
max. 1,2
WE-MAIA
SMD Metal Alloy Power Inductor
Size 3012

www.we-online.com 2907/14 Würth Elektronik eiSos®
Electrical properties: Size 3015
Order Code L
(µH)
Tolerance
(%)
IR
(A)
Isat
(A)
RDC typ.
(mΩ)
RDC max.
(mΩ)
784 383 350 047 0.47 ±30% 4.6 5.8 20.0 23.0
784 383 350 068 0.68 ±30% 4.1 8.1 25.0 30.0
784 383 350 082 0.82 ±30% 3.5 7.0 30 35.0
784 383 350 10 1.0 ±20% 2.7 4.5 39.0 47.0
784 383 350 22 2.2 ±20% 1.8 3.5 94.0 108
784 383 350 33 3.3 ±20% 1.7 3.2 114 131
784 383 350 47 4.7 ±20% 1.5 2.8 141 162
784 383 350 68 6.8 ±20% 1.1 2.4 250 287
784 383 351 00 10.0 ±20% 0.85 2.0 446 513
784 383 351 50 15.0 ±20% 0.65 1.71 720 830
784 383 352 20 22.0 ±20% 0.60 1.60 940 1040
784 383 353 30 33.0 ±20% 0.50 1.30 1210 1330
784 383 354 70 47.0 ±20% 0.39 1.18 2090 2300
IR referring to 40 K heating above ambient temperature
Isat referring to inductance loss of 20% typical
Dimensions (in mm)
Soldering Pad (in mm)
3,40
0,80
3,40
Solder Resist
no vias and traces in restricted area
3,00 ±0,2
3,00 ±0,2
max. 1,50
max. 1,2
WE-MAIA
SMD Metal Alloy Power Inductor
Size 3015

www.we-online.com30 07/14Würth Elektronik eiSos®
Design Kit WE-CBA
SMD EMI Suppression Ferrite Bead
Order Code 782 792, Version 1.1
Electrical properties
Order Code Size Z @ 100 MHz
(Ω)
IR
(mA)
RDC
(Ω)
Type of
Application
782 422 101
0402
100 500 0.300 Wide Band
782 422 221 220 400 0.300 Wide Band
782 422 331 330 300 0.500 Wide Band
782 422 511 510 200 0.800 Wide Band
782 422 601 600 200 0.800 Wide Band
782 422 102 1000 200 1.000 Wide Band
782 423 100 10 1500 0.030 High Current
782 423 700 70 1000 0.090 High Current
782 631 101
0603
100 500 0.200 High Speed
782 631 331 330 400 0.250 High Speed
782 631 182 1800 100 0.750 High Speed
782 632 620 62 500 0.150 Wide Band
782 632 121 120 500 0.200 Wide Band
782 632 181 180 500 0.200 Wide Band
782 632 511 510 300 0.350 Wide Band
782 632 102 1000 200 0.500 Wide Band
782 633 620 62 2500 0.040 High Current
782 633 601 600 1000 0.200 High Current
782 851 102
0805
1000 300 0.350 High Speed
782 851 202 2200 200 0.450 High Speed
782 853 200 20 5000 0.008 High Current
782 853 270 27 4000 0.015 High Current
782 853 680 68 3000 0.025 High Current
782 853 910 91 2000 0.060 High Current
782 853 121 120 2500 0.035 High Current
782 583 221 220 2000 0.050 High Current
782 853 561 560 1500 0.100 High Current
782 853 112 1100 800 0.300 High Current
752 853 152 1500 700 0.350 High Current
782 762 301
1206
300 500 0.100 Wide Band
782 763 820 82 3000 0.025 High Current
782 763 621 620 1500 0.100 High Current
782 763 102 1000 1000 0.300 High Current
782 963 560 1806 56 5000 0.008 High Current
782 963 820 82 3500 0.020 High Current
Characteristics
Reliable Ni-Sn electrodes
High rated current up to 5 A
Recommended soldering: Reflow
Operating temperature: -55 °C to +125 °C
Applications
Perfect as data lined filter and for uncoupling
of distribution voltage

www.we-online.com 3107/14 Würth Elektronik eiSos®
Design Kit WE-AEFA
Axial EMI Suppression Ferrite
Order Code 782 013, Version 1.1
Characteristics
Ferrite core made of NiZn, a material which works
in a wide frequency range
Many different types for the best possible
interference suppression
Operating temperature: -55 °C up to +150 °C
Applications
In general for: wires, coaxial cables, wire-wrapping
cables, multiconductor wires
Data and signal lines
On board power supply line
Multimedia cable interfaces
Various, other cable interfaces
Electrical properties
Order Code OD
(mm)
ID
(mm)
H
(mm) Cable Diameter (mm) Z @ 25 MHz
1 turn (Ω)
Z @ 100 MHz
1 turn (Ω)
782 013 033 150 12.0 3.55 15.0 ≤ 3.3 150 205
782 013 044 095 9.5 4.75 9.5 ≤ 4.4 60 84
782 013 046 185 11.5 5.0 18.5 ≤ 4.6 135 186
782 013 046 250 11.5 5.0 25.0 ≤ 4.6 185 255
782 013 057 450 12.0 6.1 45.0 ≤ 5.7 255 370
782 013 059 285 14.0 6.3 28.5 ≤ 5.9 195 270
782 013 068 250 14.0 7.2 25.0 ≤ 6.8 150 210
782 013 069 155 12.0 7.3 15.5 ≤ 6.9 70 100
782 013 069 285 15.5 7.3 28.5 ≤ 6.9 190 270
782 013 076 285 16.0 8.0 28.5 ≤ 7.6 170 240
782 013 076 508 16.0 8.0 50.8 ≤ 7.6 325 460
782 013 079 285 14.0 8.2 28.5 ≤ 7.9 140 200
782 013 086 280 16.0 9.0 28.0 ≤ 8.6 140 205
782 013 091 285 17.5 9.5 28.5 ≤ 9.1 150 220
782 013 100 280 15.5 10.5 28.0 ≤ 10.0 100 150
782 013 110 508 19.0 11.5 50.8 ≤ 11.0 235 345
782 013 125 280 19.0 13.0 28.0 ≤ 12.5 95 150
782 013 125 285 26.0 13.0 28.5 ≤ 12.5 170 240
782 013 150 285 26.0 15.5 28.5 ≤ 15.0 130 190

www.we-online.com32 07/14Würth Elektronik eiSos®
Design Kit WE-PDA
SMD Power Inductor
Order Code 784 770 & 784 778, Version 1.1
Electrical properties: Order Code 784 770
Order Code Size L
(μH)
RDC
(Ω)
IR
(A)
Isat
(A)
784 771 010
1260
1 8.50 9.00 16.50
784 771 022 2.2 12.50 7.20 10.50
784 771 033 3.3 14.50 6.50 9.00
784 771 047 4.7 17.50 6.20 8.00
784 771 068 6.8 21.50 5.50 6.00
784 771 082 8.2 24.00 5.05 5.50
784 771 100 10 26.50 5.00 5.25
784 771 220 22 40.00 3.20 3.50
784 771 470 47 77.00 2.30 2.50
784 771 101 100 174 1.50 1.70
784 771 221 220 348 0.99 1.10
784 771 102 1000 1705 0.48 0.53
784 770 10
1280
1 9.00 8.30 22.00
784 770 22 2.2 14.50 7.00 15.00
784 770 33 3.3 17.00 6.60 12.00
784 770 47 4.7 20.00 6.00 11.00
784 770 68 6.8 25.00 5.20 8.50
784 770 100 10 31.00 5.00 6.80
784 770 220 22 44.50 4.00 4.70
784 770 470 47 71.00 3.10 3.40
784 770 101 100 144.00 2.10 2.30
784 770 471 470 570.00 0.80 1.00
784 770 102 1000 1200.00 0.72 0.80
784 770 901 0
1210
1 8.50 9.20 23.00
784 770 902 2 2.2 14.50 7.50 16.00
784 770 903 3 3.3 17.00 7.00 13.50
784 770 904 7 4.7 19.00 6.00 11.00
784 770 906 8 6.8 24.00 5.50 9.00
784 770 910 0 10 30.00 5.00 7.50
784 770 922 0 22 44.00 4.30 5.00
784 770 947 0 47 67.00 3.20 3.50
784 770 910 1 100 120.00 2.20 2.40
784 770 922 1 220 245.00 1.45 1.60
784 770 947 1 470 490.00 0.90 1.10
784 770 910 2 1000 1060 0.63 0.70
Electrical properties: Order Code 784 778
Order Code Size L
(μH)
RDC
(Ω)
IR
(A)
Isat
(A)
784 777 010
7332
1 39 3.70 8.00
784 777 022 2.2 61 2.70 5.25
784 777 033 3.3 70 2.50 4.70
784 777 047 4.7 84 2.35 3.70
784 777 068 6.8 98 2.20 3.20
784 777 082 8.2 117 2.00 2.80
784 777 100 10 126 1.90 2.60
784 777 220 22 215 1.40 1.80
784 777 470 47 300 1.15 1.25
784 777 101 100 470 0.72 0.80
784 777 221 220 2720 0.50 0.55
784 777 471 470 5750 0.35 0.38
784 777 102 1000 5760 0.25 0.28
784 778 010
7345
1 36 3.50 7.00
784 778 022 2.2 50 3.10 5.00
784 778 033 3.3 65 2.65 3.70
784 778 047 4.7 79 2.40 3.10
784 778 068 6.8 107 2.30 2.50
784 778 082 8.2 103 2.20 2.40
784 778 100 10 126 1.85 2.20
784 778 220 22 187 1.55 1.60
784 778 470 47 348 1.10 1.05
784 778 101 100 720 0.72 0.75
784 778 221 220 1620 0.48 0.50
784 778 471 470 3300 0.30 0.35
784 778 102 1000 7200 0.23 0.25
Characteristics
Wire connection: welding technology
Operating Temperature -40 °C up to +125 °C
Highes possible current loading for SMD Inductors
Magnetically shielded version which results in a
low leakage field
High storage capacity
Low self-losses
Core Material: NiZn
Applications
Multimedia applications
Switching regulators with low operating voltages
(Computer, Notebook, smart phones)
Integrated DC/DC-converter
Perfect suitable for switching regulators with
extremely high efficiency (> 86 %)
low leakage field

www.we-online.com 3307/14 Würth Elektronik eiSos®
Design Kit WE-PD2A
SMD Power Inductor
Order Code 784 773 & 784 775, Version 1.1
Characteristics
Open size
Current capability up to 14 A
Operating temperature: -40 °C to +125 °C
Recommended solder profile: Reflow
Applications
Switching regulators with low operating voltage
(navigation system, air conditioning, entertainment,
park assistance control)
Integrated DC/DC-converter
Perfectly suitable for switching regulators with
extremely high efficiency
Electrical properties: Order Code 784 775
Order Code Size L
(μH)
RDC
(Ω)
IR
(A)
Isat
(A)
784 775 10
7850
10 0.040 2.30 2.95
784 775 112 12 0.042 2.18 2.23
784 775 115 15 0.044 1.93 2.20
784 775 118 18 0.053 1.89 2.14
784 775 122 22 0.065 1.76 1.81
784 775 127 27 0.074 1.48 1.62
784 775 133 33 0.130 1.35 1.47
784 775 139 39 0.116 1.25 1.33
784 775 147 47 0.134 1.17 1.24
784 775 168 68 0.218 0.99 1.05
784 775 182 82 0.248 0.90 0.95
784 775 20 100 0.281 0.77 0.86
784 775 215 150 0.467 0.60 0.71
784 775 218 180 0.574 0.55 0.57
784 775 222 220 0.614 0.51 0.56
784 775 227 270 0.699 0.47 0.51
784 775 239 396 1.151 0.38 0.43
784 775 247 470 1.370 0.36 0.38
784 776 10
1054
10 0.028 2.98 3.24
784 776 118 18 0.043 2.36 2.43
784 776 122 22 0.051 2.04 2.07
784 776 127 27 0.063 1.95 1.98
784 776 133 33 0.083 1.78 1.89
784 776 139 39 0.088 1.62 1.80
784 776 147 47 0.095 1.45 1.62
784 776 156 56 0.112 1.36 1.53
784 776 168 68 0.138 1.19 1.49
784 776 182 82 0.150 1.11 1.17
784 776 20 100 0.200 1.02 1.10
784 776 212 120 0.243 0.94 0.99
784 776 215 150 0.300 0.81 0.90
784 776 218 180 0.320 0.76 0.78
784 776 222 220 0.451 0.67 0.77
784 776 233 330 0.750 0.52 0.59
784 776 247 470 0.969 0.44 0.50
Electrical properties: Order Code 784 773
Order Code Size L
(μH)
RDC
(Ω)
IR
(A)
Isat
(A)
784 773 0
4532
1.00 0.014 4.0 5.72
784 773 018 1.8 0.028 2.70 3.60
784 773 022 2.2 0.034 2.50 3.38
784 773 033 3.3 0.041 2.00 2.88
784 773 039 3.9 0.054 1.88 2.57
784 773 047 4.7 0.059 1.82 2.46
784 773 068 6.8 0.076 1.54 2.10
784 773 10 10 0.118 1.45 1.74
784 773 112 12 0.156 1.28 1.62
784 773 115 15 0.204 1.20 1.46
784 773 118 18 0.225 1.10 1.29
784 773 122 22 0.261 1.00 1.22
784 773 127 27 0.328 0.94 1.00
784 773 133 33 0.370 0.86 0.90
784 773 147 47 0.523 0.68 0.77
784 773 168 68 0.754 0.56 0.68
784 774 022
5848
2.2 0.026 4.60 8.20
784 774 027 2.7 0.032 4.00 8.00
784 774 033 3.3 0.042 3.70 7.50
784 774 047 4.7 0.056 3.00 5.50
784 774 068 6.8 0.071 2.40 5.00
784 774 10 10 0.078 2.20 2.5
784 774 112 12 0.082 2.00 1.94
784 774 115 15 0.089 1.53 1.90
784 774 118 18 0.104 1.45 1.69
784 774 122 22 0.109 1.28 1.53
784 774 127 27 0.133 1.19 1.40
784 774 133 33 0.150 1.09 1.17
784 774 147 47 0.260 0.86 1.00
784 774 156 56 0.298 0.77 0.90
784 774 168 68 0.313 0.64 0.86
784 774 182 82 0.475 0.60 0.72
784 774 20 100 0.510 0.57 0.68
784 774 215 150 0.720 0.46 0.54
784 774 222 220 0.945 0.41 0.47
Operating temperature: -40 °C to +125 °C
Recommended solder profile: Reflow

www.we-online.com34 07/14Würth Elektronik eiSos®
Design Kit WE-MAIA
SMD Metal Alloy Power Inductor
Order Code 784 3833 & 784 3832, Version 1.0
Characteristics
Magnetic iron alloy allows high rated currents
Compact design
Magnetically shielded
High current capability and handles high transient
current spikes
Low acoustic noise and low leakage flux noise
Operating temperature: –40 °C to 125 °C
Applications
DC/DC-converter for high current power supplies
DC/DC-converter for Field Programmable Gate Array
(FPGA)
POL-converters
Portable power like PDA, digital camera
Mainboards/graphic cards
Battery powered devices
Wireless communication devices
Power supplies for smartphones, tablet PCs and
other mobile devices
Electrical properties: Order Code 784 3833
Order Code Size L
(μH)
IR
(A)
Isat
(A)
RDC
(Ω)
784 383 330 22
3010
2.2 1.4 3.9 150
784 383 330 33 3.3 1.1 2.95 232
784 383 330 47 4.7 0.9 2.4 356
784 383 340 033
3012
0.33 4.8 11.1 19.0
784 383 340 047 0.47 4.0 9.4 22.0
784 383 340 056 0.56 3.6 8.5 29.0
784 383 340 068 0.68 3.5 7.7 36.0
784 383 340 10 1.0 2.75 6.6 42.1
784 383 340 12 1.2 2.65 6.0 55.0
784 383 340 15 1.5 2.0 5.7 80.0
784 383 340 22 2.2 1.80 5.0 100
784 383 340 33 3.3 1.4 4.0 156.3
784 383 340 47 4.7 1.1 3.80 267.7
784 383 340 56 5.6 1.0 3.0 338.3
784 383 340 68 6.8 0.88 2.7 368.2
784 383 350 10
3015
1.0 2.7 4.5 39.0
784 383 350 22 2.2 1.8 3.5 94.0
784 383 350 33 3.3 1.7 3.2 114
784 383 350 47 4.7 1.5 2.8 141
784 383 350 68 6.8 1.1 2.4 250
784 383 351 00 10.0 0.85 2.0 446
784 383 351 50 15.0 0.65 1.71 720
784 383 352 20 22.0 0.60 1.60 940
784 383 353 30 33.0 0.50 1.30 1210
784 383 354 70 47.0 0.39 1.18 2090
Electrical properties: Order Code 784 3832
Order Code Size L
(μH)
IR
(A)
Isat
(A)
RDC
(Ω)
784 383 210 047 2506 0.47 2.2 3.7 76.0
784 383 210 10 1.0 1.25 2.5 163.0
784 383 220 047
2508
0.47 2.25 4.4 70.0
784 383 220 10 1.0 1.75 3.35 107.0
784 383 220 22 2.2 1.34 2.2 252.0
784 383 230 033
2510
0.33 3.4 6.2 29.0
784 383 230 047 0.47 3.2 5.5 37.0
784 383 230 068 0.68 3.1 4.7 46.0
784 383 230 082 0.82 2.6 4.25 53.0
784 383 230 10 1.0 2.5 4.0 63.0
784 383 230 12 1.2 1.9 3.8 82.0
784 383 230 15 1.5 1.8 3.5 92.0
784 383 230 22 2.2 1.3 2.5 147
784 383 230 33 3.3 1.25 2.1 220
784 383 230 47 4.7 0.94 1.75 338
784 383 230 68 6.8 0.85 1.55 563
784 383 230 82 8.2 0.7 1.45 646
784 383 231 00 10.0 0.6 1.35 733
Order Code 784 3833 & 784 3832, Version 1.0
Characteristics

www.we-online.com 3507/14 Würth Elektronik eiSos®
Total Quality Management
Analysis laboratory:
XRF
IFR
Computer Tomography
Hi Pot Tester up to 10 kV
Network Analyzer
Oscilloscopes
Precision LCR
Source Meter
Efficiency Measurement
Twister Thermal Characterisation
Moisture Balance
Vision Measuring
Profile Projector
DSC
Precision Magnetics Analyzer
Hi Pot Tester 6,0 kV
Multiohmmeter
Stereomicroscope 45x with camera
Impedance Analyzer
Reflow Oven
Stereomicroscope 5000X
Reliability laboratory:
Glow Wire Tester
Salt Spray Chamber
Flammability Tester
Steamaging Machine
Temperature Cycling Oven
Thermal Shock Oven
Thermal Oven
Wetting Balance Machine
Push and Pull Tester
Wave Soldering
DC Bias Measurement System
Epoxy chamber
PCB sample boards
LED Measurement Equipment
Grinding Machine
Force Meter
Mechanical tools
Vibration up to 50g
Mechanical Shock up to 100g

DIENECKARPRINZEN 999931.0614.5‘.FLY
General:
All recommendations according to the general technical specifications of the datasheet have to be complied with.
The disposal and operation of the product within ambient conditions which probably alloy or harm the component surface
has to be avoided.
If the product is potted in costumer applications, the potting material might shrink during and after hardening. According-
ly to this the product is exposed to the pressure of the potting material with the effect that the ferrite body and termination
is possibly damaged by this pressure and so the electrical as well as the mechanical characteristics are endanger to be
affected. After the potting material is cured, the ferrite body and termination of the product have to be checked if any
reduced electrical or mechanical functions or destructions have occurred.
The responsibility for the applicability of customer specific products and use in a particular customer design is always
within the authority of the customer. All technical specifications for standard products do also apply for customer specific
products.
Washing varnish agent that is used during the production to clean the application might damage or change the charac-
teristics of the plating. The washing varnish agent could have a negative effect on the long term function of the product.
Direct mechanical impact to the product shall be prevented as the ferrite material of the ferrite body could flake or in the
worst case it could break.
Product specific:
Follow all instructions mentioned in the datasheet, especially:
The solder profile has to be complied with according to the technical reflow soldering specification,
otherwise no warranty will be sustained.
Wave soldering is only allowed after evaluation and approval.
All products are supposed to be used before the end of the period of 12 months based on the
product date-code, if not a 100 % solderability can’t be warranted.
Violation of the technical product specifications such as exceeding the nominal rated current
will result in the loss of warranty.
Cautions and Warnings
Information in this catalogue is subject to change. The process of continually improving our product range leads to changes
in content. For new designs please refer to our latest data sheets on www.we-online.com or contact our field staff.
www.we-online.com
Products related to this Datasheet
FERRITE BEAD 600 OHM 0603 1LN
FERRITE BEAD 10 OHM 0402 1LN
FERRITE BEAD 330 OHM 0402 1LN
FERRITE BEAD 1 KOHM 1206 1LN
FERRITE BEAD 82 OHM 1206 1LN
FERRITE BEAD 1 KOHM 0603 1LN
FERRITE BEAD 1.5 KOHM 0805 1LN
FERRITE BEAD 68 OHM 0805 1LN
FERRITE BEAD 220 OHM 0402 1LN
FERRITE BEAD 100 OHM 0402 1LN
FERRITE BEAD 330 OHM 0603 1LN
FERRITE BEAD 1.1 KOHM 0805 1LN
FERRITE BEAD 560 OHM 0805 1LN
FERRITE BEAD 1 KOHM 0805 1LN
FERRITE BEAD 560 OHM 0805 1LN
FERRITE BEAD 510 OHM 0603 1LN
FERRITE BEAD 82 OHM 1206 1LN
FERRITE BEAD 620 OHM 1206 1LN
FERRITE BEAD 1 KOHM 0603 1LN
FERRITE BEAD 27 OHM 0805 1LN
FERRITE BEAD 620 OHM 1206 1LN
FERRITE BEAD 120 OHM 0603 1LN
FERRITE BEAD 1 KOHM 0402 1LN
FERRITE BEAD 70 OHM 0402 1LN
FERRITE CORE 345 OHM SOLID
FERRITE BEAD 220 OHM 0805 1LN
FERRITE BEAD 1.1 KOHM 0805 1LN
FERRITE BEAD 82 OHM 1806 1LN
FERRITE BEAD 68 OHM 0805 1LN
FERRITE BEAD 1.5 KOHM 0805 1LN