MLX90288 Datasheet by Melexis Technologies NV

View All Related Products | Download PDF Datasheet
Meleiié' ‘JLHHED :N’LWEEMM,
MLX90288
Datasheet
REVISION 5 21 JULY 2017
3901090288
1. Features and Benefits
Surface mounted device
Analog ratiometric output
Measurement range from ±6mT to
±650mT bipolar full scale
Digital IIR filtering for accurate bandwidth
Offset trimming possible outside output
range
1st and 2nd order magnet TC
compensation
Reverse polarity and overvoltage
protection
Extensive diagnostic features
2. Application Examples
Rotary position sensor
Linear position sensor
Proximity sensor
3. Description
The MLX90288 is a cost-effective monolithic
programmable linear Hall sensor which provides
an analog ratiometric output signal proportional
to the magnetic flux density that is applied
perpendicular to the die surface. The MLX90288 is
fully programmable (offset, sensitivity, clamping
levels, magnet temperature drift, digital IIR
filtering ) through the connector, using the PTC-
04 programming tool. It supports both linear and
quadratic magnet Thermal Compensation.
Figure 1 gives the block diagram
Mele_)'('i§""’
MLX90288
Datasheet
Page 2 of 23
REVISION 5 21 JULY 2017
3901090288
Contents
1. Features and Benefits ............................................................................................................................ 1
2. Application Examples ............................................................................................................................. 1
3. Description ............................................................................................................................................ 1
4. Ordering Information ............................................................................................................................ 4
5. Glossary of Terms .................................................................................................................................. 4
6. Pin Definitions and Descriptions ............................................................................................................ 5
7. Absolute Maximum Ratings ................................................................................................................... 5
8. General Electrical Specifications ............................................................................................................ 6
9. Timing Specification............................................................................................................................... 7
10. Transfer Characteristic Specification ................................................................................................... 8
11. Accuracy Specification ......................................................................................................................... 9
12. Diagnostic Specification ..................................................................................................................... 10
13. Startup, Undervoltage, Overvoltage and Reset Specification ............................................................. 11
14. EMC/ESD Specification ...................................................................................................................... 12
15. EEPROM Mapping ............................................................................................................................. 13
15.1. EEPROM Description ...................................................................................................................... 13
15.2. Melexis Programmable Parameters .............................................................................................. 13
15.2.1. OSCTRIM [4:0] ........................................................................................................................... 13
15.2.2. TRIMCTAT [4:0] ......................................................................................................................... 13
15.2.3. ITRIM[2:0] ................................................................................................................................. 13
15.2.4. IPLATE[3:0] ................................................................................................................................ 13
15.2.5. TC1ST[6:0] ................................................................................................................................. 13
15.2.6. TC2ND[5:0] ................................................................................................................................ 14
15.2.7. TC3RD[2:0] ................................................................................................................................ 14
15.2.8. PLATEPOL .................................................................................................................................. 14
15.2.9. OFFCST[4:0] ............................................................................................................................... 14
15.2.10. OFFDRIFT[5:0] ......................................................................................................................... 14
15.2.11. ROUGHGAIN[2] ....................................................................................................................... 14
15.2.12. XA[13:0] ................................................................................................................................... 14
15.2.13. MLXID[31:0] ............................................................................................................................ 14
15.2.14. CRC[9:0] .................................................................................................................................. 15
Mele_)'('i§""’
MLX90288
Datasheet
Page 3 of 23
REVISION 5 21 JULY 2017
3901090288
15.3. Melexis Programmable Parameters .............................................................................................. 15
15.3.1. FAULTONCLIP ............................................................................................................................ 15
15.3.2. DIAGINFAULT ............................................................................................................................ 15
15.3.3. FILTCODE[3:0] ........................................................................................................................... 15
15.3.4. TEMPSENSOR ............................................................................................................................ 16
15.3.5. SECONDORDERTC ..................................................................................................................... 16
15.3.6. TEMPOFF[9:0] ........................................................................................................................... 16
15.3.7. TEMPTC[7:0] ............................................................................................................................. 16
15.3.8. CLPLow[8:0] .............................................................................................................................. 16
15.3.9. CLPHigh[9:0].............................................................................................................................. 16
15.3.10. ROUGHGAIN[1:0] .................................................................................................................... 16
15.3.11. ATTN2P5 .................................................................................................................................. 16
15.3.12. FINEGAIN[12:0] ....................................................................................................................... 16
15.3.13. YA[13:0] ................................................................................................................................... 17
15.3.14. CSTID[15:0] ............................................................................................................................. 17
16. Thermal Sensitivity Drift Compensation............................................................................................. 18
16.1. Introduction .................................................................................................................................... 18
16.2. Linear Compensation (1st Order) ................................................................................................... 18
17. Standard Information ........................................................................................................................ 19
18. ESD Precautions ................................................................................................................................. 19
19. Package Specification ........................................................................................................................ 20
19.1. Package Dimensions ....................................................................................................................... 20
19.2. Package Marking ............................................................................................................................. 21
19.3. Recommended Application Diagram ............................................................................................. 22
20. Revision History Table ....................................................................................................................... 22
21. Contact .............................................................................................................................................. 22
22. Disclaimer .......................................................................................................................................... 23
Melex'i "" wswkin muwzmc
MLX90288
Datasheet
Page 4 of 23
REVISION 5 21 JULY 2017
3901090288
4. Ordering Information
Product
Temperature
Package
Option Code
Packing Form
MLX90288
L
DC
CAA-000
TU
MLX90288
L
DC
CAA-000
RE
MLX90288
K
DC
CAA-000
TU
MLX90288
K
DC
CAA-000
RE
Temperature Code:
L: from -40°C to 150°C
K:from -40°C to 125°C
Package Code:
“DC” for SOIC-8 package, 150Mil
Option Code:
CAA-000
Packing Form:
“RE for Reel”, “TU for Tube”
Ordering Example:
MLX90288LDC-CAA-000-RE”
Table 1
5. Glossary of Terms
Gauss (G), Tesla (T)
Units for the magnetic flux density 1 mT = 10 G
TC
Temperature Coefficient (in ppm/Deg.C.)
NC
Not Connected
ADC
Analog-to-Digital Converter
DAC
Digital-to-Analog Converter
LSB
Least Significant Bit
MSB
Most Significant Bit
DNL
Differential Non-Linearity
INL
Integral Non-Linearity
ASP
Analog Signal Processing
Melex'i "" wswkin muwzmc
MLX90288
Datasheet
Page 5 of 23
REVISION 5 21 JULY 2017
3901090288
Gauss (G), Tesla (T)
Units for the magnetic flux density 1 mT = 10 G
DSP
Digital Signal Processing
EMC
Electro-Magnetic Compatibility
FSM
Finite State Machine
Table 2
6. Pin Definitions and Descriptions
Pin #
Name
Description
1
VDD
Supply
2
VSS
Ground
3
N/C
Not connected
4
OUT
Analog + PTC communication
5
IDDQ
Test
6
TESTOUT
Test
7
MUST0
Test
8
MUST1
Test
Table 3 gives the pinout
The pinout of the MLX90288 of the global pins is identical to that of the MLX90291 (PWM output), making drop -in
replacements possible for multi-protocol applications. Both ICs have differences in architecture, apart from the
protocol only.
7. Absolute Maximum Ratings
Item
Symbol
Rating
Supply Forward-Voltage
VDDFWD
+ 30 V (continuous)
(Breakdown at + 40 V)
Supply Forward-Current
IDDFWD
+ 20 mA
Melex'i "" wswkin mmmmc
MLX90288
Datasheet
Page 6 of 23
REVISION 5 21 JULY 2017
3901090288
Item
Symbol
Rating
Supply Reverse-Voltage
VDDREV
14.5 V (continuous)
(Breakdown at 19 V)
Supply Reverse-Current
IDDREV
2 mA
Output Forward-Voltage
VOUTFWD
+ 18 V
Output Forward-Current
IOUTFWD
60 mA
Output Reverse-Voltage
VOUTREV
14 V
Output Reverse-Current
IOUTREV
+ 20 mA
Storage Temperature Range
(Non Operating)
TS
-55°C to +165°C
Operating Ambient
Temperature Range
TA
-40°C to +150°C
Junction Temperature
TJ
+165°C
Package Thermal Resistance
RTH
100 K/W
Maximum Flux Density
BMAX
2T
Table 4 gives the maximum ratings.
Exceeding the absolute maximum ratings may cause permanent damage. Exposure to absolute maximum-rated
conditions for extended periods may affect device reliability.
8. General Electrical Specifications
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Supply Voltage
VDD
Guaranteed spec operation
4.5
5
5.5
V
Supply Current
IDD
Worst case (min RPD, max
VDD)
-
8.8
10
mA
Regulated Voltage
VREG
Internal voltage
3.0
3.3
3.6
V
Reset Voltage
VPORRISE
Output is high impedant for
VPOR < VDD < VUNDER
2.5
3.4
V
VPORFALL
2.4
3.3
V
Undervoltage Threshold
VUNDERRISE
Operating if VDD > VUNDER
3.4
4.4
V
VUNDERFALL
3.3
4.3
V
MeleXIs ' wswkin mmmmc
MLX90288
Datasheet
Page 7 of 23
REVISION 5 21 JULY 2017
3901090288
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Programming Voltage(1)
VPROGRISE
6.2
7.2
V
VPROGFALL
Device not locked
6.1
7.1
V
Overvoltage Threshold(2)
VOVER
Disconnect VPROT from VDD
8.4
14
V
Load Resistance Range
RPD
Pull-down to GND
8
10
330
Load capacitor range
CL
Between OUT and GND
47
1000
nF
Output Saturation
Voltage(3)
VSATHI
Including RPD
96
100
%VDD
VSATLO
Including RPD
0
2
%VDD
Output Current
Limitation(4)
IOUTLIMGND
Output amplifier sourcing
strength
2
5
8
mA
IOUTLIMVDD
Output amplifier sinking
strength
2
5
8
mA
Supply Current Limitation
IVDDLIM
Same condition as above
5
18
mA
Output Diagnostic Band
Leakage Current(5)
IDIAGLO
Leakage current over TA
VDD=5V
500
nA
Output Diagnostic Level
VDIAGLO
Leakage current over TA and
VDD span
RPD x
IDIAGLO
V
Table 5 gives the electrical specifications
(1) The programming voltage defines the threshold at which the ASIC goes into PTC mode, where the output pin
becomes bidirectional. Write access is eventually defined by the locking bits as described in subsequent sections.
(2) The overvoltage threshold will disconnect all internal supplies (Vana, Vdig & Vprot) from VDD; the output becomes
high impedant.
(3) The saturation voltage is the rail voltage the output amplifier can reach actively with RPD connected.
(4) The maximum current the output stage can deliver to keep its DC value, in case the output is pulled to one of the
rails by means of an external power supply, while VDD = 5V.
(5) The leakage current is in fact the current sourced by the output in case of an OBD detection (broken ground), where
the output goes into high-Z mode. For better contacting at the connectors over lifetime and bigger rail-to-rail
operation, the smaller pull-down resistors from this specification are recommended at ECU side.
9. Timing Specification
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Power Supply Slew Rate
VDDSR
External supply VDD
5e-6
5
V/µs
Melex'i "" wswkin mmmmc
MLX90288
Datasheet
Page 8 of 23
REVISION 5 21 JULY 2017
3901090288
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Startup time(1)
tSTARTUP
200
500
800
µs
Main Oscillator Frequency
FOSC
Tolerance 10%
900
1000
1100
kHz
Conversion Rate
tCONV
Acquisition of Hall and
Temperature signals (no
digital filtering)
130
144
158
µs
fCONV
6.33
7
7.7
kHz
Programmable Filtering(2)
BW
Tempsensor enabled
0.004
1.114
kHz
Output Amplifier Rise Time
(10%-90%)(3)
tRISEPP
RL = 8 k to Ground
CL = 330 nF to Ground
300
µs
Output Amplifier Fall Time
(90%-10%)(3)
tFALLPP
RL = 330 k to Ground
CL = 330 nF to Ground
200
µs
Calibration Time(4)
tCALIB
EE Full Erase + Write
6
ms
EE Full Read
180
ms
RAM Write
3
ms
Table 6 gives the timing specifications
(1) Startup time is defined as the time between crossing the POR level and having the first DAC output update. It
includes loading of the parameters from EEPROM, checking the CRC validity, initializations and the signal latency
between the first Hall plate acquisition and the DAC output update.
(2) Filtering is programmable with the FILTCODE parameter in EEPROM. The filter consists of an IIR filter in the digital.
For more details about the corresponding bandwidths, see subsequent sections.
(3) Rise and fall times are measured for worst case conditions, hence the difference in Rload for both parameters.
These specifications are only defined by the output amplifier and its load. The output amplifier (Gain=2) is given a
step response at the input from 5%VDD to 45%VDD and the rise/fall times are measured as the time between
reaching 10% and 90% of the step response DC output voltages (10%VDD to 90%VDD).
(4) Calibration times measured at room temperature with PTC-04 and DB-HALL03 daughterboard, FIR090288AAMLX
firmware loaded onto the PTC-04 and on a MLX90288 in the recommended application diagram from subsequent
sections at 10kbit/s.
10. Transfer Characteristic Specification
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Output Clamping Range
CLAMPLO
9 bits(1)
0
50
%VDD
CLAMPHI
10 bits (1)
0
100
%VDD
Melex'i "" wswkin mmmmc
MLX90288
Datasheet
Page 9 of 23
REVISION 5 21 JULY 2017
3901090288
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Output Quiescent (Offset)
Voltage Range
VOQ
14 bits (YA setting) (1)
200
200
%VDD
Sensitivity Range
S
RG[2] = 1 (1)
For full-scale output(2)
0.04
0.4
%VDD/G
Table 7 gives the transfer characteristic specifications
(1) Please refer to subsequent sections for more detailed information.
(2) The full-scale output corresponds to 100%Vdd output range. This corresponds to 100% of the ADC range when
FINEGAIN is set to 1 (1024LSB) in a bipolar application. The DSP chain can additionally increase sensitivity by a
factor 4.
11. Accuracy Specification
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Output DAC Resolution
LSBDAC
12 bits
0.0244
%VDD
Output DAC Linearity
DNLDAC
1
+ 1
LSBDAC
INLDAC
2
+ 2
LSBDAC
Ratiometric Error(1)
OUTratiom
with TEMPTC=0
0.1
+ 0.1
%VDD
with TEMPTC=128
0.2
+ 0.2
%VDD
Output Noise(2)
OUTnoise
RG = 4, FG = 800
FILTCODE = 4
0.12
0.18
mVRMS
RG = 7, FG = 800
FILTCODE = 4
0.13
0.2
mVRMS
RG = 4, FG = 4095
FILTCODE = 4
0.75
1.1
mVRMS
RG = 7, FG = 4095
FILTCODE = 4
1
1.5
mVRMS
Thermal Output Quiescent
(Offset) Drift
ΔT VOQ
RG = 4
10
+ 10
LSBDAC
RG = 5
10
+ 10
LSBDAC
RG = 6
15
+ 15
LSBDAC
Melex'i "" wswkin muwzmc
MLX90288
Datasheet
Page 10 of 23
REVISION 5 21 JULY 2017
3901090288
Parameter
Symbol
Remark
Min
Typ
Max
Unit
RG = 7
20
+ 20
LSBDAC
Thermal Sensitivity Drift(3)
ΔT S
No magnet TC
150
0
+ 150
ppm/°C
Using 1st and 2nd order
magnet TC(4)
200
+ 200
ppm/°C
Sensitivity Thermal
Hystersis
ΔH S
After full thermal excursion
0.5
0.2
+ 0.5
%
Table 8 gives the accuracy specifications
(1) Ratiometric performance of the IC is measured as a difference in output voltage (expressed as %VDD) between the
nominal case with VDD = 5V and the limits of the supply ratiometric operating range (4.5V and 5.5V). The difference
between TEMPTC = 0 (or TEMPSENSOR disabled altogether) and TEMPTC = 128 originates in the fact that the on-
chip temperature is also a function of the supply voltage. Since the TEMPTC changes the gain of the IC to
compensate for the magnet TC, and it relies on the fact that the on-chip temperature is the same as the magnet
temperature, an extra error occurs compared to TEMPTC = 0 case.
(2) The noise measurements are performed on the recommended application diagram, with a supply voltage of 5V at
room temperature. Increased capacitance values compared to the recommended application diagram, contribute
to lower output noise. For peak-to-peak values, the RMS value is typically multiplied by a factor of 6.
(3) The Sensitivity Thermal Drift is within these boundaries for all ICs with the default setting for gain compensation i.e.
fixed to 1, which is obtained by setting TEMPTC to 0, but leaving the TEMPSENSOR bit set (see Subsequent Section).
If the value is not fixed to 1, the sensitivity of the IC will exhibit a sensitivity thermal drift curve such as the one
shown in the section on magnet compensation (if SECONDORDERTC is set) or with a linear temperature coefficient
(if SECONDORDERTC is cleared) depending on the setting of TEMPTC, but 150ppm/°C.
(4) This limit is an indication of what can be achieved for a typical magnet. The main assumption is that the magnet
strength monotonically decreases over temperature. Then, the 2nd order implementation as described in
subsequent sections has been designed to work up to ferrite magnets with a magnet TC of -2000ppm/°C. Please
contact Melexis when in doubt over the achievable specification for your magnet.
12. Diagnostic Specification
Parameter
Symbol
Remark
Min
Typ
Max
Unit
ADC Clipping Signaling(1)
DIAGCLIP
DIAGINFAULT = 0
-
-
VSATLO
%VDD
DIAGINFAULT = 1
VSATHI
-
-
%VDD
ADC Clipping Criterion(1)
NCLIP
ADC clipping count before
Diagnostic is set
-
4
-
Count
CRC Fail Signaling
DIAGPAR
DIAGINFAULT = 0
-
-
VSATLO
%VDD
DIAGINFAULT = 1
VSATHI
-
-
%VDD
CRC Fail Criterion
NCRC
CRC Fail count before
-
3
-
Count
Melex'i "" wswkin muwzmc
MLX90288
Datasheet
Page 11 of 23
REVISION 5 21 JULY 2017
3901090288
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Diagnostic is set
Broken VSS
(2)
VOUTbrVSS
Over RPD range
-
-
VDIAGLO
%VDD
Broken VDD
(2)
VOUTbrVDD
Over RPD range
-
-
VDIAGLO
%VDD
Table 9 gives the diagnostic level specifications
(1) ADC clipping is only flagged if the FAULTONCLIP bit in EEPROM is set. If the bit is cleared, the ADC will clamp at
either the maximum code or the minimum code, depending on the clipping condition. Reporting after 4 sequential
clipping conditions is required for an EMC robust design. Clipping reporting does not apply to ADC values of the
temperature signal.
(2) Diagnostics that are the result of a passive settling because the output stage becomes high impedant (such as
broken wire) are governed by the RC time constant of the capacitive load on the output and the RPD resistor at ECU
side. The OBD detection time is negligible in comparison to the settling time in case of a broken wire. The settling
time should be taken as 4 times the RC time constant. E.g. with a load of 330nF and 330kOhm, the RC time constant
equals 109ms. Settling time then corresponds to 4 RC time constants, i.e. 436ms.
13. Startup, Undervoltage, Overvoltage and Reset Specification
During power-up (supply rising from 0V upwards) the MLX90288 remains in a zone where the output is
undefined (grey triangular area in the plot) because there is no active circuitry putting the output stage in a
specific condition. Most likely the output remains close to the low rail because of the passive external pull -
down, but it cannot be predicted what happens exactly inside the IC at this point. This is also depicted in the
signal waveforms of this section.
The POR phase is the phase where the supply is still below VPORRISE, but above the undefined region. In
this case the digital is in a reset state, which puts all flip-flops in a known state, and the output is high
impedant. Due to the external pull-down resistive load, the output is at the low rail.
When the supply rises above the VPORRISE threshold (which has built-in hysteresis: for the falling edge,
VPORFALL), an initialization occurs which includes loading all EEPROM settings into RAM. After this
initialization phase, the chip will start its FSM program and provide a valid output signal, for as long as the
supply voltage is above the VUNDERRISE threshold (which has built-in hysteresis: for the falling edge,
VUNDERFALL). If the supply is below this threshold, the output remains in high impedant state,
corresponding to an output voltage at the low rail.
Whenever the MLX90288 goes from normal operation to undervoltage or via undervoltage to reset state,
and vice versa, the output has a settling time which is a function of both the output load and the driving
capability. On top of this, there is a startup time (tSTARTUP) in case the chip comes out of reset.
Meleiié' \ Mxl
MLX90288
Datasheet
Page 12 of 23
REVISION 5 21 JULY 2017
3901090288
Figure 2 Operating, undervoltage and reset functionality
In case the supply is raised above the VPROGRISE threshold (which has built -in hysteresis: for the falling
edge, VPROGFALL), but below the VOVER threshold, the IC goes in programming mode: the output becomes
high impedant and after proper commands coming from the programming unit (PTC04), the IC can respond
on the output pin as well. The communication protocol on the output (PTC -04 communication) is bi-
directional. If the supply is higher than the VOVER threshold, the internal regulated supply is disconnected
from the external supply, as are most blocks of the IC. A reset will be the result when the supply is restored.
14. EMC/ESD Specification
Parameter
Symbol
Remark
Min
Typ
Max
Unit
Micro-interrupt without
reset(1)
µI
-
-
0.1
µs
ESD Human Body Model(2)
ESDHBM
2
kV
ESD Charged Device
Model(3)
ESDCDM
500
V
(1) If the digital regulated voltage drops below POR level, the ASIC will reset nearly immediately; this is a
necessity from a DFMEA point of view. The only way to make the ASIC immune for longer micro-interrupts is
to have external components (Rseries and Csupply) filtering these micro -interrupts for the ASIC. Introducing
an Rseries in the supply line will have a negative impact on ratiometricity.
Vdd
time
Vout
time
tSTARTUP
Vporrise
Vporfall
Vunderrise
Vunderfall
INIT ratiometric normal operation (RNO) underV (uV) RNO INITPOR
tSTARTUP
uV
uVundefined POR
Mele_)'('i§""’
MLX90288
Datasheet
Page 13 of 23
REVISION 5 21 JULY 2017
3901090288
(2) ESD HBM test performed on all pins according to JEDEC-22-A-114 standard.
(3) ESD CDM test performed on all pins according to AEC-Q100-011 standard.
15. EEPROM Mapping
15.1. EEPROM Description
All calibration parameters on the MLX90288 are stored in a 32 x 16bit non-volatile EEPROM.
The EEPROM parameters from the first 29 addresses are stored with triple redundancy, to correct if any EEPROM bit would
loose its content, by using majority voting. Consequently, an EEPROM word in this part of EEPROM only holds the
information of 5 calibration bits + 1 locking bit at index 15. The EEPROM word stored at address 0 thus looks like this:
{LOCK0,PARAM[4:0],PARAM[4:0],PARAM[4:0]}
If bit index 15 is set, the EEPROM word is permanently locked, making it impossible to overwrite the given address in PTC
mode.
ID bits from the last 3 addresses are not stored with redundancy. The MLXID is not programmable in PTC mode, hence
guaranteeing traceability of the parts.
There are no constraints on the EEPROM readout in PTC mode.
15.2. Melexis Programmable Parameters
15.2.1. OSCTRIM [4:0]
Will be calibrated at MLX production
Trims oscillator frequency around 1 MHz
15.2.2. TRIMCTAT [4:0]
Will be calibrated at MLX production
Trims PTAT and CTAT to have both current sources at the same level at 25°C
This calibration is necessary to allow correct TC1 trimming with a single measurement at either hot or cold
The calibration compensates mismatch in both PTAT and CTAT current sources
15.2.3. ITRIM[2:0]
Will be calibrated at MLX production
Trims the current reference used throughout the analog part to a predefined value
15.2.4. IPLATE[3:0]
Will be calibrated at MLX production
Defines the current through the Hall plates, impacting the total gain
15.2.5. TC1ST[6:0]
Mele_)'('i§""’
MLX90288
Datasheet
Page 14 of 23
REVISION 5 21 JULY 2017
3901090288
Will be calibrated at MLX production
Programming first order sensitivity temperature drift compensation
Piecewise linear compensation between hot and cold temperatures = TC1ST
15.2.6. TC2ND[5:0]
Will be calibrated at MLX production
Programming piecewise linear sensitivity temperature drift compensation
It is like an additional TC1 starting at 25 °C +/-30 °C
Piecewise linear compensation for hot temperatures = TC1ST + TC2ND
15.2.7. TC3RD[2:0]
Will be calibrated at MLX production
Programming piecewise linear sensitivity temperature drift compensation
It is like an additional TC1 starting at - 5 °C
Piecewise linear compensation for cold temperatures = TC1ST + TC2ND + 2*TC3RD
15.2.8. PLATEPOL
Will be calibrated at MLX production
Changes the polarity of the Hall plates, inverting the sensing nodes
Changing the plate polarity will make the MLX production calibration void
Changing the polarity of the output signal is recommended to be achieved by changing the FINEGAIN MSB
15.2.9. OFFCST[4:0]
Will be calibrated at MLX production
Residual offset calibration (at Integrator stage) to make sure that the ADC input is at half of the ADC span when no
field is applied
Analog compensation, sign magnitude number
15.2.10. OFFDRIFT[5:0]
Will be calibrated at MLX production
Compensates linearly for residual offset temperature drift at the Integrator stage
Analog compensation, sign magnitude number
15.2.11. ROUGHGAIN[2]
Set by default to 1 by Melexis
15.2.12. XA[13:0]
Will be calibrated at MLX production
Gain-dependent offset, should not be modified after calibration
Removes the residual offset of the ADC output when no field is applied
15.2.13. MLXID[31:0]
Melex'is "" wswkin mmuzmc
MLX90288
Datasheet
Page 15 of 23
REVISION 5 21 JULY 2017
3901090288
Melexis ID bits for traceability
Can not be overwritten in PTC mode
15.2.14. CRC[9:0]
Standard CRC10 for data integrity
Polynomial is x10+x9+x5+x4+x1+1
EEPROM data is fed LSB first, per address (5bits, after majority voting) sequentially
The CRC integrity will be preserved by the PSF software when using the PTC04. It could not be changed manually
15.3. Melexis Programmable Parameters
15.3.1. FAULTONCLIP
Enable error reporting if ADC is clipping for 4 or more successive times
The diagnostic side for this error is defined by DIAGINFAULT
15.3.2. DIAGINFAULT
Defines to which side the output will go in case of an active error such as CRC fail or ADC clipping, the latter only in
case FAULTONCLIP is set
The thresholds are specified under the section on diagnostics.
15.3.3. FILTCODE[3:0]
The digital IIR filter offers noise reduction and low pass filtering with programmable cut off frequency
FILTCODE[3:0]
Cut-off frequency [Hz]
0
1114
1
557
2
279
3
139
4
70
5
35
6
17
7
9
8
4
Table 10: Filter cut-off frequencies
Mele_)'('i§""’
MLX90288
Datasheet
Page 16 of 23
REVISION 5 21 JULY 2017
3901090288
For Filter code from 9 to 15, the rounding error becomes too high versus the resolution so those codes are not
to be used.
This table only applies in case the temperature sensor is enabled, otherwise the cut-off frequency should be
multiplied by a factor of 2 since no more temperature ADC’s are performed anymore.
15.3.4. TEMPSENSOR
Enables digital gain compensation over temperature (GainMag)
Requires proper calibration of TEMPOFF and TEMPTC, as well as the SECONDORDERTC
15.3.5. SECONDORDERTC
Chooses between linear gain compensation over temperature (cleared) and ROM based 2nd order compensation
(set) as described under the section on magnet compensation
15.3.6. TEMPOFF[9:0]
Will be calibrated at MLX production
Defines the offset of the GainMag temperature compensation as described under Section Error! Reference source
ot found.
15.3.7. TEMPTC[7:0]
Will be calibrated at MLX production
Defines the slope of the GainMag temperature compensation as described under Section Error! Reference source
ot found.
15.3.8. CLPLow[8:0]
Low clamp level programmability range from 0% to 50% of VDD
Resolution is 1/4th of the outDAC resolution, i.e. 0.098% of VDD
15.3.9. CLPHigh[9:0]
High clamp level programmability range from 0% to 100% of VDD
Resolution is 1/4th of the outDAC resolution, i.e. 0.098% of VDD
15.3.10. ROUGHGAIN[1:0]
These 2 bits control the gain of the MAIN AMPLIFIER
15.3.11. ATTN2P5
Enables the attenuation in the analog chain by a factor of 4.5
15.3.12. FINEGAIN[12:0]
Mele_)'('i§""’
MLX90288
Datasheet
Page 17 of 23
REVISION 5 21 JULY 2017
3901090288
Sign-magnitude 13bit digital fine gain (not 2’s complement!)
The code 1024 (400h) corresponds to a gain of 1
The code 5120 (1400h) corresponds to a gain of -1
The MSB is a sign bit
FINEGAIN range is therefore from -4095 (1FFFh) to +4095 (FFFh), which corresponds to a gain range of -3.999 to
+3.999
15.3.13. YA[13:0]
Output offset programming, not gain dependent
Defines the offset on the output in case no field is applied, inside a range of -200%Vdd to +200% Vdd with the 12-bit
resolution of the output DAC, i.e. 0.0244% of VDD
15.3.14. CSTID[15:0]
Customer ID bits for traceability
Melex'is "" wswkin mmuzmc
MLX90288
Datasheet
Page 18 of 23
REVISION 5 21 JULY 2017
3901090288
16. Thermal Sensitivity Drift Compensation
16.1. Introduction
The embedded temperature sensor is digitized via the main path ADC before each analog amplified Hall
sensor voltage ADC in case TEMPSENSOR is enabled. This temperature information is used to generate eith er
an address for a ROM Look-up Table in order to obtain a quadratic temperature compensation
(SECONDORDERTC=1), or a value proportional to the temperature that allows a linear IC gain compensation
(SECONDORDERTC=0). Both compensations rely on the TEMPOFF and TEMPTC parameters.
16.2. Linear Compensation (1st Order)
The conventional linear temperature compensation proves to be adequate for small application temperature
ranges and/or small magnet temperature coefficients. In such cases the error induced by the line ar approach
are limited and prove to be good enough for the desired system sensitivity drift.
8.3 Quadratic Compensation (2nd Order)
This look up table is stored in ROM and contains the inverse transfer function of a specific magnetic flux
density over temperature. It should be used for magnets with temperature coefficients lower than -1500
ppm/degC, as is typically the case for plastic bonded magnets. Such magnet temperature coefficients cannot
optimally be compensated by the linear method. However, Melexis tooling together with the stored
compensation characteristic enable improved thermal drift compensation.
The correction factor GainMag is multiplied with the measured magnetic flux density. This multiplication
results in a (nearly) temperature independent sensitivity of the whole system (magnet + IC).
Figure 3: ROM table - 2nd order gain compensation (for illustrative purposes only)
The factory calibration performed by Melexis targets a specific magnet TC, which serves as accurate basis for
any delta calibration that should be performed when using a magnet with a different TC. This is performed
Gain compensation
0.85
0.9
0.95
1
1.05
1.1
1.15
1.2
1.25
1.3
-50.00 -30.00 -10.00 10.00 30.00 50.00 70.00 90.00 110.00 130.00 150.00
Temperature [Degree]
MeleXIs' soldermg recommendation. lead trimming and forming recommendations ht! www.me‘exis com an ualit renvwronmem
MLX90288
Datasheet
Page 19 of 23
REVISION 5 21 JULY 2017
3901090288
via the solver software provided by Melexis. The solver enables customers to address different sections in
the lookup table for different temperature ranges. This flexibility is to ensure a good match between
magnet TC and applied compensation.
17. Standard Information
Our products are classified and qualified regarding soldering technology, solderability and moisture sensitivity level
according to standards in place in Semiconductor industry.
For further details about test method references and for compliance verificati on of selected soldering method for
product integration, Melexis recommends reviewing on our web site the General Guidelines soldering
recommendation. For all soldering technologies deviating from the one mentioned in above document (regarding peak
temperature, temperature gradient, temperature profile etc), additional classification and qualification tests have to
be agreed upon with Melexis.
For package technology embedding trim and form post-delivery capability, Melexis recommends to consult the
dedicated trim&form recommendation application note: lead trimming and forming recommendations
Melexis is contributing to global environmental conservation by promoting lead free solutions. For more information
on qualifications of RoHS compliant products (RoHS = European directive on the Restriction Of the use of certain
Hazardous Substances) please visit the quality page on our website: http://www.melexis.com/en/quality-environment
18. ESD Precautions
Electronic semiconductor products are sensitive to Electro Static Discharge (ESD).
Always observe Electro Static Discharge control procedures whenever handling semiconductor products.
Melex'i?
MLX90288
Datasheet
Page 20 of 23
REVISION 5 21 JULY 2017
3901090288
19. Package Specification
19.1. Package Dimensions
Package Type: SOIC-8 (8-pin Small Outline Integrated Circuit Package)
Die placement accuracy is ± 2 mils = ± 50 microns.
0.19
0.25
NOTES:
All dimensions are in millimeters (angles in degrees).
* Dimension does not include mold flash, protrusions or
gate burrs (shall not exceed 0.15 per side).
** Dimension does not include interleads flash or protrusion
(shall not exceed 0.25 per side).
*** Dimension does not include dambar protrusion.
Allowable dambar protrusion shall be 0.08 mm total in
excess of the dimension at maximum material condition.
Dambar cannot be located on the lower radius of the foot.
5.80
6.20**
1.27 TYP
4.80
4.98*
1.52
1.72
0.100
0.250
1.37
1.57
0.36
0.46***
3.81
3.99**
0.41
1.27
Dimensions
2
0 +/- 0.30
0.44 +/- 0.10
1 43
78 56
3.90
+/- 0.09
Hall Plate location
Figure 4: Package Dimensions
Melex'ié'”
MLX90288
Datasheet
Page 21 of 23
REVISION 5 21 JULY 2017
3901090288
19.2. Package Marking
The package is labelled for traceability purposes, as depicted in this section’s figure.
The first line is reserved for the project number at Melexis, 90288 followed by the ASIC silicon version. The line below refers
to the wafer fab. The bottom line is the date code indicating when the bare dies were packaged at the assembly house. The
black dot indicates the position of pin #1.
MXXXXX = 5-digit lot number (M = wafer fab)
YYWW = last 2 digits of the year, followed by the calendar week
1 4
58
90288C
MXXXXX
YYWW
Figure 5: Package markings
—IF 4W l www.melexis.com. Melex'ié'”
MLX90288
Datasheet
Page 22 of 23
REVISION 5 21 JULY 2017
3901090288
19.3. Recommended Application Diagram
1 4
58
VDD
OUT
GND
C1 C2
C1 = 100nF
C2 = 100nF
Figure 6: Recommended Application Diagram
The testpins (#5, #6, #7, #8) need to be grounded to avoid the risk of the chip going into testmode because
of RF/noise entering the test controller on these pins. The test input pins have an internal pull -down
resistor.
The recommended application diagram is not a mandatory design guide. For better ESD and EMC
performance external components can be modified for as long as the electrical specifications are followed
under previous sections. For good EMC performance the components should be placed as close as possible
to the IC.
20. Revision History Table
21/07/2017
Conversion of 90288CA datasheet to new template of datasheet
Table 11
21. Contact
For the latest version of this document, go to our website at www.melexis.com.
Melex'is "" wswkin mwmm
MLX90288
Datasheet
Page 23 of 23
REVISION 5 21 JULY 2017
3901090288
For additional information, please contact our Direct Sales team and get help for your specific needs:
Europe, Africa
Telephone: +32 13 67 04 95
Email : sales_europe@melexis.com
Americas
Telephone: +1 603 223 2362
Email : sales_usa@melexis.com
Asia
Email : sales_asia@melexis.com
22. Disclaimer
The information furnished by Melexis herein (“Information”) is believed to be correct and accurate. Melexis disclaims (i) any and all liability in connection with or arising out of the
furnishing, performance or use of the technical data or use of the product(s) as described herein (“Product”) (ii) any and all liability, including without limitation, special,
consequential or incidental damages, and (iii) any and all warranties, express, statutory, implied, or by description, including warranties of fitness for particular purpose, non-
infringement and merchantability. No obligation or liability shall arise or flow out of Melexis’ rendering of technical or other services.
The Information is provided "as is” and Melexis reserves the right to change the Information at any time and without notice. Therefore, before placing orders and/or prior to
designing the Product into a system, users or any third party should obtain the latest version of the relevant information to verify that the information being relied upon is current.
Users or any third party must further determine the suitability of the Product for its application, including the level of re liability required and determine whether it is fit for a
particular purpose.
The Information is proprietary and/or confidential information of Melexis and the use thereof or anything described by the Information does not grant, explicitly or implicitly, to
any party any patent rights, licenses, or any other intellectual property rights.
This document as well as the Product(s) may be subject to export control regulations. Please be aware that export might require a prior authorization from competent authorities.
The Product(s) are intended for use in normal commercial applications. Unless otherwise agreed upon in writing, the Product(s) are not designed, authorized or warranted to be
suitable in applications requiring extended temperature range and/or unusual environmental requirements. High reliability applications, such as medical life-support or life-
sustaining equipment are specifically not recommended by Melexis.
The Product(s) may not be used for the following applications subject to export control regulations: the development, product ion, processing, operation, maintenance, storage,
recognition or proliferation of 1) chemical, biological or nuclear weapons, or for the development, production, maintenance o r storage of missiles for such weapons: 2) civil
firearms, including spare parts or ammunition for such arms; 3) defense related products, or other material for military use or for law enforcement; 4) any applications that, alone
or in combination with other goods, substances or organisms could cause serious harm to persons or goods and that ca n be used as a means of violence in an armed conflict or any
similar violent situation.
The Products sold by Melexis are subject to the terms and conditions as specified in the Terms of Sale, which can be found at https://www.melexis.com/en/legal/terms-and-
conditions.
This document supersedes and replaces all prior information regarding the Product(s) and/or previous versions of this documen t.
Melexis NV © - No part of this document may be reproduced without the prior written consent of Melexis. (2016)
ISO/TS 16949 and ISO14001 Certified

Products related to this Datasheet

SENSOR HALL EFFECT ANALOG 8SOIC
SENSOR HALL EFFECT ANALOG 8SOIC
SENSOR HALL EFFECT ANALOG 8SOIC
SENSOR HALL EFFECT ANALOG 8SOIC
SENSOR HALL EFFECT ANALOG 8SOIC
SENSOR HALL EFFECT ANALOG 8SOIC