AD62x/AD822x Eval Brd Guide Datasheet by Analog Devices Inc.

ANALOG DEVICES
Evaluation Board User Guide
UG-261
One Technology Way P. O. Box 9106 Norwood, MA 02062-9106, U.S.A. Tel: 781.329.4700 Fax: 781.461.3113 www.analog.com
Evaluation Boards for the AD62x Series and the AD822x Series
Instrumentation Amplifiers
PLEASE SEE THE LAST PAGE FOR AN IMPORTANT
WARNING AND LEGAL TERMS AND CONDITIONS. Rev. C | Page 1 of 8
FEATURES
3 generic, easy-to-use evaluation boards
Shipped with an assortment of Analog Devices, Inc., in-amps
Solder in the in-amp to be tested
Test pins already populated
Decoupling capacitors already populated
EVAL-INAMP-62RZ board
Compatible with AD620, AD621, AD622, AD623, AD627,
AD8223, and AD8225 in SOIC or PDIP
EVAL-INAMP-82RZ board
Compatible with AD8221, AD8226, AD8227, AD8228,
AD8229, AD8421, AD8428, and AD8429 in SOIC package
EVAL-INAMP-82RMZ board
Compatible with AD8220, AD8221, AD8226, AD8227,
AD8228, AD8236, and AD8421 in MSOP package
09753-001
Figure 1.
GENERAL DESCRIPTION
This user guide describes three generic evaluation boards that
can be used to evaluate many of Analog Devices instrumentation
amplifiers. For information on the performance of a specific
instrumentation amplifier, see the data sheet for that
instrumentation amplifier.
EVAL-INAMP-62RZ (SOIC or PDIP)
The EVAL-INAMP-62RZ is designed for evaluation of
instrumentation amplifiers in the legacy pinout. This board
can be used to evaluate the AD620, AD621, AD622, AD623,
AD627, AD8223, and AD8225 instrumentation amplifiers. In
addition to the basic in-amp connection, circuit options enable
the user to adjust the offset voltage, apply an output reference,
or provide shield drivers with user-supplied components. The
board is shipped with an assortment of instrumentation amplifier
ICs in the legacy SOIC pinout, typically AD620, AD621, AD622,
AD623, AD8223, and AD8225. The board also has an alternative
footprint for a through-hole, 8-lead PD I P.
EVAL-INAMP-82RZ (SOIC)
The EVAL-INAMP-82RZ is designed for evaluation of
instrumentation amplifiers in the high performance pinout.
This board can be used to evaluate the AD8221, AD8226,
AD8227, AD8228, AD8229, AD8421, AD8428, and AD8429
in SOIC packages. The board is shipped with an assortment of
instrumentation amplifier ICs in the high performance SOIC
pinout, typically AD8221, AD8226, AD8421, AD8428, and
AD8429. The evaluation board is arranged so that users can
easily solder on the gain resistor. The in-amp reference pin can
be connected to ground through a solder short or connected to
the users source through the test pin. A small prototyping area
allows interfacing to another part in an SOIC package.
Users can add their own SMA or SMB connector to interface
the evaluation board with complementary tools, such as an
analog-to-digital converter (ADC) evaluation board, available
from Analog Devices.
EVAL-INAMP-82RMZ (MSOP)
The EVAL-INAMP-82RMZ board is exactly the same as the
EVAL-INAMP-82RZ board, except that is designed for the
MSOP pinout. This board can be used to evaluate the AD8220,
AD8221, AD8226, AD8227, AD8228, AD8236, and AD8421 in
MSOP packages. The EVAL-INAMP-82RMZ board ships with
an assortment of in-amp ICs in the high performance MSOP
pinout, typically AD8220, AD8221, AD8226, AD8228, and
AD8421.
UG-261 Evaluation Board User Guide
Rev. C | Page 2 of 8
TABLE OF CONTENTS
Features .............................................................................................. 1
General Description ......................................................................... 1
Revision History ............................................................................... 2
E VA L-INAMP-62RZ Details ........................................................... 3
Quick Start for the EVAL-INAMP-62RZ Board .......................... 4
Circuit Options ............................................................................. 4
Load Resistor ................................................................................. 4
CMRR Performance ..................................................................... 4
Guard Drivers ................................................................................5
Component Locations ..................................................................5
User Options ..................................................................................6
Quick Start for the EVAL-INAMP-82RZ and EVAL-INAMP-
82RMZ Boards ...................................................................................7
Reference ........................................................................................7
Output .............................................................................................7
REVISION HISTORY
6/12Rev. B to Rev. C
Changes to Features Section, EVAL-INAMP-62RZ (SOIC or
PDIP) Section, E VA L -INAMP-82RZ (SOIC) Section, and
E VA L-INAMP-82RMZ (MSOP) Section ...................................... 1
Changes to Quick Start for the EVAL-INAMP-82RZ and
EVAL-INAMP-82RMZ Boards Section ........................................ 7
3/11Rev. A to Rev. B
Changed Format to User Guide ................................... Throughout
Changes to Document Title ............................................................ 1
Changes to Features Section............................................................ 1
Deleted Applications Section .......................................................... 1
Changes to General Description Section ...................................... 1
Added CMRR Performance Section .............................................. 4
Added Component Locations Section ........................................... 5
11/08Rev. 0 to Rev. A
Combined AD623-EVALZ Data Sheet and AD623-EVA L
Data Sheet ............................................................................ Universal
Added AD8220/AD8221-EVAL Z .............................. Throughout
Changed AD623-EVALZ to AD620 Series-E VA L Z ........ Throughout
Changes to General Description ..................................................... 1
Added EVAL-INAMP-62RZ Details Section ................................. 3
Added Quick Start for the EVAL-INAMP-62RZ Boards Section ..... 4
Changes to Gain Adjustment Section ............................................. 4
Added Table 1 and Table 2; Renumbered Sequentially ................ 4
Changed Appendix Heading to User Options ............................... 6
Added Quick Start for the EVAL-INAMP-82RZ Section and
E VA L-INAMP-82RMZ Boards Section ......................................... 7
Changes to Ordering Guide ............................................................. 8
12/07Revision 0: AD623-EVALZ Initial Version
6/03Revision 0: AD623-EVAL Initial Version
Evaluation Board User Guide UG-261
Rev. C | Page 3 of 8
EVAL-INAMP-62RZ DETAILS
5
W15
A3
OUTPUT
REF
7
45
6OUTPUT
EXT_REF
R8
2
37
4
6
6
4
7
OFFSET ADJ.
OP177
W13
W11
W12
2
38
1
W8
W10
3
8
1
2
W5
W9
W2
W1
W3
GND2
+IN
+GUARD
–GUARD
–IN
GND1
W14
A2
A2
A1
R2
100Ω
R4
100Ω
REMOVE W3 AND W4 FOR AC COUPLING.
C1, 0.1µF
+V
AUX
C6
0.1µF
C5
0.1µF –V
AUX
R3
100kΩ
1
R5
100kΩ
1
R5
2
R6
2
W4
C3, 0.1µF
R
G
–R
G
+R
G
+V
S
–V
S
C4
0.1µF
C2
0.1µF C10
0.1µF
C7
0.1µF
+V
AUX
–V
AUX
–V
AUX
C8
0.1µF
OP177
CS2
J500
240µA
CS2
J500
240µA
R9
5.9kΩ, 1%
R10
5.9kΩ, 1%
R1
100kΩ
C9
0.1µF
NOTES
1
INSTALL FOR AC COUPLING ONLY.
2
TO USE GUARD DRIVER, INSTALL R5 AND R6
INSTEAD OF R
G
. R5 AND R6 = 0.5R
G
.
W6
W7
C12
10µF
25V
C11
10µF
25V
GND
+
+
–V
AUX
+V
AUX
+V
S
–V
S
COMPONENTS IN SHADED AREAS
ARE USER SUPPLIED.
+
AD708J
AD708J
09753-002
Figure 2. EVAL-INAMP-62RZ (AD62x Series) Schematic Diagram
Table 3‘ AD623 Gain Resistor Values
UG-261 Evaluation Board User Guide
Rev. C | Page 4 of 8
QUICK START FOR THE EVAL-INAMP-62RZ BOARD
CIRCUIT OPTIONS
Single-Supply Operation
A jumper is provided to select between single or dual power
supplies. The evaluation board is shipped with W14 in the dual-
supply position. To convert to single supply, place W14 in the
position marked with a ground symbol.
Gain Adjustment
The gain of the AD621 is pin selectable where G = 1 (default) or
G = 100 (strap Pin 1 and Pin 8). In contrast, the gain of the AD620,
AD622, and AD623 devices is resistor dependent (the resistor is
connected between the RG pins). Without a resistor, the gain is
unity. Table 1 to Table 3 provide calculated gains for each device.
See the individual product data sheet for the gain equations.
Table 1. AD620 Gain Resistor Values
1% Standard
Value of RG (Ω)
Calculated
Gain
0.1% Standard
Value of RG (Ω)
Calculated
Gain
49.9 k 1.990 49.3 k 2.002
12.4 k
4.984
12.4 k
5.49 k 9.998 5.49 k 9.998
2.61 k 19.93 2.61 k 19.93
1.00 k 50.40 1.01 k 49.91
499 100.0 499 100.0
249 199.4 249 199.4
100 495.0 98.8 501.0
49.9 991.0 49.3 1003.0
Table 2. AD622 Gain Resistor Values
Desired Gain 1% Standard Value of RG (Ω) Calculated Gain
2 51.1 k 1.988
5 12.7 k 4.976
10 5.62 k 9.986
20 2.67 k 19.91
33 1.58 k 32.96
40 1.3 k 39.85
50 1.02 k 50.50
65 787 65.17
100 511 99.83
200 255 199.0
500 102 496.1
1000 51.1 989.3
Table 3. AD623 Gain Resistor Values
Desired Gain
1% Standard Value of RG (Ω) Calculated Gain
2 100 k 2
5
24.9 k
5.02
10 11 k 10.09
20 5.23 k 20.12
33 3.09 k 33.36
40 2.55 k 40.21
50 2.05 k 49.78
65 1.58 k 64.29
100 1.02 k 99.04
200 499 201.4
500 200 501
1000 100 1001
External Reference or Offset Adjustment
When shipped, the reference of the EVAL-INAMP-62RZ board
is connected to ground. Certain single-supply applications (for
example, an ADC connected to the output of the in-amp) require a
symmetrical output voltage centered on a nonzero value. The
reference can be equal to half the supply, or an application-specific
voltage can be provided by an ADC. The user can install a jumper
at W13 and connect an external reference to the EXT_REF pin.
To maintain proper operation of the in-amp, the reference
should be provided by a voltage source.
Similarly, a provision is made for an offset adjustment of ±1.12 V
by installing the parts listed in Table 6. Although the A2 and A3
ICs can be used with a single or dual power supply connection,
A1 requires a dual supply. To enable the offset feature, install a
shunt in Position W11. To adjust the offset of the in-amp,
ground both inputs and measure the output voltage. Adjust
Potentiometer R1 for 0 V.
LOAD RESISTOR
Although not required for normal operation, a load resistor can
be inserted at Position R8.
CMRR PERFORMANCE
The AD621 CMRR performance degrades at gains of 100 when
using this board due to the high performance of the AD621.
Evaluation Board User Guide UG-261
Rev. C | Page 5 of 8
GUARD DRIVERS
When interference from sources such as power lines must be
reduced to levels below those provided by standard shielded
cables, guard drivers may be effective. A guard equalizes the ac
potential between the in-amp input and the cable shield of the
line, effectively reducing the low frequency interference voltage.
A2 in Figure 3 is a dual op amp AD708 driving the shield(s) of
the input cable(s) from the gain resistor pins of the in-amp. The
voltages at these pins are equal to the input voltages plus 0.6 V
(see the device data sheet).
The E VA L -INAMP-62RZ provides single and differential guards.
Differential guards drive the shields with essentially the same
signals as the inputs, whereas the single guard can be used for
dual conductor cables. In this mode, the +GUARD drives the
shield at ½(VIN DIFF) + 0.6 V.
To activate the guard drivers, +VAUX and VAUX must be connected.
For shielded cables at both inputs, install the W1, W2, W5,
and W8 jumpers.
Using a Single Guard
When using the AD620, AD622, and AD623 for gains greater
than 1, install Resistors R6 and R11 (which are each half the
calculated resistance of RG) and Jumpers W1, W2, and W10.
For a gain of 1, either Position R6 or Position R11 can be shorted
to enable the guard driver input. Connect the shield to +GUARD.
On the header pins that do not bear the ground symbol, insert a
shunt across Position W1.
The guard drivers can be assembled using the components
listed in Table 6.
COMPONENT LOCATIONS
Figure 3 shows the component layout and the location of
connections for the EVAL-INAMP-62RZ board.
INPUT
OUTPUT
POWER
09753-003
Figure 3. Component Location for the EVAL-INAMP-62
UG-261 Evaluation Board User Guide
Rev. C | Page 6 of 8
USER OPTIONS
Table 4. Jumpers
Jumper Function Description Status
W1
+GUARD select
Allows the shield of the positive input cable to be connected to the guard driver or ground.
Not installed
W2 −GUARD select Allows the shield of the negative input cable to be connected to the guard driver or ground. Not installed
W3 +Input coupling Installed; the positive input is dc-coupled. Installed
W4 −Input coupling Installed; the negative input is dc-coupled. Installed
W5 Guard driver −IN Connects the negative shield guard driver to Pin 1 of the in-amp. Not installed
W6 −VS to − VAUX Connects the negative supply voltage to the negative auxiliary voltage of the same value. Not installed
W7 +VS to + VAUX Connects the positive supply voltage to the positive auxiliary voltage of the same value. Not installed
W8 Guard driver +IN Connects the positive shield guard driver to Pin 8 of the in-amp. Not installed
W9 Guard driver +IN Connects the positive shield guard driver to ground. Not installed
W10 Guard driver +IN Selects the single-shield guard driver. Not installed
W11 Reference input Connects the reference of the in-amp to the offset-adjustable voltage reference. Not installed
W12 Reference input Connects the reference of the in-amp to ground. Installed
W13 Reference input Connects the reference of the in-amp to an external reference supply. Not installed
W14 In-amp −VS source Connects the in-amp −VS pin to GND or to −VS of the evaluation board. Connected to −VS
W15 Guard driver −IN Connects the negative shield guard driver to ground. Not installed
Table 5. Input/Output
I/O Function
+VS/−VS Positive and negative rails of the in-amp.
GND Ground for the board. GND1, GND2, GND3, and GND4 designate pins.
+IN/−IN
Positive and negative inputs of the in-amp.
+GUARD/−GUARD Positive and negative terminals for use with a shielded cable.
EXT_REF External reference input for the in-amp.
OUTPUT Output of the in-amp.
+VAUX/−VAUX Auxiliary power rails for guard drivers and offset reference circuitry.
Table 6. User-Supplied Parts for Guard and Offset Circuits
Reference Designation Part
Guard Drivers
C5, C6
0.1 µF, 25 V ceramic capacitor
A2 AD708JN dual precision op amp
Offset Regulators
C7 to C10 0.1 µF, 25 V ceramic capacitor
A1 OP177 precision op amp
CS1, CS2 J500 240 µA current source
R9, R10 5.9 k, 1% metal film resistor
Table 7‘ Factory mung oo j a 67 Q} 3} {
Evaluation Board User Guide UG-261
Rev. C | Page 7 of 8
QUICK START FOR THE EVAL-INAMP-82RZ AND EVAL-INAMP-82RMZ BOARDS
The quick start instructions in this section assume that the
evaluation board is in default condition as shown in Table 7.
This section describes two separate evaluation boards, where
the EVAL-INAMP-82RZ has an SOIC footprint and the
EVAL-INAMP-82RMZ has an MSOP footprint.
Table 7. Factory Setting
Connection Purpose
W1 is soldered. REF is tied to ground.
Follow Step 1 through Step 3 to get started using these boards
(see Figure 4).
1. Connect a ±2.3 V to ±15 V supply to +VS and VS. (Consult
the specific data sheet for power supply operating range.)
2. Drive the inputs with a signal.
3. Measure the output on a multimeter or oscilloscope. The
output voltage is the voltage measured between VOUT (OUT)
and VREF (REF). The output can drive another device, such
as an ADC.
10µF0.1µF
10µF 0.1µF
+V
S
–V
S
+IN +IN 48+V
S
5–V
S
7 V
OUT
6 V
REF
–IN 1
R
G
3
R
G
2
IN
W1
REF
OUT
R1 DUT
+
SMA/SMB
CONNECTOR
(OPTIONAL)
09753-004
Figure 4. EVAL-INAMP-82RZ Schematic
REFERENCE
The reference level of the instrumentation amplifier can be set
by driving the REF pin with a precision voltage reference or by
using the solder jumper, W1. By default, W1 is soldered, shunting
REF to ground. If a reference voltage other than ground is used,
the solder must be removed from W1 before driving REF with
the reference voltage, as shown in Figure 5.
+IN
IN
W1
REF
OUT
10V
5V
5V
10µF0.1µF
10µF 0.1µF
DUT
+
1V p-p, 1kHz
+V
S
–V
S
0V
OSCILLOSCOPE
+COM
09753-005
Figure 5. Using an External Voltage Source to Set the
Reference Level (Circled) Input
Do not leave the in-amp inputs floating, that is, without a dc
return path. This often occurs when the inputs are connected to
a transformer, a thermocouple, or a pair of series capacitors.
The inputs should have a dc path to ground, as shown in Figure 5
and Figure 6.
The circuit shown in Figure 6 has series capacitors, C1 and C2,
between the signal generator and the input. The series capacitors
prevent a dc current from flowing into the input transistors of
the instrumentation amplifier. Two matched 10 kΩ resistors are
used between the instrumentation amplifier inputs and ground
to provide the necessary current path. Closely match these
resistors to reduce offset and CMRR errors.
OSCILLOSCOPE
+COM
W1
REF
OUT
+15V 10µF
–15V
0.1µF
10µF 0.1µF
DUT
+
+VS
–VS
R1
499Ω
10kΩ 10kΩ
+IN
–IN
C2
C1
09753-006
Figure 6. AC Input Coupling Using a Resistive DC Return Path
OUTPUT
Output measurements should be made by monitoring the voltage
between the OUT and REF tie points of the board, as shown in
Figure 7. If an external voltage reference is used, the output can
be measured, referred to ground, as shown in Figure 5. The
evaluation board offers an SMA/SMB outline. By default, the
output voltage measured using an SMA/SMB connector is with
respect to ground.
W1
REF
OUT
+15V 10µF
–15V
0.1µF
10µF 0.1µF
DUT
+
500mV p-p,
100Hz
10V p-p,
10Hz
+V
S
–V
S
OSCILLOSCOPE
+COM
R1
5.49kΩ
+IN
–IN
09753-007
Figure 7. Correct Output Connection Using the REF Pin
UG-261 Evaluation Board User Guide
Rev. C | Page 8 of 8
NOTES
ESD Caution
ESD (electrostatic discharge) sensitive device. Charged devices and circuit boards can discharge without detection. Although this product features patented or proprietary protection
circuitry, damage may occur on devices subjected to high energy ESD. Therefore, proper ESD precautions should be taken to avoid performance degradation or loss of functionality.
Legal Terms and Conditions
By using the evaluation board discussed herein (together with any tools, components documentation or support materials, the “Evaluation Board”), you are agreeing to be bound by the terms and conditions
set forth below (“Agreement”) unless you have purchased the Evaluation Board, in which case the Analog Devices Standard Terms and Conditions of Sale shall govern. Do not use the Evaluation Board until you
have read and agreed to the Agreement. Your use of the Evaluation Board shall signify your acceptance of the Agreement. This Agreement is made by and between you (“Customer”) and Analog Devices, Inc.
(“ADI”), with its principal place of business at One Technology Way, Norwood, MA 02062, USA. Subject to the terms and conditions of the Agreement, ADI hereby grants to Customer a free, limited, personal,
temporary, non-exclusive, non-sublicensable, non-transferable license to use the Evaluation Board FOR EVALUATION PURPOSES ONLY. Customer understands and agrees that the Evaluation Board is provided
for the sole and exclusive purpose referenced above, and agrees not to use the Evaluation Board for any other purpose. Furthermore, the license granted is expressly made subject to the following additional
limitations: Customer shall not (i) rent, lease, display, sell, transfer, assign, sublicense, or distribute the Evaluation Board; and (ii) permit any Third Party to access the Evaluation Board. As used herein, the term
“Third Party” includes any entity other than ADI, Customer, their employees, affiliates and in-house consultants. The Evaluation Board is NOT sold to Customer; all rights not expressly granted herein, including
ownership of the Evaluation Board, are reserved by ADI. CONFIDENTIALITY. This Agreement and the Evaluation Board shall all be considered the confidential and proprietary information of ADI. Customer may
not disclose or transfer any portion of the Evaluation Board to any other party for any reason. Upon discontinuation of use of the Evaluation Board or termination of this Agreement, Customer agrees to
promptly return the Evaluation Board to ADI. ADDITIONAL RESTRICTIONS. Customer may not disassemble, decompile or reverse engineer chips on the Evaluation Board. Customer shall inform ADI of any
occurred damages or any modifications or alterations it makes to the Evaluation Board, including but not limited to soldering or any other activity that affects the material content of the Evaluation Board.
Modifications to the Evaluation Board must comply with applicable law, including but not limited to the RoHS Directive. TERMINATION. ADI may terminate this Agreement at any time upon giving written notice
to Customer. Customer agrees to return to ADI the Evaluation Board at that time. LIMITATION OF LIABILITY. THE EVALUATION BOARD PROVIDED HEREUNDER IS PROVIDED AS IS AND ADI MAKES NO
WARRANTIES OR REPRESENTATIONS OF ANY KIND WITH RESPECT TO IT. ADI SPECIFICALLY DISCLAIMS ANY REPRESENTATIONS, ENDORSEMENTS, GUARANTEES, OR WARRANTIES, EXPRESS OR IMPLIED, RELATED
TO THE EVALUATION BOARD INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTY OF MERCHANTABILITY, TITLE, FITNESS FOR A PARTICULAR PURPOSE OR NONINFRINGEMENT OF INTELLECTUAL
PROPERTY RIGHTS. IN NO EVENT WILL ADI AND ITS LICENSORS BE LIABLE FOR ANY INCIDENTAL, SPECIAL, INDIRECT, OR CONSEQUENTIAL DAMAGES RESULTING FROM CUSTOMER’S POSSESSION OR USE OF
THE EVALUATION BOARD, INCLUDING BUT NOT LIMITED TO LOST PROFITS, DELAY COSTS, LABOR COSTS OR LOSS OF GOODWILL. ADI’S TOTAL LIABILITY FROM ANY AND ALL CAUSES SHALL BE LIMITED TO THE
AMOUNT OF ONE HUNDRED US DOLLARS ($100.00). EXPORT. Customer agrees that it will not directly or indirectly export the Evaluation Board to another country, and that it will comply with all applicable
United States federal laws and regulations relating to exports. GOVERNING LAW. This Agreement shall be governed by and const
rued in accordance with the substantive laws of the Commonwealth of
Massachusetts (excluding conflict of law rules). Any legal action regarding this Agreement will be heard in the state or federal courts having jurisdiction in Suffolk County, Massachusetts, and Customer hereby
submits to the personal jurisdiction and venue of such courts. The United Nations Convention on Contracts for the International Sale of Goods shall not apply to this Agreement and is expressly disclaimed.
©20032012 Analog Devices, Inc. All rights reserved. Trademarks and
registered trademarks are the property of their respective owners.
UG09753-0-6/12(C)