Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
sound requirements2
The first requirement is that the fundamental frequency must be between 150Hz and 1kHz. The fundamental frequency is the first main frequency component of a sound. As shown in this graph, the first frequency component of this sound is around 900Hz. Therefore, this sound does have a fundamental frequency between 150Hz and 1kHz.
PTM Veröffentlicht am: