Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
High Performance X2 Film Capacitors, the F862 Series Slide 14

This table here just shows that the dissipation factor of polypropylene is one order of magnitude lower than polyester. This allows continuous operation with no ‘self-heating’ also in presence of ripple current. X2 capacitors need sometimes to withstand not only to 50 – 60 Hz voltage, but to high frequency voltage ripple, too.

PTM Veröffentlicht am: